全 2268 件が検索されました。(541 - 560件を表示)

  • マニュアル

    ...US(0x1F) または Delete(0x7F) 文字シフトインジケータ 1 1 1 1 1 1 入力文字と Code Set A / B における意味入力 Sp ! " # $ % & ' ( ) * + , . / Code A Sp ! " # $ % & ' ( ) * + , . / Code B Sp ! " # $ % & ' ( ) * + , . / 入力 0 1 2 3 4 5 6 7 8 9 : ; < = > ? Code A 0 1 2 3 4 5 6 7 8 9 : ; < = > ? Code B 0 1 2 3 4 5 6 7 8 9 : ; < = > ? 入力 @@ A B C D E F G H I J K L M N...

  • マニュアル

    ...Alarm display Temp. Alarm 11:01 Screen 1 7 8 9 4 5 6 Menu Touch switch SV PV Fixed display-text Graph display String Display Data input (numeral input) 1 2 3 SP 0 CR Numeral display 3 What Is Support Tool? Section 1-1 Product Configuration The NT-series Support Tool for Windows (Ver. 4.) consists of the following software and data. Support Tool Specifications Model number NT-ZJCAT1-EV4 For IBM PC/AT or compatible, media: CD-ROM Keyboard tenkey library Color pallette symbols (Library of parts for filling with color models) System Installer (to replace PT ...

  • マニュアル

    ... info Display, I/O Status Monitor etc. 7. Device Net (DRT2-xx) Models integrated in one SMART Active Parts.DRT2 maintenance/Status info, IN/OUT Info. Etc. 8. Temperature Controller (E5[]R, E5ZN, E5[]N)- Direct Connection with NS. Run Monitor, PID Settings, ...

  • マニュアル

    ..., displaying the first two letters of the network provider name followed by the error ID, as shown below. The error ID is displayed 2 digits at a time. CL → 00 → 08 → DR → 00 → 52 → HL → 00 → 13 syslog File CP CPU_UNIT ...

  • マニュアル

    ... Unit, providing an easy means to see trends in process data, analyze relationships between data and quality, and achieve other data/ system management applications. 2 Section 1-2 SYSMAC SPU Unit Features CS-series CPU Unit SPU Unit Setting/Monitoring Software ...

  • マニュアル

    ... tool 】 The address used on the screen is displayed The CX-Programmer (CXSimulator) of the back is [Monitor mode]. PV on the screen is added automatically by pressing the “RUN” button. The ”STOP” button lights up when PV reaches ...

  • マニュアル

    ...1. Turn ON the power for the V680-CA5Dxx. 2. The following appears on the monitor display. - Label None - Label Unit Version Model V680-CH1D/-CHUD/-CH1D-PSI Model V680-CH1D/-CHUD/-CH1D-PSI - Parameter data L of PARAMETER SET (...

  • マニュアル

    ...を使用してください。 推奨電源 : 形 S8VS-03024 (オムロン製) 24V GND (7) アンテナ接続コネクタ GR アンテナ形V680-HS63-SPを接続 (1) 動作表示LED ■DEV (デバイスステータス) 状態意味緑点灯正常状態赤点灯致命的な故障赤点滅軽微な故障消灯電源供給なし 28.5...

  • マニュアル

    ... FORCED SET/RESET STATUS READ (C200H, C200HS, C200HX, C200HG, C200HE, and Mini H-type only.) Reads the forced set or forced reset status of the PC to which the specified Host Link Unit is mounted. When the operand is a timer/counter instruction (i.e., TIM(...

  • マニュアル

    ... character set comprises alphabetical characters, numeric characters, and special characters. The alphabetic characters in BASIC are the upper case and lower case letters of the alphabet. The numeric characters in BASIC are the digits 0 through 9. The following special characters are recognized by BASIC: ...

  • マニュアル

    ... a heater burnout detection setting range of 0.1 to 4.9 A, and allows for the rapid correction of problems. Heater burnout detection is possible for each of the two control loops. Eight Banks of Data Settings Eight data values such as set point (...

  • マニュアル

    ...口usesaplatinumresistancethermemeter. 1「woHeaVCoolControlLoopswlthaSlngleUnlt TWoheatingandcoolingcontrolloopsarep◎ssiblewithoneUnit. Comprehenslve◎utputSpeclflcatlons Threetypesofoutputspecificationversiensareavailable:C200H-↑V口口1for transistoroutput,C200H-TV口口2forvoltageoutput,andC200H-TV口口3for currentoutput. HeaterBu『nOUtDeteCtlOn ACurrentTransformer(withadetectioncurrentrangeofO.1to49.9Aandaminimumdetectioncurrentdifferenceof2.5A)canbeconnectedtoeachofthetwo controlbopstofacilitaterapidheaterburnoutdetectionandpromptcorrectionof problems. EightBanksofDataSettings EightdatavaluessuchassetpOint(...

  • マニュアル

    ... effective in quick-response systems. Comprehensive Output Specifications Three types of output specification versions are available: C200H-PID01 for transistor output, C200H-PID02 for voltage output, and C200H-PID03 for current output. Eight Banks of Data Settings Eight data values such as set point (...

  • マニュアル

    ...q N No. Communications sequence q name Function Ladder interface Send word allocation Yes Receive word allocation Yes 000 Read process value Reads the process value. 001 Read set point during SP ramp Yes Yes 002 Read MV Reads the set point during ...

  • マニュアル

    ...The BASIC character set comprises alphabetical characters, numeric characters, and special characters. The alphabetic characters in BASIC are the uppercase and lowercase letters of the alphabet. The numeric characters in BASIC are the digits 0 through 9. The following special characters are recognized by BASIC: ...

  • マニュアル

    ...Attempted to output an M code from a position data address or register, but the content wasn’t within the acceptable range for M codes (000 to 999). Make sure that the M code is from 000 to 999. 0026 Interpolation rate not set (INTER ...

  • マニュアル

    ...C T T C T C I N I T N I N M T M I T M T W W H M R (SP) (SP) Note “SP” represents a space (20 Hex). Response Format @ x 101 x 100 Unit No. (BCD) Parameters R # Header code x 161 x 160 x 103 x 102 x 101 x 100 End code SV of instruction designated by command (constant) * FCS ↵ Terminator Timer/Counter Type (Command) Designate in ASCII characters the type of TC instruction for reading the constant SV. Timer Counter Number (Command) Designate in four digits (BCD) the timer/counter ...

  • マニュアル

    ... Series Serial Communications Board/Unit Operation Manual (W336), and CQM1H Series Serial Communications Board Operation Manual (W365). Example: Protocol for the Controller (E5_K read) Sequence No. 000 001 002 003 Communications sequence Read process value Read set point during ...

  • マニュアル

    ... to set initial data S and the CX-Process Monitor is normally used to set operation data O. Data classification Initial settings Type ITEM Example: PID Block S Initial setting parameter for each function block Forward/Reverse direction, ...

  • マニュアル

    ...), 3-Position ON/OFF block (Block Model 002), Indication and Setting block (Block Model 031), Indication and Operation block (Block Model 032), Ratio Setting block (Block Model x 033), Indicator block (Block Model 034), and 4-Point Warning Indicator block (Block Model 110). An ...