全 425 件が検索されました。(321 - 340件を表示)

  • マニュアル

    ...hostl/Funit. Screencontrol:Displayofaspecificscreen,inquiryabout ascreennumber,etc. Memorytableoperation:Writingdatatoamemolytable,cepyingof amemorytable,etc. Lampandtouchswitchcontrol:lnstructiontodisplaydata,inquiryabout displaystate,inputdisabledsetting,etc. Systemcontrol:BuzzerandalarmON/OFF,inquiryabout status,screendatainitialization,screen dataprinting,etc. NotificationofDatafromtheNT612GtotheHost TheNT612GtransmitsdatatothehostinthefollowingtWocases= (1)lnresponsetoaninquiryfromthehost. (2)Whendataisenteredthroughtouchswitches. ThenotificationfunctionisdifferentdependingonthetypeofthehostI/Funit,...

  • マニュアル

    ... essential. The available area required for the support tool files and data area is 2 Mbytes. 2 Preparing Equipment Section 1-1 S Using the EMS (expansion memory) The EMS must be loaded to the support tool before using it. DEVICE=EMM386....

  • マニュアル

    ...moving on to actual operations. 161 12-6-5 Settings for the Motion Controller Perform the following settings using POWER PMAC IDE. 1) From the Solution Explorer, open Global definitions. pmh. 2) In the Global definitions.pmh file, add the following line: ...

  • マニュアル

    ... bit 15 from the PLC. (Do not use the system memory for any purpose other than communicating with the PT.) Bits 10, 11, and 13 (Backlight Color) Manipulate the bits correctly from the PLC. (Do in the first word of the Bit Area in ...

  • マニュアル

    ...Communications Mode 500 m max. 6 m max. 120 m max. 93.75 kbps CompoBus/S p i i communications DIP switch Connectable node dd addresses Max. No. of Slaves d to SYS connected SYSMAC Board Communications cycle time High-speed Communications Mode (Pin 2: OFF) Long-distance Communications Mode (Pin 2: ON) Pin 1: OFF IN 0 to 7/OUT 0 to 7 16 Slave nodes 0.5 ms 4.0 ms Pin 1: ON IN 0 to 15/OUT 0 to 15 32 Slave nodes 0.8 ms 6.0 ms 17 Section Programmable Controller Functions 1-5...

  • マニュアル

    ...HR AR LR TC DM # P ABCD........DP LONG MESSAGE (@)LMSG(47) (CPU11) LMSG(47) S D ––– TERMINAL MODE (@)TERM(48) (CPU11) TERM(48) ––– ––– ––– SET SYSTEM (@)SYS(49) (CPU11) SYS(49) P ––– ––– Outputs a 32-character message to either a Programming Console, or a device connected via the RS-232C interface. The output message must be in ASCII beginning at address S. The destination of the message is designated in D: 000 specifies that the message is to be output to the GPC; 001 specifies the RS-232C interface, starting with the leftmost byte; and 002 specifies the RS-232C ...

  • マニュアル

    ...-IDS02-V1 accesses the EEPROM Data Carrier. Neither of these modes are, however, available when the ID Sensor Unit accesses the SRAM Data Carrier or when the C500-IDS21/IDS22 accesses any Data Carrier, in which case turn pin 2 OFF. Refer to the V600 FA ID ...

  • マニュアル

    ... stop operation. If SR 25211 is ON, bit status will be maintained; if SR 25211 is OFF, all bits will return to default status when operation is started or stopped. The Force Status Hold Bit is only effective when enabled with the Set System instruction (...

  • マニュアル

    ...}ns詐uct拍nI…xgc戯}onErrerFlaD,1三R A巾h舗tioO声atbnFla目s 3●3、毒OCIockPulse$ 3-3匂tlSpeciail/O持ags −P己Linki/0ETrorFiags −PCLinkR亀5ta貧F{ags ・RemoteV()EvrerFlag −sys蛭TErrorandglvnFlags −{・40stLiBki三rForl=iagS ' 一}fiostLin}文窮estartFlagS 3-4Hold拍目F{e捷yA把a−封R 3『STemperaryR剖ayArea−TR 3・6LlnkRelayArga-Lgl 3.7'Timerノ〔k:)unterArea-T(二 3-80蹴aMemoryArea」£)縫 3・9PrograrnMemOilf-VM 888890]111222345667 丁丁7778B888888888888 書ffCTS◎...

  • マニュアル

    ... extensive list of error messages, their meanings, and the appropriate responses. 00000 00000 FUN (??) 00000ERR CHK OK MEMORY ERR NO END INST I/O BUS ERR I/O SET ERR I/O UNIT OVER Fatal errors SYS FAIL FALS ...

  • マニュアル

    ...pressing ENT. The sequence in which error messages are displayed depends on the priority levels of the errors. Some errors are fatal and will cause the CPU to halt; others are non-fatal. If no errors exist or when all existing errors have been cleared, ...

  • マニュアル

    ...2・4 S◎ftwareC◎nfigurations ThefollowingillustrationshowstheSYSMACNETsonwareconfigurationfor lBMPC!ATorcompatiblecomputers.{レF=interface) Userapp翫caUons Diagnos匠cu61i取 Diagnosticservicθdriver BASlCl/F Datagramservicedriver(DGIOX) CP-32◎OBIOS SYSMACNETSupportBoard CP3200BIOS DatagramServlceDriver BASICVF DiagnOstiCServlceDriver DiagnostlCUtility TheCP_3200....

  • マニュアル

    .../O bus error I/O BUS ERR Check the number of points with I/O Table Read and use I/O Table Register to match the registered table to the actual table. Clear the error after correcting it. System error SYS...

  • マニュアル

    ... switching between PROGRAM and MONITOR mode to start or stop operation. If SR 25211 is on, bit status will be maintained; if SR 25211 is off, all bits will return to default status when operation is started or stopped. Unless the system operation instruction (...

  • マニュアル

    ...SYSMAC NET ) SYSTEM MANUAL 1 ち/ ∵/! ∴"1"2」㌧!/// 」//■._i. /・・聴蕪憲誌蒸§憲認総繕ζ∴//∵ ---------------------[End of Page 8397]--------------------- 、 ---------------------[End of Page 8398]--------------------- ---------------------[End of Page 8399]--------------------- ---------------------[End of Page 8400]--------------------- SYSMACNET ...

  • マニュアル

    ...3G2A7-LK201-・EVI 3G2A7-LK-202-EV1 o ぽパコ嬬犀';:腰噸`嬰:)i:抽11:':`:・:・1:9 のロ ココロゆ _避』…璽 o SWl SW2 SW3 2 ---------------------[End of Page 8486]--------------------- Sys彪mConプigz〃'ation Section1-2 1-2 SystemC◎nfigurati◎n ThefollowingexamplesiliustratepossibleapplicationsofHostLinkUnitsin wiredoroptlcalsystems,orboth. SomesystemswillcontainjustoneHostLinkUnitconnectedtoasinglehost computer.Thisisknownasa"single-link"system.Otherssystemsmightcon・tainseveralHostUnkUnitsconnectedtoahostcomputer.Thisconfiguration isknownasa"multiple-link"system.Althoughmostsystemswiilrequireonly onehostcomputer,ifbQthRack-mountingandCPU-mountingHostLink Unitsareusedtogether,twohostcomputerscanbeconnectedtothesame PC,independentofeachother.ThePCcanthenexecutecommandssent fromeitherhostcomputer. lnallbutthefirstconfigurationexample,LirlkAdaptersareusedtobranch betweensystemdevices,ortoconvertbetweendjfferenttypesofcables,or toperformbothofthesefunctions.ThefirstpartoftheLinkAdaptermodel rlumbers(i.e.,3G2A9→intheexampieshasbeenomitted. 1-2-1 C◎nnecti◎ns SystemcomponentscanbecomectedusingRS-232CorRS-422cables,or...

  • マニュアル

    ...offI onI onln op opt OUT pwr rak rec RET reg RM RT stat schI sel ser spec stop error sht SIO ST stan SV sys swit tbl TN trans trigg TRN UM undef WDT interrupt interrupt I/O Interface Unit ladder link monitor network offline online online operation optical output power Rack reception return register/registration Master Slave status scheduled select series specified/special stop error (fatal error) sheet Special I/O Unit step standard set value system switch table transition transition trigger transition User Program Memory undefined watchdog timer SECTION 2 Getting Started This section explains how to ...

  • マニュアル

    ...) andthePC, Select"C:Trans.prog&data"fromthemainonlinemenu.Thefollowingmenu wiiiappear, [Ttsartsfer] P:Computer(S∼♪st㎝w◇rk)一>PC C:Comp∂rePro9, G:PC->Computer(Datadisk) L:Computer(Datadisk)一>PC Operation Bbckbad PC->Computer(Systemwork) TransfersdatafromthePCtothecornputerworkdisk. Comρuter(...

  • マニュアル

    ...ー凸-↓ーユー-▲-上-ふ-上-▲-↓ーユー↓ーユ哨141■11▲-▲-ふ唱』竜五 129 ---------------------[End of Page 9159]--------------------- 4-6.Ed垣ngNetworkS叩portTables 4-6-1 4・6・2 4・6-3 SYSMACNETDataLinkTables ...

  • マニュアル

    ...卿ト{et∈]0②NodeO{2}2} DRU [FlLnction6〕 DRU [Function3】 CCCCCCCCCCCCCCC 阻`研撒商R:Debug〔=):Tra}●15fらrprogr、arfl2、dataD:E(:litDドll:E・:litl!OtableT:Datat{'aceF:'FnemanagementP:Progr、amtraceQ:SUstemsetuP自:PCsetuPZ:C{」stomlzeX:CPUBusUnitSetupr、1:NetWO「kSupporttableS:DiagnosisnetuorkB:...