全 425 件が検索されました。(381 - 400件を表示)
- マニュアル
...region 0 to 15 Area & gravity → p. 67 Gravity & axis → p. 67 Edge → p. 63 Search → p. 55 Expression Judge → p. 75 Data→ p. 75 MON (Monitor) → p. 84 RUN → p. 92 SYS (System) White balance → p. 96 Communications settings→ p. 118, 121 Output → p. 97 Backup → p. 97 Display settings → p. 100 Set key operation → p. 106 Startup mode → p. 107 Error method → p. 108 Version → p. 110 SAVE → p. 18 5 Section Features Color Filter Scene 0 SET Adjust Scene 15 → p. 16 Shutter speed → p. 24 Color filter → p. 24 Color select → p. 26 Filtering → p. 33...
- マニュアル
... properly performed under the set conditions. Judgments are displayed on the video monitor and are not output to external devices. RUN (Run) Used to read codes. The judgment is output to external devices or RS-232C via the terminal blocks. ...
- マニュアル
...6 +5 V Power supply (+5 V) 9 SG (GND) Signal ground 5V power supply V530-R150 Settings 1 Go into system mode and select multi drop. –––– –––ms System settings SET MON RUN SYS SAVE Communications Backup Image storage Startup mode Multi drop Error method Version 2 The following screen will be displayed. Set each of the displayed items. Set this to “ON.” Settings Unit number Set the unit number (00 to 31). End 3 Select End. 67 Section 4-5 Connection Examples Process Flow • Set the unit numbers for each of the V530-R150s. (In this example, the unit ...
- マニュアル
... under the set measurement conditions. The measurement results are displayed on the monitor only. The results cannot be output to external devices. RUN Performs measurement. The measurement results are output to an external device via a terminal block or RS-232C. ...
- マニュアル
... is being performed correctly under the set inspection conditions. The measurement results are displayed on the monitor only. The results cannot be output to external devices. RUN Performs inspection. The measurement results are output to an external device via a parallel interface. ...
- マニュアル
... section explains how to set the communications specifications. Set the same communications specifications in the F160 and the external device. 1. Move the cursor to MON or RUN and press the ENT Key. 0.Scn 0 MON SET MON RUN ...
- マニュアル
...Edge position P.126 Gray search P.141 Labeling P.155 Rotation search P.173 *2 Same as 1st region. P.225 17 Section 1-5 Menus MON P.58 RUN P.61 SYS Camera settings P.284 Communications Serial Refer to Communications Reference Manual. Normal Host Link Parallel Output P.286 Serial P.287 Memory card P.288 Display settings P.290 Monitor P.297 Designate colors P.298 Make colors P.299 Operation settings Set key operation P.301 Measurement control P.310 Display capture P.304 Display Switch menu P.319 Setting menu masking P.306 Startup ...
- マニュアル
...Move the Up, Down, Left and Right Keys to the desired setting. Mode (*1) Mode Description SET (Set) Used to set reading conditions. RUN (Run) Used to read codes. The judgment is output to external devices through RS-232C. ...
- マニュアル
... the scene. → page 219 Using 2 Cameras If an F150-A20 Two-camera Unit is used, two Cameras can be connected to one V530-R150. → page 26 Note 6 1. Change the Camera Unit to “F150-A20” in advance in the ...
- マニュアル
..., it is recommended that settings are backed up to a computer. Selection Description Scene Saves or loads the settings under Set in scene units. System Saves or loads the settings (except the settings of Slant correct) under System in scene units. ...
- マニュアル
... at the same time. For details on using different models, refer to page 146 in the Operation Manual. Section 2-2 System Configuration CHECK When Using the Z300-S60 - When using the Extension Cable, set the length of the Extension Cable in ...
- マニュアル
...with the current screen are displayed with their respective functions. "S" refers to the SHIFT Key. "S + ENT" indicates that the ENT Key should be pressed while the SHIFT Key is pressed. Mode(*) Display SET RUN VIEW TOOL ...
- マニュアル
... of monitoring p.120 Warning transition p.125 Store data to MemCard p.126 TrendMon settings QRCode Pattern registration The menu hierarchy is the same as for DataMatrix. INTRODUCTION INTRODUCTION p.71 RUN p.71 ...
- マニュアル
... is being performed correctly under the set inspection conditions. The measurement results are displayed on the monitor only. The results cannot be output to external devices. RUN Performs inspection. The measurement results are output to an external device via a parallel interface. ...
- マニュアル
... section explains how to set the communications specifications. Set the same communications specifications in the F160 and the external device. 1. Move the cursor to MON or RUN and press the ENT Key. 0.Scn 0 MON SET MON RUN ...
- マニュアル
...Rotation search P. 180 *2 Same as 1st region. P. 233 17 Z173-E1-02A.book Page 18 Monday, June 5, 2006 6:49 PM Section 1-5 Menus MON P. 60 RUN P. 63 SYS Camera settings P. 293 Communications Serial Refer to Communications Reference Manual. Normal Host Link Parallel Output P. 294 Serial P. 295 Memory card P. 296 Display settings P. 298 Monitor P. 305 Designate colors P. 306 Make colors P. 307 Operation settings Set key operation P. 309 Measurement control P. 318 Display capture P. 312 Display Switch menu P. 327 Setting menu masking P....
- マニュアル
...The selections for scenes appear. 8. Select the scene whose data is to be saved in the PC. Select [Scn0] in this example. 166 Operation Manual Scn 0䂯 Tools䂯 Test Surrounding image Backup Scene System ...
- マニュアル
...When an error occurs, Displays 1 and 2 show error messages. Refer to the following table to check the meaning of the message and how to solve the problem. Display 2 unit err Unit error unit chg Unit change disp ...
- マニュアル
... for scenes appear. 8. Select the scene whose data is to be saved in the PC. Select [Scn0] in this example. 168 Z550 Operation Manual Scn 0䂯 Tools䂯 Test Surrounding image Backup Scene System Sys+scn Scn 0䂯 Tools䂯 Test Surrounding image Back up Scene Z550㫋㫆㩷PC System PC㩷㫋㫆㩷Z550 ...
- マニュアル
..."FF" "00" 1 0 7 6 16 15 14 13 0/1 0/1 0/1 0/1 "FF" "00" 1 0 7 6 2 1 0 8 7 6 5 1 Sys Sys 0/1 0/1 0/1 0/1 0/1 0∗ 0∗ "FF" "00" "FC" ∗ These bits data are preassigned for the system. Be sure to set them to 0. A 1-setting will trigger an error (error code: "14"). ■ Response frame structure The response code (normal completion "00") and data read are returned. The read data blocks are returned in the order of designated ...