全 425 件が検索されました。(401 - 420件を表示)
- マニュアル
... the settings, back them up to a personal computer before performing initialization. Switch to the FUN mode. The top screen is displayed. FUN 2 Select [System]. 3 Select [INIT]. 4 Move to [YES] and press the SET MEAS ...
- マニュアル
... (*** is a running number starting from 000.) • Individual save: Any file name The file extension differs according to the file type, color or black-and-white. • Color image: .BYR • Black-and-white image: .GRY System data [SYSTEM] Directory for storing system data ***....
- マニュアル
... Commands ZFX-C Serial Communication Command Reference Uploading System Data < SYSLOAD command > Uploading system data to the Controller from an external device This command uploads the system data to the Controller by XMODEM protocol. No parameters are provided for this command. < Command format > ...
- マニュアル
... the file type, color or black-and-white. • Color image: .BYR • Black-and-white image: .GRY Logging data [LOG] Directory for storing logged results ***.CSV (Any file name within 8 characters) System data [SYSTEM] Directory for storing system data ***....
- マニュアル
... Commands ZFX-C Serial Communication Command Reference Uploading System Data < SYSLOAD command > Uploading system data to the Controller from an external device This command uploads the system data to the Controller by XMODEM protocol. No parameters are provided for this command. < Command format > ...
- マニュアル
... installation finishes. Wave Inspire RX Software Manual Connect the main unit to the PC using the USB cable, turn the power on, and display the [Device Manager] window. 7 In the window displayed, select the [Driver] tab and click the [Driver Details]. Select "......\GTCUSBR....
- マニュアル
...199 10-4 Updating the Software The most recent version of the software and PC Tool can be downloaded from the following website for OMRON members. Refer to the Member Registration Sheet that is enclosed with the Sensor. http://www.omron-cxone.com/vision_...
- マニュアル
... to result measureme Previous nt result value CLAMP "------" Output at clamp level Measured value not applied LED OFF FUN Display according to menu System error "SYS.ERR" blinks Voltage: 0 V output Current: 12 mA output When starting "INIT" Output at clamp level (approx. 10.8 V) LED OFF Output Enabled according to the mode (Measureme nt result/ Judgment result) Output OFF Output of the measured value: clamp level Judgment output: Output OFF Enabled Enabled Disabled Disabled Disabled Output OFF RS-232C/ Ethernet Zero reset Enabled Commands are accepted but not executed. Invalid (Note)...
- マニュアル
...The selections appear. 5. Select [Backup]. The selections appear. The selections appear. The selections for scenes appear. 8. Select the scene whose data is to be saved in the PC. Select [Scn0] in this example. Scene System ...
- マニュアル
...Output at clamp level Output OFF Measurement KEEP Previous value error CLAMP "------" Measured value not applied LED OFF FUN Display according to menu System error "SYS.ERR" blinks Voltage: 0 V output Current: 12 mA output When starting "INIT" Output at clamp level (approx. -10.8 V) Enabled Disabled Disabled Disabled Enabled Commands are accepted but not executed. Invalid (Note) Note: Do not obtain data during start-up. The RS-232C output is indeterminate at this time. 372 Specifications and External Dimensions ZW User's Manual External Dimensions ZW-CE10T/CE15T ROM mounting screw hole...
- マニュアル
... on the marking/processing to be executed. XXX Block data • Text • ID code • Straight line XXX Marking Data Block Setting • Form • Position • Fill Common Setting • Marking control • Layer • Laser power/Scan condition ...
- マニュアル
... on the marking/processing to be executed. XXX Block data • Text • ID code • Straight line XXX Marking Data Block Setting • Form • Position • Fill Common Setting • Marking control • Layer • Laser power/Scan condition ...
...加で読み出す /* チップセレクトが 10 ナノ秒ローレベルになったあとローレベルになる読み出しラインの遅延 /***********************************************************************************************/ Sys...
...DesiredPwmFreqkHz = 200 ; // kHz DesiredPwmDutyCycle = 10; // Percent DesiredPwmDelayUnit = 998; // 10 usec DesiredPwmDelay = 57; // 600 usec First84PwmMPeriod = rint( 1E5 / (16 * DesiredPwmFreqkHz) ); First84PwmDutyCycle = rint( DesiredPwmDutyCycle / 100 * 4096 ); First84PwmDelay = rint(DesiredPwmDelay * 1E3); // Logic for checking the completion of desired PWM pulses First84PwmPulseCount = 5 p0=...
...Turbo PMAC のグローバル I 変数には、100 より小さい番号が付いています。 Power PMAC でこれらに多く該当するのは、データ構造体[Sys]や、ほかの非モータや非座標系データ構造体における要素です。 サイクルタイムパラメータ • 位相サイクルの同じ拡張...
...され、[Watch]ウィンドウの応答の領域に残り、再度送信されません。 オンラインコマンドの非省略形での入力を強制する、[Sys.NoShortCmds]という名前の構造体に注意してください。 [Sys.NoShortCmds=0]の場合、#1kなどのコマンドを使用してモータ1を出力停止させる...
...時に、Power PMAC はシステム内にあるすべての ACC-24E3 ボードを自動的に検知します。 16 ビットのグローバルステータス要素 Sys.Gate3AutoDetect は、Gate3[i]に対応するアクセサリが検知された場合に、ビット i を 1 に設定します。 このステータス要素は、 DSPGATE3 ベースの...
...す。 Turbo PMAC オープンメモリレジスタ(24 ビット)、$10F0-$10FF(X と Y) Power PMAC オープンメモリレジスタ(32 ビット)、符号なし Sys.Udata[i] Sys.Udata[1]、Sys.Udata[2]、Sys.Udata[3]…を使用ユーザがオープンメモリのシングルビットの書き込み/ 読み取りを実行 PLC がオープンメモ...
...]フォルダの.cfg ファイルに保存することもできます。 // ACC-59E3 Initialization File // For Card 0 (Power PMAC I/O Base Address Offset=$900000) // Requires firmware 1.2.1.158 or newer. Sys.WpKey=$AAAAAAAA; Acc59E3[0].DacStrobe=$FFFF0000; // Up to 16-bit DACs (works for 12-bit as well) Acc59E3[0].GpioDir[0]=$FFFFFFFF; // All GPIO is output Acc59E3[0].GpioPol[0]=0; // Non-inverting IO Acc59E3[0].GpioData[0]=0; // All input filters set to 24.5 kHz cutoff freq. Acc59E3[0].Chan[0]....
..., 1ライセンス版 SYSMAC-BA201L Sysmac Studio ネットワークライセンス, ベーシックライセンス, 64bit版, 1ライセンス版 もっと見る SYSを含む形式 全26件 形式仕様一覧 Sysmac Library コントローラ NJ/NX/NY用ソフトウェア機能部品集。Sysmac Studioにインストールして、プログラ...