全 414 件が検索されました。(321 - 340件を表示)
- マニュアル
... them to the SYSMAC-CPT, an error will occur. Timer Instructions TTIM Serial Communications Instructions PMCR and STUP Network Communications Instructions SEND, RECV, and CMND Floating-point Instructions FIX, FIXL, FLT, FLTL, +F, –F, *F, /F, DEG, RAD, SIN, ...
- マニュアル
... T1 Optical Fiber Twist-relief Cable device Pull line Winch The pulling tension (T) on the cable can be calculated from the tension reading (T1) at the pulley and the angle (θ) at the pulley. T= T1 θ 2 ...
- マニュアル
... is either in BIN 16 bit or BIN 32 bit. 180 Section 7-14 Improved Instructions In 32 Bit [D]: Calculation result (rightmost 4 digits) [D+1]: Calculation result (leftmost 4 digits) In 16 Bit [D]: Calculation result (4 digits) SIN/...
- マニュアル
... commands through serial connection Inter-network communications Other funcRemote programtions ming/monitoring Configurator operations through serial connection Memory Card backup function Master Unit error log function Communications cycle time setting Message monitoring timer ...
- マニュアル
... DM Area words. Specifications Section 1-3 Item Supported connections (communications) Remote I/O Slave allocation method master communications Fixed allocations User-set allocations Specifications • Remote I/O communications (master and slave): Master/slave connection (poll, bit-strobe, ...
- マニュアル
... nodes capable of simultaneous communications as explicit servers Data length for explicit messages Response monitoring time for explicit messages (for clients) Retries for explicit messages Note Minimum System Requirements Specifications • Bit Strobe • Polling • Cyclic • Change of State (...
- マニュアル
...SINE SIN/ @SIN 460 Calculates the sine of a 32-bit floating-point number (in radians) and places the result in the specified result words. OK OK OK OK OK OK OK OK COSINE COS/ @COS 461 Calculates the cosine of a 32-bit floating-point number (in radians) and places the result in the specified result words. OK OK OK OK OK OK OK OK TANGENT TAN/ @TAN 462 Calculates the tangent of a 32-bit floating-point number (in radians) and places the result in the specified result words. OK OK OK OK OK OK OK OK FloatingFLOATING ...
- マニュアル
...2nd Term 3rd Term AND (Logical AND) & #MW- = #MW- 1st Term & #MW-; 2nd Term 3rd Term Functions NOT (Reverse) ! Absolute value ABS Sine SIN Cosine Tangent ARC Sine COS TAN ASIN ARC Cosine ACOS ARC Tangent ATAN Square root SQR Normal logarithm EXP Natural logarithm LOG Decimal point Variable R/W B W L F @ --- No No Write Yes Yes Yes No No LONGMINLONGMAX Yes Integer Read Yes Yes Yes No Yes LONGMINLONGMAX Yes Integer Read Yes Yes Yes No Yes --- No No Write No Yes Yes No No LONGMINLONGMAX Yes Integer Read No Yes Yes No Yes LONGMINLONGMAX Yes...
- マニュアル
...--- S: 1st source word R: 1st result word REAL REAL ----- S: 1st source word R: 1st result word REAL REAL ----- S: 1st source word R: 1st result word REAL REAL ----- R COSINE COS @COS 461 COS S R TANGENT TAN @TAN 462 TAN S R ARC SINE ASIN @ASIN 463 ASIN S R ARC COSINE ACOS @ACOS 464 ACOS S S: 1st source word REAL --- R: 1st result word REAL --- S: 1st source word REAL --- R: 1st result word REAL --- S: 1st source word R: 1st result word REAL REAL ----- S: 1st source word R: 1st result word REAL...
- マニュアル
...code 0372h 200Eh 200Eh The following operand has exceeded the range. • Q (MOVEC, MOVETRAV, MOVELINK, CAMBOX) 0379h Correct the applicable operands. 200Fh 200Fh The following operands have exceeded the range. • K (CAM, CAMBOX) • B (MOVELINK, CAMBOX, CONNECT, SYNC, ADDAX) • TORQUE • SIN, ...
- マニュアル
... or 08) node 63, words m+43 to m+74) Slave Verification Error Flag (bit See note 2. 01 or 09) Slave Configuration Error Flag (bit 02 or 10) Slave Remote I/O Communications Error Flag (bit 03 or 11) Master Function ...
- マニュアル
... and select Parameter – Edit – General, and then select the Smart Slave to be set. Node Address Settings and I/O Allocation Section 2-2 2. Click the Advanced Setup Button, click the Connection Tab, and select User Setup. Select Use Poll Connection and Use ...
- マニュアル
...The Setting Tool can be used to allocate the peak value, bottom value, top value, valley value, rate of change, comparator results, Status Flags, etc. Node address setting No setting required. Baud rate setting No setting required. 156 Poll, Bitstrobe, and ...
- マニュアル
... 2-2 Command List Operation Common function Name Description ABS Assigns absolute value to the result of expression AND ANDs two expressions ASC Converts specified character to character code CHR$ Converts specified character code to character ...
- マニュアル
...ATN Item Contents Function Determines arctangent. Format ATN (
) Example A!=ATN(0.5) Description Determines the arctangent in radians of . The value provided is between –π/2 and π/2. Comments ––– Reference ... - マニュアル
... display mode. Text display control Command 68 Section 1-1 OVL Alphabetical List Command/Function C D Operation Instruction Type Page CONT Continues execution of a program. Program execution control Command 68 ...
- マニュアル
...STOP command. Operations such as printing the variable names in the direct mode are possible while the program is stopped. However, a program cannot be continued if it was modified while execution was stopped. 76 Section 5 CURSOR . . Reference ...
- マニュアル
...Refer to page 215 for the list of setting items. 5. Select the item to be set. (Here, Measurement is selected as an example.) Variable0 Position Measurement Variable Data Judge Constant ← ABS SIN AND MOD ...
- マニュアル
...Remote I/O communications two-word mode Remote I/O communications two-word mode with incident light level monitoring Cannot be set. --- The DeviceNet Configurator can be used to set the connection type. The Fiber Amplifier Sensor Communication Unit supports bit-strobe, polling, ...
- マニュアル
...Refer to page 223 for the list of setting items. 5. Select the item to be set. (Here, Measurement is selected as an example.) Variable0 Position Measurement Variable Data Judge Constant ← AND ABS SIN MOD ...