全 414 件が検索されました。(301 - 320件を表示)

  • マニュアル

    ...(0°≤Θ≤ 90°). Description When the execution condition is OFF, VCAL(69) is not executed. When the execution condition is ON, the operation of VCAL(69) depends on the control word C. If C is #0000 or #0001, VCAL(69) computes sin(x) or ...

  • マニュアル

    ... closed and stops when contacts are opened) Input Voltage: 24 mA 24 VDC Control Output Signal RUN INPUT (Contacts are closed while PC is in RUN mode) Max. switching capacity: 2 A 250 VAC (resistive load) 0.5 A 250 VAC (inductive load, ...

  • マニュアル

    ... closed and stops when contacts are opened) Input Voltage: 24 mA 24 VDC Control Output Signal RUN INPUT (Contacts are closed while PC is in RUN mode) Max. switching capacity: 2 A 250 VAC (resistive load) 0.5 A 250 VAC (inductive load, ...

  • マニュアル

    .../3) Purpose: To round off a numeric value at the decimal point and convert it into an integer Format: CINT() Example: A = CINT(B#) Purpose: To return the cosine of the numeric value given by the argument Format: ...

  • マニュアル

    ... both the X and Y axes. The velocity component for each axis is illustrated below. Y axis Interpolation end point ν ν νx νy νy θ Origin νx νy νx X axis ν cos θ = ν sin θ = : Interpolation speed : X-axis speed : Y-axis speed Also refer to the programming examples in Section 9. 87 Section 4-1 Setting Up Data Memories Cautions for Using Completion Code 2: Continuous 1. Stepping Motor Avoid using continuous completion, code 2, with the stepping motor. During interpolation, pulses are output in accordance with the speed changes set for the interpolation and ...

  • マニュアル

    ...8 pts/com 2 circuits When using the High-speed Counter, the 2 pts per – common circuit is used for the High-speed Counter input and Hardware Reset on the CPU. Maximum switching capacity – Resistance load 250 VAC/ 2 A(...

  • マニュアル

    .../3) Purpose: To round off a numeric value at the decimal point and convert it into an integer Format: CINT() Example: A = CINT(B#) Purpose: To return the cosine of the numeric value given by the argument Format: ...

  • マニュアル

    ... value ACOS Gives arc cosine ASC Gives character code ASIN Gives arc sine ATN Gives arc tangent CDBL Converts integer value or single-precision value into double-precision value CINT Converts real-number value into integer value ...

  • マニュアル

    ...'0η} Calculatesthearctangentofthe,θ)¢)「θss'oη・ 32 CDBL .CDBL(θXρreSS'0η) Convertsθxρ佗ssた)nintoadouble-precisionrealnumber 33 CHRS CHRS(θκρrθSSわη} Convertsθxρ佗ssわηintocharacters. 34 CINT ,CINT(θXρrθSS氾η) Roundsanyfractionalpartofθ)ψr●ssわη 35 ...

  • マニュアル

    ... ≤ 0900 (0°≤Θ≤ 90°). Description When the execution condition is OFF, VCAL(69) is not executed. When the execution condition is ON, the operation of VCAL(69) depends on the control word C. If C is #0000 or #0001, VCAL(69) computes sin(x) or ...

  • マニュアル

    ...-POINT SUBTRACT 456 *F(j)* FLOATING-POINT MULTIPLY 457 /F(j)* FLOATING-POINT DIVIDE 458 RAD(j)* DEGREES-TO-RADIANS 459 DEG(j)* RADIANS-TO-DEGREES 460 SIN(j)* SINE 461 COS(j)* COSINE 462 TAN(j)* TANGENT 463 ASIN(j)* SINE-TO-ANGLE 464 ACOS(j)* COSINE-TO-ANGLE 465 ATAN(j)* TANGENT-TO-ANGLE 466 SQRT(j)* SQUARE ROOT 467 EXP(j)* EXPONENT 468 LOG(j)* LOGARITHM Note Instructions with one asterisk (*) are supported by the CVM1D and version-2 CVM1 CPU Units only. 152 Instructions with two asterisks (**) are supported by the CV500, CV1000, and CV2000 ...

  • マニュアル

    ...ALM ADJ Connector for resolver Insert the connector so that the cable will be pointing downward. Connector Pin Wiring Cam Positioner Unit 1 2 3 4 5 6 7 8 Sin(+) Sin(−) Cos(+) Cos(−) OUT(+) OUT(−) ----Connector case Resolver Sin(+) Sin(−) FG ...

  • マニュアル

    ... DM 6655 cannot be used for D. Description When the execution condition is OFF, APR(––) is not executed. When the execution condition is ON, the operation of APR(––) depends on the control word C. If C is #0000 or #0001, APR(––) computes sin(θ) or ...

  • マニュアル

    ... to 0900 (0°≤ q ≤ 90°). Description When the execution condition is OFF, APR(69) is not executed. When the execution condition is ON, the operation of APR(69) depends on the control word C. If C is #0000 or #0001, APR(69) computes sin(q) or ...

  • マニュアル

    ... output Screw (3.5 mm head with self-raising pressure plate) RUN Output These terminals are short-circuited during PC operation. Use them to receive PC RUN signals, for purposes such as emergency stop circuits. Maximum switching capacity: 250 VAC, 2 A (...

  • マニュアル

    ... for LRC (longitudinal parity), CRC-CCITT (XMODEM), CRC-16 (MODBUS), and SUM (1-byte or 2-byte). This allows you to eliminate the programming previously required to calculate error check codes. Special Operations Calculations are possible for exponential function (ex), square root (√), trigonometric functions (TAN, SIN, and ...

  • マニュアル

    ...switching capacity 2 A, 250 VAC (cosφ = 1) 2 A, 24 VDC (4 A/common) Min. switching capacity 10 mA, 5 VDC Service life of relay Electrical: 150,000 operations (resistive load, 24 VDC) 100,000 operations (inductive load, 220 VAC, ...

  • マニュアル

    ...be necessary to directly input settings such as the connection type and data size. (Always select the connection type that is supported by the Slave.) The following connection types are allowed in DeviceNet communications. Connection type poll bit strobe change of state (...

  • マニュアル

    ...or MONITOR mode. These terminals can thus be wired to provide an external signal indicating the operating status of the PC, such as is used in the emergency stop circuit shown in 3-6-1 Emergency Stop Circuit. Maximum switching capacity: 250 VAC/2 A (...

  • マニュアル

    .... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5-21-12 COSINE: COS(461) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5-21-13 TANGENT: TAN(462) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 216 219 222 224 225 226 227 230 232 234 236 237 238 238 238 239 241 242 243 244 245 246 249 249 250 252 253 254 255 256 257 259 259 261 263 268 272 274 276 278 280 283 284 285 285 286 287 288 289 290 291 292 293 294 97 5-22 5-23 5-24 5-25 5-26 5-27 5-28 98 5-21-14 SINE TO ANGLE: ASIN(463) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5-21-15 COSINE TO ANGLE: ACOS(464) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5-...