全 5560 件が検索されました。(2961 - 2980件を表示)

  • マニュアル

    ...°C/−199.9 to 900.0°F) Pt (0.0 to 100.0°C/0.0 to 210.0°F) JPt (−199.9 to 500.0°C/−199.9 to 900.0°F) JPt (0.0 to 100.0°C/0.0 to 210.0°F) K (−200 to 1300°C/−300 to 2300°F) K (−20.0 to 500.0°C/0.0 to 900.0°F) J (−100 to 850°C/−100 to 1500°F) J (−20.0 to 400.0°C/0.0 to 750.0°F) T (−200 to 400°C/−300 to 700°F)...

  • マニュアル

    ... symbols displayed on the displays and alphabet characters. a A b B c C d D e E f F g G h H i I j J k K l L m M n N o O p P q Q r R s S t T u U V w x V W X y Y z Z xi About this Manual: Purpose ● Overview ● Setup ● Basic Operations ● Operations for Applications ● Appendices xii Relevant section Details Section 1 introduces the features, components, and main specifications of the E5CSV/E5CS-U Digital Temperature Controllers. Section 2 describes the work...

  • マニュアル

    ...-less clamp terminals Advanced Unit Gradient Temperature Control 1 2 3 4 5 6 7 8 9 10 11 12 13 14 E J 1 G - H F U A - N F L K E J 1 G - H F U A - N F L 2 E J 1 G - H F U B - N F L K E J 1 G - H F U B - N F L 2 6 8 EDU Communications FLK Outputs Terminal type Unit name Type N A EDU C CompoWay/F 2 transistor outputs Screw terminals End Unit Common model 1 2 E ...

  • マニュアル

    ... panel mounting depth have not been changed. z E5GN Model numbers have changed accompanying the introduction of universal input capability. The default setting of the input type parameter of the E5GN-………P (models with resistance thermometers) has been changed from a Pt100 resistance thermometer to a ...

  • マニュアル

    ... 100.0°C/0.0 to 210.0°F) H'00000003 (3): JPt (−199.9 to 500.0°C/−199.9 to 900.0°F) H'00000004 (4): JPt (0.0 to 100.0°C/0.0 to 210.0°F) H'00000005 (5): K (−200 to 1300°C/−300 to 2300°F) H'00000006 (6): ...

  • マニュアル

    ... are as follows: • 15 Detection wire (red) 16 Resistance wire (white) 17 Signal wire (black) External Reset External event resets are enabled by connecting terminals 12 and 13. Do not connect a load. 6 VDC 4.7 ...

  • マニュアル

    ... for FAQs: E5@N Setting the Sensor Type Select and set the sensor type (i.e., the Input Type parameter) to the set value that corresponds to the type of sensor used in the application and the required temperature range. The parameter is set to 5 (...

  • マニュアル

    ... becomes the minimum scaling unit. xvii How to Read Display Symbols The following tables show the correspondence between the symbols displayed on the displays and alphabet characters. The default is for 11-segment displays. a b c d e f g h i j ...

  • マニュアル

    ...°C/−199.9 to 900.0°F) Pt (0.0 to 100.0°C/0.0 to 210.0°F) JPt (−199.9 to 500.0°C/−199.9 to 900.0°F) JPt (0.0 to 100.0°C/0.0 to 210.0°F) K (−200.0 to 1300.0°C/−300.0 to 2300.0°F) K (−20.0 to 500.0°C/0.0 to 900.0°F) J (−100.0 to 850.0°C/−100.0 to 1500.0°F) J (−20.0 to 400.0°C/0.0 to 750.0°F) T (−...

  • マニュアル

    ... to 0.01 m. ● Notation Used for Settings Letters, numbers, and abbreviations in settings that appear on the E5AR-T/ER-T display are as follows: a b c d e f g h i j k l m A B C D E F G H I J K L M n o p q r s t u v w x y z N O P Q R S T U V W X Y Z 0 1 2 3 4 5 6 7 8 9 -1 0 1 2 3 4 5 6 7 8 9 -...

  • マニュアル

    ...●mヒ 「Time・limitoper8tion/$elfイesetting Tme・limitoper8tlon/self・re$ettlng 1Time呼lim▲t碑r8t`on1研{㏄tricro$etti㎎⑱ 」 . int●rw●lconn●ction 'SεP8ratemotorandclutchconn㏄tion ParalIelmOtorawdclutchconnection ∼Sep8ratemotor酎†dclutchco巨n●ctlOn Termin白lform . 11弔inround5㏄...

  • マニュアル

    ...達lrl 形式名 定格入力電圧取付方法接点構成制御出力 H2ドo闘 ACm←2姻・埋込欺付 1a A口50Vl5A{抵散荷) H雄DMC k 一田FDMF ・表面取w・n恨レー碗甘 1a −H2FDMFC lc ご使用]に際してのお願い次に示†ような条件や環境で使用†る,"{Xi、定格L 機能に対して余裕を...

  • マニュアル

    ... holes 35 Reset input Start input Gate input Check input Reset input Start input Gate input Check input C M Y CM MY CY CMY K parallel possible distance. t-a Reset input Start input Gate input Check input 電源 C M Y CM MY CY CMY ...

  • マニュアル

    ...P 5 (DOWN) D (UP)  Reset Q Control output  UP operation Reset Set value Digital display 0 Set value Digital display 0 Reset 3 (DOWN) B (UP) K Control output Control output Control output R  Set value Digital display 0 Set value Digital display 0 Reset C Reset Operation SW position Mode Control output  Reset DOWN operation Set value Digital display 0 Control output Reset, gate Power reset 0.5 sec reset time (min.) (except –M type with memory backup) 0.02 sec reset signal width (min.) *Contact and transistor signal input use common terminal. External ...

  • マニュアル

    ...㢨⭬ 䏬㠼G䇴㢨⭬ ⯜⒬Go\jTs_lVTs_lk 6WHS ⯜⏼䉤ᵆG䖐㐐⬀G䚔G㄄G㉘㥉㡴G ⺼ᴴ⏙䚝⏼␘UGÝXWWW ÝXWWWG ] ஂஇஃஂஅஃ ÝXWWW 㨪 \ ⯜⒬Go\jTs_k㢌Gྙஇྚ␜㣄⏈G⇨⺴㜄G 㥅㋁╌㛨G㢼㏩⏼␘U 㨪 [ Z 9 䏭ὤ㇠䚡 இ இ o\jTs_ḻ㡴GBGCG FG[⬀G㉔䈑Gᴴ⏙ 㻐⥙㐐ᴸGWUWW㢰G⚀G䖐㐐⏈GIPME ⦐G╝⏼␘UG␜㠸ஔG㸼㻐⥙G⯜☐ᴴGB‫ޔ‬ B‫ޔ‬ B‫ޔ‬B‫ޔ‬ C‫ޔ‬...

  • マニュアル

    ...0 Digital display UP Counter 1 m 1 2 m The timing chart left hand shows the output of single preset counter, or the 2nd output of double preset counter. One-shot time (t) in C, R, K, P, and Q mode can be adjusted for between 0.1~1s by the “TIME” adjuster on the face of the counter. As shown in the table below, Double preset counter the 1st output SW2 of double No. 2nd Output 1st Output preset counter N 0 has two output F 1 modes (SelfC 2 holding output R 3 and One-shot ...

  • マニュアル

    ....1) n–1 n–2 2 3 0(n.n–1) n–2 n–3 Count up 0 0 1 n 2 n–1 n–2 F 2 C 3 R 4 K 5 P 6 Q 7 N 8 N 9 F A C B R C K D P E Q F N t n+1 0 999999 0 1 n n–1 ON OFF SW4-1 H→L at count up SW4-1 L→H at count up SW4-2 or SW4-1 H→L at count up SW4-2 or SW4-1 Constant read SW4-...

  • マニュアル

    ... an example of using a contact. In case of counting with a contact, use 30 Hz (-L) type. The use of 5 kHz (-H) type may cause the product to count bounces (chatters) generated by switching over the contact. SW2: 3 or B ...

  • マニュアル

    ... main body. Reset SAFETY PRECAUTIONS Keys to Warning Symbols 8 9 10 4 5 0V Terminals 1 and 6 are connected internally. Sensor OFF F ON C ON ON K-1 ON OFF 1 2 3 4 5 6 7 8 DIP switch Parameters that cannot be set with the DIP switch are set with the operation keys on the front panel. Note: Refer to the datasheet (Cat. No. M079) for detailed parameter settings. Change from RUN Mode to Function Setting Mode. MODE 3 s min. The characters displayed in reverse video are the default settings. When performing settings ...

  • マニュアル

    ...Up Keys 1 to 6 5 1st digit ● Change from RUN Mode to Function Setting Mode. Internal circuit Function setting mode Count Function setting mode Set value up, down --- outm Output mode n, f, c, r, k-1, p, q, aK*1 --- otim Output time 0.01 to 0.50 to 99.99 cnts iflt dp Counting speed 30hz, 5khzK*1 Reset input signal width 20ms, 1msK*1 Decimal point position ------, -----.-, ----.--, ---.--- *1 Prescale value 0.001 to 1.000 to 99.999 Set value upper limit 1 to 999999 Key protect level kp-1, kp-2, kp-3, kp-4,...