全 425 件が検索されました。(221 - 240件を表示)

  • マニュアル

    ...SP Time ON OFF ON OFF X AT ends AT starts SP Present Deviation < 10% FS Limit cycle value Change in manipulation value of 40% Set value X SP disp sys err err eep err Display unit error Repair is necessary. Main unit error Contact your dealer or our service office. Press the key in this state for at least 5 s. to return Non-volatile memory error to the factory settings. s.err Normal display [[[[[ Normal Outside display This is not an error, however, the present value is display range (below) outside of the display range (-19999 to 99999)....

  • マニュアル

    ...c嚇rol oぷput2.Youcanchoosebetwee臓relayo雛p誕,SSRoutp斑,voぬge ⑪utputandc囎eittoutputfore紬◎f伽s慨rminaisdepe城ngenthetyp¢ ◎foutputunitins投銀ed◎n血emainunit. ・桓positio汗p鱒po由onalcon愉旦sys給ms,c◎ntr◎10砿p蹴1isusedf但open outputandconM)leutput2isusedfOrclosedoutput.S《》,arelayoutputunit isusedastheeutputunit.Th▲so誕p螂磁i路1readyi轍a夏蔓¢di坤o頭oni}r◎por目.◎na}controllersbefb'reshipmentffomthe・fact《)ry,sotheuserzzeed ftottoebtainaseparatee"tp"t田虫 OTran$teer◎戒師 (...

  • マニュアル

    ...-3). 10.2 Error Messages 10.2 Error Messages When an error occurs, Displays No. 1 and 2 show error messages. Refer to the following table to check the meaning of the message and troubleshoot the problem. unit unit disp ...

  • マニュアル

    ...ThisisRot inlendedtobθanexhaustjvelistetaNpossibleusesofth白prうoducts,norlsitintendedtoImp}ythattheuses listedmaybesultableforthgprodUcts: ●Outdoo「use,usgsirlolvingpote「〕tialchemicalco「itaminatlonore!e{)tri{}allntθrf白「ence,orconditionso【 u5esnotdescrib日dlnthismamLa1. ・NUCIearenergyCentre!SyStemSgCOmbUS脆nSyStemS,「副lrOadSyStemS,aViatiOnSyStemSlmed沁al eqvipment,amusementmaChines,vehiclgs,safe1yeqU;pment,an曲stalrations$ubieCttoseparate industryergoveramentregulations. ・...

  • マニュアル

    ... connect to the SmartController EX. The figure includes the optional T20 Pendant, SmartVision MX, and SmartController EX. These items may not be present in your system. W SmartVision MX 4 HDD COM1 LAN1 USB DVI LAN2 USB ...

  • マニュアル

    ...16 16 16 17 17 18 18 18 19 19 19 19 20 20 20 Table of Contents Chapter 4: Connectors and Indicators 4.1 Front Controls and Indicators Power Switch SYS LED HDD LED MAINT Ethernet Port MGMT Ethernet Port FLEET PORTS PRIMARY WHEN LIT LED KEY Port 4.2 Rear Controls and Indicators AC Power In AC Power Switch Factory Field Service Ports 21 21 21 21 21 21 22 22 22 22 22 22 23 23 4.3 Connecting to a Network 23 Network Ports and Protocols 23 Chapter 5: Configuration 5.1 Overview 27 27 Ethernet ...

  • マニュアル

    ... Manager 2100 User’s Guide 37 4.2 Rear Panel Connectors and Features Callout Label Port Description If you press and hold the power switch for longer than 4 seconds it causes an immediate software halt (a hard stop). 4 ...

  • マニュアル

    ...functions of the EM2100. See Turn EM2100 Power ON and OFF on page 35 for more 20569-000 Rev. D EM2100 Installation Guide 15 3.2 Rear Panel Connectors and Features Callout Label Port Description information. 4 ...

  • マニュアル

    ..._to_queue(conn, inbound_queue, message): ch = conn.channel() assert ch.is_open ch.basic_publish(exchange='', routing_key=inbound_queue, body=message) #nameless ('') exchange should be used. print(" [x] published message %r to queue %r" % (message, inbound_queue)) if __name__ == '__main__': import ...

  • マニュアル

    ...automatically enabled whenever robot high power is turned ON. If the robot timing specifications in the system configuration is non-zero, enabling high power is a two-step process. In this case, after enabling high power from the T20 Pendant, Monitor Window, or software, the ...

  • マニュアル

    ... of robot not possible A program has attempted to perform a straight-line motion with a robot that does not support such motions. 187 IE_ HSTOVRE -636 overrun detec- One of these ted by host sys- three conditions has occurred: tem The time for a new trajectory point has arrived, but the internal trajectory task has not finished computing the previous point. The servos did not receive trajectory data at the expected time because the trajectory task took too long to compute and write out the data Change the program to use joint-interpolated motion. Perform one or more...

  • マニュアル

    ... to eAIB XSYSTEM cable XMCP connector or J, K 4a if no T20, install XMCP jumper or T20 Adapter Cable with T20 bypass plug. G or H 5 Connect user-supplied ground to eMB-40M. See Grounding the Robot Sys- n/a tem on page 82. 5a Connect user-supplied ground to robot. See Grounding the Robot System on page 82. n/a 5b Connect user-supplied ground to SmartVision MX. n/a 6 Connect 200-240 VAC to VAC Input on eMB-40M Interface Panel; secure with clamp. L 7 Connect 24 VDC to DC Input on robot ...

  • マニュアル

    ...Minor communication Communication timeout error Offline, power supply The system is not online. turned off Wireless network addi- Wireless network addition approved tion Approval has been received from the wireless master A wireless network is being added to the ...

  • マニュアル

    ...In the Solution Explorer pane, open Project name – PMAC Script Language – PLC Programs – plc1.plc. 29 4 In the programming area of the plc1.plc tab page, write a program as shown on the right. open plc 1 while(...

  • マニュアル

    ...30 4 In the programming area of the plc1.plc tab page, write a program as shown on the right. This example program turns a servo ON, starts user program 1 for the motor, then exits periodic open plc 1 while(...

  • マニュアル

    ...the motor by switching the frequency and rotation direction of the 3G3AX-MX2-ECT motor with the interval of 3 seconds. * In this example, PDO mapping is assumed to be the default setting. If you want to open plc 1 while(...

  • マニュアル

    .... 1 In the Solution Explorer pane, open Project name – PMAC Script Language – PLC Programs – plc1.plc. 2 In the programming area of the plc1.plc tab page, write a program as show on the right. open plc 1 while(...

  • マニュアル

    ... Explorer pane, open Project name – PMAC Script Language – PLC Programs – plc1.plc. 2 In the programming area of the plc1.plc tab page, write a program as show on the right. This sample program blinks the open plc 1 while(...

  • マニュアル

    .... 1 In the Solution Explorer pane, open Project name – PMAC Script Language – PLC Programs – plc1.plc. 2 In the programming area of the open plc 1 plc1.plc tab page, write a program as shown on the right. while(...

  • マニュアル

    ..., open Project name – PMAC Script Language – PLC Programs – plc1.plc. 2 In the programming area of the plc1.plc tab page, write a program as shown on the right. This sample program substitutes slave data open plc 1 while(...