全 425 件が検索されました。(181 - 200件を表示)

  • マニュアル

    ... from the ID Tag. The maximum number of pages that can be read at one time is 16. Command SOH Node No. Command code 01h 0 SECTION 4 When SECS Is Not Used Bit 7 - Page Sys - Designation 0* Value 1 0 7 Sys...

  • マニュアル

    ... writing to EEPROM. ■ READ Reads any pages of data from the ID Tag. The maximum number of pages that can be read at one time is 16. Command Command code 0 1 0 Bit 7 - Page Sys - Designation 0* 0* Value Page designation (8 characters) CR 0 0 0Dh 7 ...

  • マニュアル

    ... ROM damage Check to make sure that the Calibration ROM is correctly inserted. If correctly inserted, the Calibration ROM not Calibration ROM or displacement inserted sensor may be broken. Please contact an OMRON branch or sales office. (*1) BRK....

  • マニュアル

    ... ROM damage Check to make sure that the Calibration ROM is correctly inserted. If correctly inserted, the Calibration ROM not Calibration ROM or displacement inserted sensor may be broken. Please contact an OMRON branch or sales office. (*1) BRK....

  • マニュアル

    ...- The number of ber detected detected pat- in sampling terns measurement. Set the value Sets the obtained by X-axis (upper multiplying left) of the the X-axis machine co- (upper left) of ordinate sys- the machine tem where the coordinate robot is in system by touch-up op- 1000. eration. Set the value Sets the obtained by X-axis (upper 00501000 multiplying right) of the Hex the X-axis machine co- (upper right) ordinate ...

  • マニュアル

    ...15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0 Resv Resv Resv Resv Resv Resv Resv RF_ WAR SYS_ERR RF_ ERR CMD _ERR Resv ERR NORM BUSY READY +1 Error code +2 Response Information 1 +3 Response Information 2 +4 Response Information 3 +5 Update Counter Response +6 Response Data (The format depends on the command.) : +N *. Reserved (Resv) bits are for future expansion. They always output 0. Signal/data Name Data type Size Description READY *1 Ready BOOL 1 bit This bit turns ON when the Reader/Writer completes preparations and ...

  • マニュアル

    ... on the marking/processing to be executed. XXX Block data • Text • ID code • Straight line XXX Marking Data Block Setting • Form • Position • Fill Common Setting • Marking control • Layer • Laser power/Scan condition ...

  • マニュアル

    ...0Dh Details of Page designation (8 characters) Bit 7 - 0 7 - 3 2 1 0 7 6 - 1 0 7 6 - 2 1 0 Page Sys - Sys Sys - Sys 17 16 15 14 13 - 8 7 6 5 - 1 Sys Sys Designation 0* 0* 0* 0* 0/1 0/1 0/1 0/1 0/1 ••• 0/1 0/1 0/1 0/1 ••• 0/1 0* 0* 0* Value 00 00 to 07 00 to FF 00 to FC * Always specify 0. If you specify 1 an error (Response code: 14) will occur. Parameter Description Parameter Description Page designation ...

  • ... the tag data links are normally in operation. •PLC (EtherNet/IP Unit) LED indicators in normal status [MS]: Lit green [NS]: Lit green (PLC) [COMM]: Lit yellow [100M] or [10M]: Lit yellow •Robot Controller LED indicators in normal status [...

  • ... operation. •Controller (Built-in EtherNet/IP port) LED indicators in normal status [NET RUN]: Lit green [NET ERR]: Not lit [LINK/ACT]: Flashing yellow (Flashing when packets are (Controller) sent/received.) •Robot Controller LED indicators in normal status [...

  • ... operation. •Controller (Built-in EtherNet/IP port) LED indicators in normal status: [NET RUN]: Lit green [NET ERR]: Not lit [LINK/ACT]: Flashing yellow (Flashing when packets are (Controller) sent/received.) •Robot Controller LED indicators in normal status: [...

  • ...MEMORY Port Settings Back Light Auto OFF Clock Settings Clear Error History Clear All C&T Data Reset Teaching Environment Settings Ethernet Settings is displayed. Select IP Address by using the Up and Down CURSOR Keys. 1/2 I/O-...

  • ... Settings Back Light Auto OFF Clock Settings Clear Error History Clear All C&T Data Reset Teaching Environment Settings Fieldbus Settings is displayed. Select DeviceNet by using the Up and Down CURSOR Keys. Press ENTR. 1/2 I/O-...

  • ... normally. The LED indicators in normal status are as follows: NET RUN: Green lit NET ERR: Not lit LINK/ACT: Yellow flashing 2 Check the LED indicators on Robot Controller. The LED indicators in normal status are as follows: ...

  • ...: Yellow flashing (Flashing while packets are being sent and received.) 2 *The NX-series Controllers also have the same LED indicator status. Check the LED indicators on Manifold Solenoid Valve. The LED indicators in normal status are as follows: ...

  • ... indicators in normal status are as follows: MS: Green lit NS: Green lit COMM: Yellow lit 100M or 10M: Yellow lit 2 Check the LED indicators on Manifold Solenoid Valve. The LED indicators in normal status are as follows: ...

  • ... received.) 3 *The NX-series Controllers also have the same LED indicator status. Check the LED indicators on netTAP netTAP. MNS (DeviceNet) The LED indicators in normal status are as follows: MS (EtherNet/IP) NS (EtherNet/IP) ...

  • ... lit NS: Green lit COMM: Yellow lit 100M or 10M: Yellow lit 3 Check the LED indicators on netTAP netTAP. MNS (DeviceNet) The LED indicators in normal status are as follows: MS (EtherNet/IP) NS (EtherNet/IP) ...

  • ...66:M2_R 65:M1_R 64:M0_R DCMD-RDY READY HOME-END START_R IN-POS MOVE SEQ-BSY 161:AREA1 SET-ERR 7 129:ALM-A 162:AREA2 EXE-ERR 136:SYS-BSY 157:TIM DCMD-FULL 8 TRIG_R 134:MOVE STOP_R 9 TRIG-MODE_R 160:AREA0 138:IN-POS TLC Fixed I/O (OUT) ETO-MON Remote I/O (R-OUT) (Initial assignment) 15 14 13 12 11 10 140:TLC Assignment ALM-A The bit assignments of "Remote I/O (R-OUT)" and "Fixed I/O (OUT)" are shown below. Details of ...

  • ... the front of LCR Meter lights up green. *If it lights up red (suspended state), press Power button to power ON LCR Meter. 10 7.Ethernet Connection Procedure 6 LCR Meter powers ON. The measurement screen appears. Touch the ...