全 2437 件が検索されました。(2221 - 2240件を表示)
- マニュアル
...Reader/Writer Setting 51 Installation Environment 52 Installation and Wiring 53 Wiring for cable 55 UHF RFID System User's Manual 11 Introduction Introduction Command Line Interface Control method 60 Communication Sequence ...
- マニュアル
... 2 Installation and Wiring 21 Installation 22 Wiring 24 Section 3 Preparing Communications 49 Switch Settings 50 Test operation 57 Section 4 Function 59 Trigger Input (Lower Trigger Execution) 60 Write Protect Function ...
- マニュアル
...54 55 Key Operations for RUN Mode 57 Switching to Another Bank 58 Section 4 SETTING OF INSPECTION CONDITION Basic Knowledge for Operation 59 60 Displays of MENU/ADJ Mode and Key Operations 60 Teaching Flow ...
- マニュアル
... supply to which a device with a short-circuit is connected. (Prevent voltage drops due to short-circuits.) 65, 66, 31 12 In Setting Mode, set the shutdown sequence (DWS) and enable the External Tripping Input (TRG). 58, 59, 40 ...
- マニュアル
...) Not used with RS-232C communication. TRIG (Pink) RESET (Orange) RUN (Green) OK/NG (Black) ERROR (Gray) BUSY (Yellow) Section 5 RS-232C Communication Name (View of mating section) V400-F050/250/350 User’s Manual ...
- マニュアル
...measurement area. Center line that divides the top and bottom of the step Region is automatically set. → Check/adjustment P1 P2 (reference) (step=P2-P1) How to adjust the region p.66 ZG User’s Manual Measurement Settings ...
- マニュアル
...itself is output. Pos. correction When position shift correction is set, the position information is output using the coordinate system corrected to the original state when the coordinate system was registered. Coordinates mode ZFX-C User’s Manual Setting Measurement Items ...
- マニュアル
...Height Width 9. To improve reading reliability • When the digit is determined, designate the digit to use the bar code. • Use the modulus check (addition of check digit). • Bar codes other than the reading object should be set to reading prohibition. p....
- マニュアル
...: TEST.GBD Second USB memory device: TEST_CHG1.GBD Third USB memory device: TEST_CHG2.GBD Important The exchange procedure must be conducted within five minutes. Data will be lost when five minutes have elapsed. ZR-RX20 User’s Manual Setting Menus ...
- マニュアル
... settings. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 61 (3) TRIG settings . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 64 (4) USER settings . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 69 (5) Interface settings . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 70 (6) OTHR settings . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 72 (7) Other menus. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 75 WEB Server Function . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 87 3.SPECIFICATIONS Standard Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 94 Standard Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 94 Main Functions. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 96 Accessory/Option Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 98 PC Software. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 98 Battery Pack ZR-XRB1 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 99 Humidity Sensor ZR-XRH1 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 99 External Dimensions. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 100 12 ZR-RX40 User’s Manual ZR-RX40_UM_E.book 13 ページ 2009年12月11日 金曜日 午前10時58分 4.APPENDIX Error Messages and Countermeasures . . . . . . . . . . . . . . . . . . . . . . . . . 102 List of Error Messages . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 102...
- マニュアル
...200 Read Write 50 0 50 100 150 200 X -250 -200 -150 -100 -50 0 50 100 150 200 X RFID System User's Manual 61 Section 3 Communications Specifications Communication Time (Reference) Communications Time (Reference) Communications Time V680-HA63A:V680-HS:V680-H01-V2:V680-D1KP Communications speed setting Command Communications time N: No. of bytes processed Normal mode Read T = 1.3 N + 31 T = 2.1 N + 58 Write (without verification) T = 1.8 N + 56 Read T = 1.0 N + 29 Write (with verification) T = 1.8 N + 51 Write (...
- マニュアル
... position information of the input image coordinate system itself is output. Pos. correction When position shift correction is set, the position information is output using the coordinate system corrected to the original state when the coordinate system was registered. Setting Measurement Items ...
- マニュアル
.... . . . . . . . . . 57 Version Upgrade Information. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 61 Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 64 ZFX-C Serial Communication Command Reference 1 ■ Differences in functions between controllers This manual is intended for following Controllers. Unless otherwise specified, explanations are given for the ZFX-C20/C25. The following table summarizes the main differences. Item ZFXZFXC20/C25 C10H/ C15H ZFX-C10/C15 ZFXZFXZFX-C10-CD/C15C20-CD/ C10H-CD/ CD C25-CD C15H-CD Number of connected cameras 2 1 2 Shape Pattern Search inspection Sensitive Search Flexible Search Graphic Search Pattern search Sensitive search Pattern Search Graphic Search Flexible Search Sensitive Search Pattern search Sensitive search Size...
- マニュアル
... for RSS-limited codes JY _JY_ Reading permission for RSS-expanded codes DR _DR_ Reading permission only for DataMatrix (ECC200) codes [BCC _BCC_ Reading permission for QR codes [BCD _BCD_ V400-R1CF/R1CS User’s Manual ...
- マニュアル
...Selects the digital input processing method. Setting Description Off Disables the measurement of digital input. Logic Digital input is processed as logic signals. Pulse Digital input is processed as pulse signals. ZR-RX70 User’s Manual Setting Menus ...
- マニュアル
...Reference: Reference: Reference: Reference: Reference: Reference: Reference: Reference: Measuring folding of papers and sheets (p.60) Checking the interior/exterior and direction (p.60) Checking for mixing of different objects (p....
- マニュアル
... are displayed in the "Setting model" area. 2 Measurement 3. The image specified for the model is displayed in the Image Display area. 5. To register two or more models, repeat the Steps Reference: 2(p.60) to Reference: 4(p....
- マニュアル
... performance flag Get/Set 0: OFF 1: ON 151 Edge level (defect width and depth edge measurement) Get/Set 0 to 100 152 Noise level (defect width and depth edge measurement) Get/Set 0 to 255 61 No. Data name Get/Set Range 153 Region width (defect width and depth edge measurement) Get only 0 to 10 154 Noise width (defect width and depth edge measurement) Get/Set 0 to 640 155 Corner judgement (start angle) Get/Set 0 to 30 156 Corner length Get/Set 0 to 9999 157 Corner judgement (start–end angle) Get/Set 0 to ...
- マニュアル
... and performs measurements. FQ User’s Manual Measurement region Max. color change: 25 Min. color change: 10 25 − 10 < 30 Judges that there is no edge (measurement result is NG). Inspecting with the Edge Position Inspection Item ...
- マニュアル
... 85 for details on setting the date and time. 9. AC/battery display : Running on AC or DC power supply. : Running on the battery. The remaining battery power is 100 to 91%. : Running on the battery. The remaining battery power is 90 to ...