全 2436 件が検索されました。(2161 - 2180件を表示)
- マニュアル
... the digital input port when the period key is pressed. 10 CLS 20 IF KEYIN=1 THEN GOSUB 100 30 SMEASURE 40 LOCATE 1, 19:PRINT AR 50 GOTO 20 100 S=INPW AND 15 110 CHANGE S 120 RETURN 61 Commands, Statements and Functions Section 2 INT Item Contents Function Returns an integer with the fractional part removed. Format INT (
) Example A!=INT(1.23) Description Returns the largest integer which does not exceed the value given by . For example, INT(1.23) will be 1 and INT(–1.23) will be –2 after ... - マニュアル
.... . . . . . . . . . . . . . . . . . 48 48 49 50 50 50 50 50 51 56 56 56 57 57 58 59 61 64 64 65 67 72 47 Section 4–1 Communications Connectors 4–1 Communications Connectors 4–1–1 Connection of E5AX-A20 and PC The E5AX Controller with BCD communications can be directly connected to a PC (Programmable Controller) or a personal computer. E5AX-A20 PC (SYSMAC) DSL1 Input circuit DSL2 External power supply DSL3 +24 V DSL5 4.7 kW DSL4 DSL6 WD1 WD2 WD3 WD4 VAL RD1 RD2 RD3 RD4 BUSY GND Output circuit 24 DC GND 1 OUT 2...
- マニュアル
...4 5 6 7 8 10 11 12 16 16 17 18 20 23 24 28 32 36 48 49 50 52 53 54 58 61 62 63 Appendices A B C D Codes . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Auto Read/Auto Write . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Specifications and Ratings . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Conformity to Standards . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 69 71 73 77 81 ix About this Manual: This manual describes the operation of the V600/620 RFID System and includes the sections described below. Please read this manual completely and be sure you understand the information provided before attempting to operate the system. Section 1 Provides a general introduction to the RFID ...
- マニュアル
.... . . . . . . . . . . . 1 2 3 4 5 6 8 11 12 16 25 27 28 33 36 41 55 59 60 61 62 63 63 Appendices A B C D Standard Models . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Codes . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Auto Read/Auto Write . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Specifications and Ratings . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Index . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 69 71 73 75 79 81 vii About this Manual: This manual describes the operation of the V630 FA ID System and includes the sections described below. Please read this manual completely and be sure you understand the information provided before attempting to operate the system. Section 1 provides a general introduction to the V630 FA ID System....
- マニュアル
.... . . . . . . . . . . . . . 1 2 6 9 10 22 34 39 40 41 42 44 47 55 56 56 58 59 61 vii About this Manual: This manual describes the basic installation and specifications of Units used in F300 Visual Inspection System and includes the sections described below. Please read this manual completely and be sure you understand the information provided before attempting to install and operate an F300 Visual Inspection System. Section 1 presents a brief introduction to the F300 Visual Inspection System, its required Units, and optional Units. This section also includes examples of system configurations. Section 2 describes the ...
- マニュアル
...When “O. Draw” is selected, a message will be displayed in the comment line asking you to designate a square area. 8. Designate a square in an area that will not be affected by the presence of the object that is to be measured. ...
- マニュアル
...60 CAMERA Switches cameras. Camera/strobe control Command 60 CAMMODE Selects the image output from a Camera I/F Unit. Camera/strobe control Command 60 CDBL Converts to a double-precision value. Calculation Function ...
- マニュアル
... = 0.65 α = 1.00 (Proportional preceding PID) Difference in set point response due to α. To increase the set point response speed, decrease the value of parameter α. If the value of parameter α is decreased, however, the overshooting value will increase. ...
- マニュアル
...Section 3-2 9. Set the binary level for the measurement so that the marks will be displayed in white. Setting the Output Data 10. Set the output expression. Set the center of gravity X and Y coordinates for each mark. ...
- マニュアル
... the OVL Area Size Setting the RS-232C Communications Specifications Setting the Output Specifications for Parallel Data Page 53 Page 54 Page 57 Setting Specifications of the Camera to be Connected Page 60 Setting the Date and Time for the Timer Page ...
- マニュアル
...: Stop the buzzer. 1: Continuously sound the buzzer. The buzzer sounds for a fixed time if the parameter is omitted. After the buzzer is turned on, it can be turned off again only with the BEEP command. The buzzer remains on if program operation stops. ...
- マニュアル
... Plate PFP-M (Supplied by OMRON) Clearance Between Amplifiers When installing multiple V600-HAR91, V600-HAR81, or V600-HAR92 Amplifiers side by side, provide at least 10 mm clearance between Amplifiers to allow them to dissipate heat properly. 10 mm min. Amplifiers ...
- マニュアル
.... . . . . . . . . . . . . Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 59 61 63 65 ix About this Manual: This manual describes the installation and operation of the V600 Hand-held Reader Writer and includes the sections described below. Please read this manual carefully and be sure you understand the information provided before attempting to install and operate the Hand-held Reader Writer. Section 1 describes the features and system configuration of the Hand-held Reader Writer. Section 2 provides information on the specifications and functions of the Hand-held Reader Writer. Section 3 describes the command and response formats for communications between the host device and the ...
- マニュアル
... where it can correctly view the object. If the field of vision of the Camera is too small for the object being measured, use the Camera with a normal CCTV lens and light. → p. 14 Measurement object Distance 20-mm lens: ...
- マニュアル
.... . . . . . . . . . . . . . . . 1 2 3 3 5 7 8 18 21 26 33 34 37 39 40 44 52 61 62 64 66 68 70 71 73 74 75 Appendices A B C D Accessories (Sold Separately) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . I/O Allocation . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Multi-vendor Applications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Conformity to Standards . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 79 81 83 87 89 xi About this Manual: This manual describes the installation and operation of the V600 RFID System Intelligent Flag III for the DeviceNet and includes the sections described below. Please read this manual carefully and be sure you understand the information provided before attempting to install and operate the ...
- マニュアル
...The camera’s set distance is an approximate value. The camera’s mounting allows it to be adjusted slightly nearer to or farther from the object. F150-SL20A/SL50A Mounting dimensions → p. 63 Measurement object Camera distance 20-mm lens: ...
- マニュアル
.... . . . . . Saving to Flash Memory . . . . . . . . . . . . . . . . . . . . . . 16 17 18 21 24 28 29 44 46 61 SECTION 4 Terminal Block . . . . . . . . . . . . . . . . . . . . . . 63 4-1 4-2 4-3 I/O Formats . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Terminal Signal Operation and Timing . . . . . . . . . . . Communications Settings . . . . . . . . . . . . . . . . . . . . . . 64 65 72 SECTION 5 CompoBus/D Settings . . . . . . . . . . . . . . . . . 75 5-1 5-2 5-3 5-4 5-5 Communications Settings . . . . . . . . . . . . . . . . . . . . . . Input Format . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Output Format . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Timing Charts . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Allocation Charts . . . . . . . . . . . . . . . . . . . . . . . . . . . . 76 81 83 85 88 v TABLE OF CONTENTS vi SECTION 6 RS-232C Communications Settings . . . . . 91 SECTION 7 Troubleshooting . . . . . . . . . . . . . . . . . . . . . 95 Index . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 99 Revision History . . . . . . . . . . . . . . . . . . . . . 101 About this Manual: This manual describes the operation of ...
- マニュアル
... the reference. Therefore, draw the region after putting the measurement object in a position where the part to be measured lies totally inside the screen. 43 Section 3-2 Position Compensation The procedure is the same as for ordinary measurement. → p. ...
- マニュアル
... can be made on the whole input screen. However, the search range can be limited to reduce the processing time and increase the accuracy. The procedure is the same as for measurement. Refer to Setting the Search Region under 3-3-3 Searches → p. ...
- マニュアル
... during readings. Writes data to Write Area. Returns write completed response. End A timeout error occurs if there is no response within 5 s. An error message appears on the screen and the ERR (error) terminal turns ON. Program example → p. ...