全 2904 件が検索されました。(2101 - 2120件を表示)
- マニュアル
...Suitability for Use Approx.110g FLV-XC5EPR 5m OMRON Corporation Approx.130g Hold "the tab of the plug connector" in the arrow (←) direction and pull it straight. 【Note】 Do not pull out with excessive force without pressing the tab. Doing ...
- マニュアル
... then insert it until it clicks. Before mounting Controller side After mounting ●Removing Hold "the tab of the plug connector" in the arrow (←) direction and pull it straight. 【Note】 Do not pull out with excessive force without pressing the tab. Doing ...
- マニュアル
....1 Always follow the rules below to ensure safety. 1. Installation environment · Do not use in a location where there is flammable or explosive gas. · To ensure safe operation and maintenance, install away from high-voltage equipment and power equipment. · Install the unit ...
- マニュアル
... overall system, use a UL Class II DC power supply. · Use an independent power source for this product. Do not use a shared power source. 3. Handling · Do not peel off or damage the waterproof sheet attached to the side of the unit. Doing ...
- マニュアル
... potentially hazardous situation which, if Caution not avoided, may result in minor or moderate injury, or property damage. Warnings and Cautions Do not attempt to take any Modules apart or touch WARNING any internal parts while the power is being supplied. Doing ...
- マニュアル
... which it will be used. Know and observe all prohibitions of use applicable to this product. Stand bars: 2 pieces See detail drawing of screw tightening. Features Tilt angle of LCD (60 degrees) (247) fitted. At this time, insert it ...
- マニュアル
...2-M3 DEPTH 5 max Specification Light source White LED Part 0 Part 1 Part 5 Part 2 Part 6 Part 3 Part 7 Old version FZ Controller recognizes this illumination and strobe controller as FZ-SLC100.And so, the image of LED’s allocation on the Menu is displayed as FZ-SLC100’s one. THE PRODUCTS CONTAINED IN THIS SHEET ARE NOT SAFETY RATED. THEY ARE NOT DESIGNED OR RATED FOR ENSURING SAFETY OF PERSONS, AND SHOULD NOT BE RELIED UPON AS A SAFETY COMPONENT OR PROTECTIVE DEVICE FOR SUCH PURPOSES. Please refer to separate catalogs for OMRON's ...
- マニュアル
... your OMRON sales representative. ·When disposing of the Illumination, dispose of it as industrial waste. ■Dimensions 66 PRECAUTIONS FOR SAFE USE NOTE1.FZ-LTW31DR is adjusted in 3block. NOTE2.Old version FZ Controller recognizes this illumination and strobe controller as FZ-SLC100.And ...
- マニュアル
... (safety extra low-voltage circuits on the secondary side). ■Installation environment ・ Do not use the product in environments where it may be exposed to inflammable/explosive/corrosive gas. ・ Do not use the product outdoors or in environments exposed to direct sunlight. ・ Install the unit ...
- マニュアル
.... For your convenience, keep the sheet at your disposal. · Keep foreign matter away from the connector. Otherwise a failure may occur. · Do not touch the terminal portion (connecting portion) of this product directly or allow it to come in contact with metals. Doing ...
- マニュアル
.... For your convenience, keep the sheet at your disposal. · Keep foreign matter away from the connector. Otherwise a failure may occur. · Do not touch the terminal portion (connecting portion) of this product directly or allow it to come in contact with metals. Doing ...
- マニュアル
... Headquarters OMRON EUROPE B.V. Sensor Business Unit Carl-Benz-Str. 4, D-71154 Nufringen, Germany Tel: (49) 7032-811-0/Fax: (49) 7032-811-199 Camera cable connector Camera FZ-SC2M FZ-S2M *The camera cable is polarized, ...
- マニュアル
...: (49) 7032-811-0/Fax: (49) 7032-811-199 OMRON ELECTRONICS LLC 2895 Greenspoint Parkway, Suite 200 Hoffman Estates, IL 60169 U.S.A. Tel: (1) 847-843-7900/Fax: (1) 847-843-7787 Approx. 85g (including base) *The camera cable is polarized, ...
- マニュアル
... the Controller immediately, turn OFF the power supply, and consult your OMRON representative. ・Dispose of FZ-SC components as industrial waste. Camera Name plate Camera cable FZ-SC/S connector *The camera cable (FZ-VS,FZ-VSL,FZ-VSB) is polarized, ...
- マニュアル
... 4 年 7月 TRACEABILITY INFORMATION: Importer in EU: Manufacturer: Omron Europe B.V. OMRON Corporation, Wegalaan 67-69, Shiokoji Horikawa, Shimogyo-ku, NL-2132 JD Hoofddorp Kyoto. 600-8530 JAPAN The Netherlands *The camera cable is polarized, ...
- マニュアル
...immediately, turn OFF the power supply, and consult your OMRON representative. ・ Dispose of FZ-SHC/SC components as industrial waste. Camera cable connector Name plate Camera FZ-SHC FZ-SH *The camera cable (FZ-VS,FZ-VSL,FZ-VSB) is polarized, ...
- マニュアル
...Weight Approx. 70 g Dimensions 12 35.5 (Unit: mm) Item FZ-SLC100-DL Transmittance 87% (typical value) 78 Performance Specifications Removal 1. Loosen the screws of the mounting brackets and turn the brackets ...
- マニュアル
... on the back of the camera and the camera connector on Controller FZ-3□□. Extension Camera cable Camera cable connector connector FZ-VS□ Nameplate Intelligent camera FZ-SLC100 *The camera cable (FZ-VS,FZ-VSL,FZ-VSB) is polarized, ...
- マニュアル
...-DL Transmittance 87% (typical value) Mounting brackets 73 93 38 39 40.5 36 20 11.5 Item 1. Loosen the screws of the mounting brackets with the provided hexagonal wrench and turn the brackets so that they will not catch on the illumination part of the FZ-SLC15. 1.5 Performance Specifications (Unit: mm) Diffusion Board φ28 73 92.5 Operating: 0 to 50°C (with no icing or condensation) Storage: −25 to 60°C (with no icing or condensation) 12.5 Thank you for selecting this OMRON product. This Instruction Sheet primarily describes precautions required ...
- マニュアル
...OMRON ELECTRONICS LLC One Commerce Drive Schaumburg,IL 60173-5302 U.S.A Phone:1-847-843-7900 Telephone Consultation 1-800-55-OMRON Fax : 1-847-843-7787 Intelligent camera FZ-SLC15 *The camera cable (FZ-VS,FZ-VSL,FZ-VSB) is polarized, ...