全 2739 件が検索されました。(1601 - 1620件を表示)
- マニュアル
.... Indicator PWR (Green) ( ) Display ERC (Red) ON OFF ON OFF ON Flashing OFF ON OFF ON OFF ON COMM (Yellow) OFF Flashing RUN ((Green)) ERR ((Red)) SD ((Yellow)) RD ((Yellow)) OFF 16 2-2 Status Power is being supplied. Power is not being supplied. In RUN mode or MONITOR mode In PROGRAM mode or fatal error has occurred. Fatal error has occurred. Non-fatal error has occurred. Normal operation CompoBus/S data is being sent. Data is not being sent. CompoBus/S data is being received. Data is not being received. A CompoBus/S communications error has occurred. Normal ...
- マニュアル
... 25-pin Connector Adapter required for 9-pin connector. Section Formatting Floppy Disks 2-2 2-1-4 Preparing the Connecting Cable Personal Computer with D-sub 9-pin RS-232C Connector PCU or CPU Unit Personal computer ...
- マニュアル
...35 15 101 (16.5 including cover) (Unit: mm) 130 CS1W-ETN11 35 101 (Unit: mm) 9 Section 1-6 Software Configuration CJ1W-ETN11 65 2.7 31 ETN11 RUN ERC SD RD ERH TCP FTP EF012 6789 345 ABCD EF012 6789 345 TS UNIT No. NODE No. x161 ABCD EF012 6789 345 ABCD 90 x160 2.7 ETHERNET 1-6 (Unit: mm) Software Configuration The software supported by the Ethernet Unit runs in the layers shown in the following diagram. The components that form the various layers are defined below the diagram. Memory Card/ EM File Memory CS/CJ-...
- マニュアル
... Units RS-232C Connector Pin Arrangement (Same for Ports 1 and 2) Pin No. Symbol Signal name Signal direction RS-232C Unit ↔ External devices 1 2 --RD Not used Receive data --← 3 4 SD --- Send data Not used → --- 5 6 SG --- Signal ground Not used ----- 7 8 RS CS Request send (See note.) Can send (See note.) → ← 9 --- Not used --- Note The CS signal is always checked. Data will not be output if CS is not connected. Short-circuit the RS-CS signals when they are not used. A connection example using applicable connectors and recommended cables is provided ...
- マニュアル
...RS-232C cable Wiring Connect the Units with the cables wired as shown below. CQM1H CQM1H or another C–series PC Signal Abb. Pin No. Pin No. Signal Abb. FG Hood Hood FG SD 2 2 SD RD 3 3 RD RTS 4 4 RTS CTS 5 5 CTS – 6 6 – – 7 7 – – 8 8 – SG 9 9 SG Recommended Cables UL2464 AWG28x5P IFS-RVV-SB (UL-approved, Fujikura Ltd.) AWG28x5P IFVV-SB (not UL standard) (not UL-approved, Fujikura Ltd.) UL2464-SB (MA) 5Px28AWG (7/0.127) (UL-approved, Hitachi Cable, Ltd.) CO-MA-VV-SB 5Px28AWG (7/0....
- マニュアル
... inclusion) Orange Lit Not lit Unit is part of Network. Unit is not part of Network. M/S (polling node) Orange Lit Not lit Unit is polling node. Unit is not part of Network or is polled node. SD (send) Orange Lit Not lit Unit is sending data. Unit is not sending data. RD (receive) Orange Lit Unit is receiving data. LNK (data link) Orange Not lit Lit Unit is not receiving data Unit is part of active data link. Flashing Data link error has occurred. Rapid flash- Data link table communications cycle time is too short. ing Not ...
- マニュアル
... interface error, EEPROM error, unit number error, I/O table not set, duplex communications setting error, or duplex settings incomplete INS (network participation) Yellow Not lit Lit No error. Unit is participating (inserted) in the network. Not lit ...
- マニュアル
... Controller Link Support Board...................................................................................... 67 59 Section Names and Functions of Parts 2-1 2-1 Names and Functions of Parts 2-1-1 Names and Functions of Parts 34.5 mm CS LC001 RUN ERC ...
- マニュアル
... 9-pin male) RS-232C 15 m Hood: XM2S-0911-E Plug: XM2A-0901 (Provided with Loop Control Unit) ES100X (with RS-232C serial communications) ES100 01 Wiring Loop Control Unit ES100X RS-232C Signal FG SD RD RS CS 5V DR ER SG Pin No. 1 2 3 4 5 6 7 8 9 D-Sub 9-pin female Shield (Cable connector: male) RS-232C Signal Terminal ...
- マニュアル
... included with the CPU Unit or an equivalent connector to connect to the DeviceNet transmission line. 5. PC Status Indicators The following indicators show the operating status of the PC. Indicator PWR (green) RUN (green) ERR/ALM (red) ...
- マニュアル
... a cable using the connection method and components given below. Connector Pin Arrangement The pin arrangement for the CPU Unit connector is shown below. Pin number Signal abbreviation Signal name 1 FG Frame ground --- 2 ...
- マニュアル
.... When constructing an intranet, communication failure may occur due to cable disconnection or the influence of unauthorized network equipment. Take adequate measures, such as restricting physical access to network devices, by means such as locking the installation area. When using a device equipped with the ...
- マニュアル
... mm (W × H × D) Conform to general specifications for the SYSMAC CJ Series. 14 Section 1-4 Specifications 1-4-2 Dimensions CS1W-ETN21 ETN21 100M ERH TCP FTP HOST RUN ERC SD RD LNK UNIT NO. 0 1 ×161 ×160 130 NODE NO. 0 100BASE-TX 10BASE-T 35 101 (Unit: mm) CJ1W-ETN21 Back Front • Unit Version 1.5 or Later ETN21 65 31 2.7 2.7 31 • Unit Version 1.4 or Earlier ETN21 ERC ...
- マニュアル
...Weight Dimensions 200 g max. 35 × 130 × 101 mm (W × H × D) 11 Section 1-4 Specifications 1-4-2 Dimensions CS1D-ETN21D ETN21D 100M ERH TCP RUN ERC SD RD LNK DPL UNIT NO. 0 1 ×161 ×160 130 NODE NO. 0 100BASE-TX 10BASE-T 35 101 (Unit: mm) 1-4-3 Software Configuration The software supported by the Ethernet Unit runs in the layers shown in the following diagram. The components that form the various layers are defined below the diagram. CS-series CPU Unit CS-series CPU Unit FINS communication service 7....
- マニュアル
...given below. Connector Pin Arrangement The pin arrangement for the CPU Unit connector is shown below. Pin number 1 2 3 4 5 6 7 8 9 Metal cap Signal abbreviation FG SD (TXD) RD (RXD) RS (RTS) CS (CTS) 5V DR (DSR) ER (DTR) SG (0V) FG CS-series Pin Arrangement Signal direction --Output Input Output Input --Input Output ----- CJ-series Pin Arrangement 5 1 1 5 9 6 Signal name Frame ground Send data Receive data Request to send Clear to send Power supply Data set ready Data terminal ready Signal ground Frame ground 6 9 13 Connecting ...
- マニュアル
... occur if any of these mode numbers is set. 1-3 Devices in a CompoNet Network 1-3-1 Master Units CompoNet Master Units Name CS-series Master Unit CRM21 MS NS Model CS1WCRM21 +100 SD RD 109 X101 87 4 32 87 65 4 32 MACH No. 109 65 MODE X100 87 4 32 109 65 ON 1 2 3 4 1 DR0 2 DR1 3 ESTP 4 REGS NETWORK POWE SUPPLRY BS+ BSDC24V INPUT BS + BD H Unit classification Maximum number per CPU Unit CS-series Communications Special I/O mode No. Unit 8 (1 unit number...
- マニュアル
...[W461-E1-06] CP1L, CP1E Programmable Controller Introduction Manual W461-E1-06 CP1L-L10D- CP1L-L14D- CP1L-L20D- CP1L-M30D- CP1L-M40D- CP1L-M60D- CP1E-ESD- CP1E-NSD- CP1E-ED- CP1E-ND- CP1E-NAD- CP1L/CP1E CPU Unit Introduction Manual Notice: OMRON products are manufactured for use according to proper procedures by a qualified operator and only for the purposes described in this manual. The following conventions are used to indicate and classify precautions in this manual. Always heed the information provided with them. Failure to heed precautions can result in injury to ...
- マニュアル
...Temperature Controller CS/CJ Series PLC Input Power RS-232C Cable Attachment adapter K32-23209 RS-232C Port To attachment adapter To PLC Signal Signal Pin No. Pin No. RD 2 2 SD SD 3 3 RD ER 4 4 RS SG 5 5 CS DR 6 7 DR RS 7 8 ER CS 8 9 SG FG - - FG Procedure for Smart Sensors 1. Right-click Smart Sensor in the Network Configuration Window and select Parameter – Edit. 2. The Edit Parameters Dialog Box will be displayed. After setting the parameters, select Transfer [PC to Unit] to download the settings to ...
- マニュアル
... the wire insulation in the wire hole) and pull out the screwdriver to lock the wire in place. 21 Section 3-2 Wiring Recommended Components • The following screwdriver can be used when inserting and removing wires. Recommended screwdriver Model number ...
- マニュアル
.... Note 3: An action program is executed just once per cycle (unlike the CV-series SFC operation), even if the action program is used in multiple steps and the multiple steps are active at the same time. N, P, P1, P0, L, D, R, S, SL, ...