全 2739 件が検索されました。(1701 - 1720件を表示)
- マニュアル
... 2 3 4 5 Fitting 10 1 6 7 NC Pin No. 1 Pin No. 1 Signal name 4-4 ZS-DSU User’s Manual 8 9 Signal name NC SD(TXD) 2 2 RD(RXD) RD(RXD) 3 3 SD(TXD) RS(RTS) 4 4 NC CS(CTS) 5 5 SG(GND) NC 6 6 NC NC 7 7 RS(RTS) NC 8 8 CS(CTS) SG(GND) NC 9 9 NC 10 Section 4 RS-232C Input/Output Setting the Communication Specifications Set the RS-232C communications specifications. Match the communication specifications of the ZS-DSU to ...
- マニュアル
... the 24 VDC power supply ter- 6 7 8 9 Pin No. Signal name Symbol minals. Signal direction Remarks 1 — NC — Not connected 2 Receive data RD Input 3 Send data SD Output 4 — — Output 5 Signal ground SG — 6 — — Input Use in the open status. 7 Request send RS Input Always ON during normal operation 8 — NC — Not connected 9 — NC — Not connected Always OFF Recommended model Manufacturer Cable Connector Socket Hood 28 CIDRW System User’s Manual Model Hitachi Cable CO-MA-VV-SB 5PX28AWG OMRON XM2D-0901 XM2S-0913 SECTION 2 Installation and Connections/Wiring • Wiring...
- マニュアル
...10 1 2 6 NC Pin No. 1 Pin No. 1 Signal name Section7 USB/RS-232C COMMUNICATION Controller side 3 7 4 8 5 9 Signal name NC SD(TXD) 2 2 SD(TXD) RD(RXD) 3 3 RD(RXD) RS(RTS) 4 4 RS(RTS) CS(CTS) 5 5 CS(CTS) NC 6 6 NC NC 7 7 NC NC 8 8 NC SG(GND) NC FG 9 9 SG(GND) 10 Shell Shell FG Note 1: Plug type connector ZS-HL User’s Manual 7-5 Section7 Connecting Using a RS-232C Cable RS-232C Cable ...
- マニュアル
..., Connections, and Wiring RS-232C Port Pin Arrangement SECTION 2 Connection and Wiring Pin No. Symbol 9 2 3 RD 4 RS 5 CS Signal direction Input Output SG --- --- SD --- • ID Controller Terminal Arrangement Signal name 5 1 Signal ground or common return line Send data ----- Receive data Request to send --- Clear to send 9 6 The pin arrangement is different from that of the V680-CA1A. Use an RS-232C cable for the V680-CA5D@@V2. Connections to Host Device Example Connection to OMRON PLC Host device ID Controller Pin No. Symbol Pin No. Symbol...
- マニュアル
... a 9-pin D-sub (female-female) cross cable. 2 6 7 Pin No. 3 4 5 8 9 Signal name 1 N.C. 1 CD 2 RD 2 RD 3 SD 3 SD 4 N.C. 4 ER 5 SG 5 SG 6 N.C. 6 DR 7 N.C. 7 RS 8 N.C. 8 CS 9 N.C. 9 CI Shell FG COMMUNICATIONS WITH EXTERNAL DEVICES Connector Pin Arrangement and Connection Example with a PC * Pin Nos. may vary with the type and model of the external device to be connected. For details, refer to the ...
- マニュアル
... in improving -SF 12 OPE1 OPE2 OPE3 ZN product quality. By connecting Interface Units, you can log the measured data of Air Particle Sensors at up to ten locations at once on a personal computer. The Electrostatic Sensor (ZJ-...
- マニュアル
.... • Install firewalls to shut down unused communications ports and limit communications hosts and isolate control/monitor systems and equipment from the IT network. • Use a virtual private network (VPN) for remote access to control/monitor systems and equipment. • Scan virus to ensure safety of ...
- マニュアル
... Preparations V680-CH1D Communications Preparations Pin Arrangement of the Host Device Interface Connector V680-CH1D 1 Signal (See note.) 1 --- 2 Receive data RD Hand-held Reader/Writer to host device 3 Send data ...
- マニュアル
... connector. Prepare a compatible connector. Recommended part: XM3A-0921 (plug) XM2S-0911 (hood) 5 4 9 8 3 2 7 6 1 Pin No. 1 Signal Name Description FG (GND) Protective ground 2 SD (TXD) Send data 3 RD (RXD) Receive data 4 NC Not connected 5 NC Not connected 6 NC Not connected 7 NC Not connected 8 NC Not connected 9 SG (GND) Signal ground ● Setting the communication specifications Set the RS-232C communications specifications. Match the communication specifications of the ZUV to those of the external device. LOCK mode-[SYSTEM]--[COMM PORT] Setting value 4-10...
- マニュアル
... computer Use a cable with the following pin layout. ZS-XRS2 (cable length: 2 m) 4 10 Fitting section 1 Personal computer side (PC/AT compatible) (Note 1) 5 4 3 2 1 9 Signal name NC SD (TXD) RD (RXD) RS (RTS) CS (CTS) NC NC NC SG (GND) NC FG Pin No. 1 2 3 4 5 6 7 8 9 10 Shell 8 7 6 Pin No. 1 2 3 4 5 6 7 8 9 Signal name NC RD (RXD) ...
- マニュアル
... the 24 VDC power supply ter- 6 7 8 9 Pin No. Signal name Symbol minals. Signal direction Remarks 1 — NC — Not connected 2 Receive data RD Input 3 Send data SD Output 4 — — Output 5 Signal ground SG — 6 — — Input Use in the open status. 7 Request send RS Input Always ON during normal operation 8 — NC — Not connected 9 — NC — Not connected Always OFF Recommended Models Manufacturer Cable Connector Socket Hood 38 CIDRW System User’s Manual Model Hitachi Cable CO-MA-VV-SB 5PX28AWG OMRON XM2D-0901 XM2S-0913 SECTION 2 Installation and Connections/Wiring • Wiring...
- マニュアル
... combinations may cause malfunction or damage. • Do not turn the power OFF in the following instances. Doing so will damage data that is in the process of being saved. - While data is being saved in internal memory - While data is being saved on the ...
- マニュアル
... turned ON after the control power supply, temporary errors may result in incorrect control system signals because the output terminals on Output Units may momentarily turn ON when power supply is turned ON to the Controller. • If you transfer data from a backup file on an ...
- マニュアル
... combinations may cause malfunction or damage. • Do not turn the power OFF in the following instances. Doing so will damage data that is in the process of being saved. - While data is being saved in internal memory - While data is being saved on the ...
- マニュアル
... Connection Pin arrangement (Pin alignment) Connector part (DIN: 8P plug) Made by Hosiden Corporation TCP1394-715267 (Type A) Connection with upper equipment p.33, p.34 Wire color Pin No. Signal name Function Reader Green 1 ...
- マニュアル
...User’s Manual Section 2 Wiring and Installation This section explains about the wiring method and installation method of the 29 Section 2 Wiring and Installation Wiring • • • • Section 2 Wiring Extension length of the RS-232C line (...
- マニュアル
... intranet, communication failure may occur due to cable disconnection or the influence of unauthorized network equipment. Take adequate measures, such as restricting physical access to network devices, by means such as locking the installation area. When using a device equipped with the USB flash drive or ...
- マニュアル
... on the previously loaded image. p.222 8010 0010 Set Registered Image Sets the latest image or a specified logging image as a registered image. p.223 8020 0010 Acquire Registered Image Loads a registered image saved to the ...
- マニュアル
... other countries. • Intel, Core and Pentium are trademarks of Intel Corporation in the U.S. and/or other countries. • EtherCAT® is registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany. • ODVA, CIP, CompoNet, DeviceNet, and EtherNet/IP are trademarks of ODVA. • The ...
- マニュアル
... with the GR (frame ground) in the 24 VDC power supply terminals. Pin No. 1 Signal name Symbol Signal direction Remarks — NC — Not connected 2 Receive data RD Input 3 Send data SD Output 4 — — Output 5 Signal ground SG — 6 — — Input Use in the open status. 7 Request send RS Output Always ON during normal operation 8 Clear to send CS Input Operates even if not connected. 9 — NC — Not connected Always OFF Recommended Models Manufacturer Cable*1 Connector Socket Hood Model Hitachi Cable CO-MA-VV-SB 5PX28AWG OMRON XM2D-0901 XM2S-0913 *1: The bending radius ...