全 2739 件が検索されました。(1581 - 1600件を表示)
- マニュアル
... Edge, Excel, and Visual Basic are either registered trademarks or trademarks of Microsoft Corporation in the United States and other countries. • EtherCAT® is registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany. • ODVA, CIP, CompoNet, DeviceNet, and EtherNet/IP are trademarks of ODVA. • The ...
- マニュアル
... Vista, Excel, and Visual Basic are either registered trademarks or trademarks of Microsoft Corporation in the United States and other countries. • EtherCAT® is registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany. • ODVA, CIP, CompoNet, DeviceNet, and EtherNet/IP are trademarks of ODVA. • The ...
- マニュアル
... Edge, Excel, and Visual Basic are either registered trademarks or trademarks of Microsoft Corporation in the United States and other countries. • EtherCAT® is registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany. • ODVA, CIP, CompoNet, DeviceNet, and EtherNet/IP are trademarks of ODVA. • The ...
- マニュアル
... (COM1, COM2, or COM3) of the Open Network Controller to port A of the PT. Open Network Controller 1 2 3 4 SG 5 6 RS 7 CS 8 9 COM1 COM2 COM3 RD SD 3-7 PT 1 2 SD 3 RD 4 RS 5 CS 6 7 8 9 SG PORT A Connecting DeviceNet Cables This section explains how to connect DeviceNet cables to the Open Network Controller. 3-7-1 Connectors Model Specifications Manufacturer MSTB2.5/5-ST5.08AU For node connections. Connector screws not supplied. XW4B-05C1-H1-D For node connection and T-branch ...
- マニュアル
... using the Special Cable. For the UPS setting in the Setup Tool, set the power failure signal as a negative logic input. UPS BU606F BU70XS Applicable Special Cable BUC10 BUC16 Special Cable Wiring (Reference) SPU Cable: BUC10/BUC16 ...
- マニュアル
...-40UNC) 1 6 9 5 Connector Pin Arrangement Pin No. 1 2 3 4 5 6 7 8 9 Shell 2-5 2-5-1 Abbrev. NC RD SD NC SG NC RS CS NC FG Signal name Not used. Receive Data Send Data Not used. Signal Ground Not used. Request to Send Clear to Send Not used. Shield I/O --Input Output ------Output Input --- Handling a PC Card or Memory Card CS1W-SPU01/SPU02-V2 Inserting a PC Card 1,2,3... This section describes how to insert a PC card into the PC card slot on the...
- マニュアル
... settings are checked in the following order. • FTP send settings: 0→1→2→3→5→6→7→9 • Recipe receive settings: 0→3→1→2→4→5→7→8→9 Sequential Display The connection will be checked in order of the functions from FTP Send (...
- マニュアル
... Step 2 appear. You can recover from the problem by referring to what is displayed in “Detailed Information”. 4. In Steps 2 and 3, if you press the “Screen Shot” button, the currently displayed screen can be captured and saved in an ...
- マニュアル
...□□□□-V1 (j) (a) (b) (a) (j) (d), (e) (c) (d), (e) (c) (f) (b) (f) (g) (i) (i) (g) (h) (a) Battery cover (b) Expansion unit connector cover*1 (c) SD memory card slot (d) Ethernet port (e) Serial port*1 (f) USB port(host) (g) USB port(slave) (h) Reset switch (i) 24VDC (j) Identification label (h) (a) Battery cover (b) ...
- マニュアル
...φ20 37 2-M5×10 取付穴寸法 R18 ■配線図形V500-R2CF (ピン配列) 18 24 形式 緑白灰青茶 − 黒赤黄橙 信号名 SD 1 2 RD RS 3 4 CS TRIG 5 6 NC S GND 7 8 VCC −(注) OK −(注) NG 役割 バーコードリーダ 送信パラメ−タ受信パラメ−タ送信要求送信可外部トリガ信号無接続 0V 電源読...
- マニュアル
...* Frame ground Signal ground Send data Receive data Request to send Clear to send Equipment Ready Send signal element timing 1*** Send signal element timing 2*** Receive timing*** 5-V power supply** Symbol FG SG ...
- マニュアル
...Cable Length: 15 m 9 6 9 6 ····· ···· ····· ···· 5 Port 1 1 5 Port 2 1 Pin No. Symbol Name Direction 1 FG Frame ground – 2 SD Send data Output 3 RD Receive data Input 4 RTS Request to send Output 5 CTS Clear to send Input 6 – Not used – 7 DSR Data send ready Input 8 DTR Data terminal ready Output 9 SG Signal ground – 111 Appendix B Specifications Connections to Peripheral Devices RS-232 Printer Connections ASCII Unit Printer FG 1 1 FG SG 9 7 SG ...
- マニュアル
...SYSMAC C-series SYSMAC LINK C-series SYSMAC LINK System Manual Revised September 2003 SLK11 SLK21-V1 RUN ERC P/S ERH RUN ERC ERH INS M/S INS M/S SD RD SD RD TS LNK TS LNK SLK24 SLK14 RUN ERC INS SD P/S ERH M/S RD TS LNK RUN ERC INS ...
- マニュアル
...these specifications can be connected. Connector Pin Assignments Pin assignments for the RS-232C port are given in the following table. Pin 1 6 9 5 Abbreviation Name Direction 1 FG Field ground --- 2 SD...
- マニュアル
... Communications Section 8-2 The connections between the C200HX/HG/HE and a personal computer are illustrated below as an example. C200HX/HG/HE Personal computer Signal Pin No. Pin No. Signal FG 1 1 – SD...
- マニュアル
...-point Transmission distance 15 m max. Interface Complies with EIA RS-232C Connector Pin Assignment Connectors Specification Pin No. Signal name Abbreviation Signal direction 1 Safety ground FG – 2 Send data ...
- マニュアル
... match the external device interface. C200H-ASC11/21 1 C200H-ASC31 6 9 9 6 5 5 Pin 1 Symbol Name Direction Frame ground Comments 1 FG - 2 SD Send data Output 3 RD Receive data Input 4 RTS Request to send Output 5 CTS Clear to send Input 6 - Not used - Only for terminal port of C200H-ASC31. 5V 5V output Output Other ports 7 DSR Data set ready Input 8 DTR Data terminal ready Output 9 SG Signal ground - Hood FG Frame ground - RS-232C Interface Specifications Item Specifications Electrical characteristics Conform to EIA RS-232C Synchronization...
- マニュアル
... CJ-series PLCs, one for the C200HX/HG/HE PLC, and one for CQM1H-series PLCs. Item Model Specifications CJ1W-CLK23 CJ1W-CLK21-V1 CS1W-CLK23 CS1W-CLK21-V1 External appearance C200HW-CLK21 CLK21 RUN ERC INS ...
- マニュアル
...-sub connector (female) IBM PC/AT or compatible Connect as shown below. Connector for the personal computer IBM PC/AT Computer Female 25-pin CV500-CIF01 Female 25-pin RS-232C Connector Computer 2 SD 3 ...
- マニュアル
... for the personal computer 24 Connecting the Teaching Box Section 3-2 Wire the following. RS-232C MC Unit side (20 pins) Personal computer side (9 pins) 1 Connector hood 2 RD 2 3 SD 3 7 RS 4 8 CS 5 5 SG 6 6 DR 7 4 ER Connector hood 8 9 10 11 12 Shielded wires (see note) 13 14 15 16 17 18 19 20 Note Connect the shielded line to the FG (pin 1) at the computer, and to the connector hood at the MC Unit. 3-2 Connecting the Teaching Box The procedure ...