全 5559 件が検索されました。(1381 - 1400件を表示)

  • カタログ

    ...No 100-125 VAC 24-48 VAC 48-125 VAC Model J76KC-RC-1 J76KC-RC-2 J76KC-RC-3 Yes J76KC-RC-N-1 J76KC-RC-N-2 Insulation stop Model Minimum order (bag) J77KC-K 1 (30 pcs./bag) 3 J7KCA Series Ratings/Specifications Coil rating AC operated Rated voltage Displayed model 50 Hz Allowable voltage range 60 Hz 50 Hz 60 Hz AC 24 24 VAC 24-26 VAC 21-27 VAC 21-29 VAC AC 48 48 VAC 48-52 VAC 41-53 VAC 41-58 VAC AC 100 100 VAC 100-110 VAC 85-110 ...

  • カタログ

    ...) J7MC-3R-16 20 (14-20) J7MC-3R-20 Options (Order Separately) Auxiliary contact unit Model Auxiliary contact J73MC-W-10 SPST-1NO J73MC-W-01 SPST-1NC Alarm contact unit Model Auxiliary contact J73MC-K-10 SPST-1NO J73MC-...

  • カタログ

    ...-9 A J7TC-01-9 7-10.5 A J7TC-01-10 9-13 A J7TC-01-13 Accessories (Order Separately) Insulation stop Model Minimum order (bag) J77KC-T (for main circuit) 1 (30 pcs./bag) J77KC-K (for auxiliary circuit) Removal tool Model J78KC For selection of J7TC for each motor capacity, refer to the following table. 3-phase standard motor capacity and full load current (reference values) Main circuit voltage 200-240 VAC 380-440 VAC Setting current range [A] Thermal overload relay model Capacity [kW] Current [A] 0.1 0.68 0.48-0.72 J7TC-...

  • カタログ

    ...例 ●CTが1個の場合(R2ケースの例です) R S T パレットスイッチ CB 引きはずし用電源 TC PT a2 K L CM2 b2 a1 a11 P3 OCR C1 C2 P1 P2 CT 負荷側 注. 配線時は極性にご注意ください。 CB :しゃ断器 TC :しゃ断器トリップコイル PS :しゃ断器パレットスイッチ...

  • カタログ

    ... current 0 to 20mA K3CV-1ADIB-IL3 Main Unit Fixture* K3CV-F-2 Analog voltage 0 to 10V K3CV-1ADVA-IL3 DIN Track Mounting Adapter K3CV-F-3 Analog voltage -10 to 10V K3CV-1ADVB-IL3 K thermocouple -20.0 to 500.0 ℃ K3CV-1TCKA-IL3 Thermocouples Resistance temperature detector Resistance temperature detector: -200.0 to 500.0 ° C •K3CV-F-2 fixture can only be used with our IO-Link Master Units NXR-ILM08C-EIT/NXR-ILM08C-ECT. K3CV-1PTPA-IL3 QR code is the registered trademark of DENSO WAVE. is a trademark or registered trademark of OMRON ...

  • カタログ

    ... Input TC Thermocouple PT Resistance thermometer detector IA Analog current 4 to 20 mA IB Analog current 0 to 20 mA VA Analog voltage 0 to 10 V VB Analog voltage -10 to 10 V KA K Thermocouple -20.0 to 500.0°C PA Resistance temperature detector: -200.0 to 500.0°C IL3 IO-Link (COM3) List of Models Number of channels Input Type Analog Input 1 Input type details Communications method Model Analog current 4 to 20 mA K3CV-1ADIA-IL3 Analog current 0 to 20 mA K3CV-1ADIB-IL3 Analog voltage 0 to 10 V...

  • カタログ

    ...アナログ電圧 0 ~ 10V 熱電対 名称 形式 形式 K3CV-F-1 * K3CV-F-2 DIN レール取付アダプタ K3CV-F-3 K3CV-1ADVB-IL3 K 熱電対 -20.0 ~ 500.0 ℃ 測温抵抗体 -200.0~500.0℃ K3CV-1TCKA-IL3 設定方法 など 詳細に関しては K3CV-1PTPA-IL3 当 社サイトをご覧ください *本 体 固 定 具 (K3CV-F-2) は 弊 社 製の ...

  • カタログ

    ...0 to 20 mA DC, 4 to 20 mA DC Outputs Outputs relay or transistor outputs. There is also a PASS output for models with transistor outputs. C-A 0 to 5 VDC, 1 to 5 VDC, 0 to 10 VDC I,K-L I,J,K-L 6 K3GN ■ Block Diagram Key Analog input terminal Display Transistor output (See note 1.) A/D conversion circuit Input circuit Drive circuit Output circuit Drive circuit EEPROM Microcomputer Communications terminal (See note 4.) Communications driver Drive circuit Waveform rectification circuit Control input circuit Contact output (See note 3.) X Output circuit Drive ...

  • カタログ

    ...Characteristics Indication accuracy (at 23±5°C) (See note.) Thermocouple: (±0.5% of indication value or ±1°C, whichever greater) ±1 digit max. Platinum-resistance thermometer: (±0.5% of indication value or ±1°C, whichever greater) ±1 digit max. Input Thermocouple: ...

  • カタログ

    ...XS6W-6LSZH8SS100CM-Y 2 XS6W-6LSZH8SS200CM-Y 3 XS6W-6LSZH8SS300CM-Y 5 Cable with Connectors on Both Ends (RJ45/RJ45) Rugged RJ45 plug type *1 Cable color: Light blue Model XS6W-6LSZH8SS500CM-Y 0.3 XS5W-T421-AMD-...

  • カタログ

    ...Cable length (m) Model 0.3 XS6W-6LSZH8SS30CM-Y 0.5 XS6W-6LSZH8SS50CM-Y 1 XS6W-6LSZH8SS100CM-Y 2 XS6W-6LSZH8SS200CM-Y 3 XS6W-6LSZH8SS300CM-Y 5 XS6W-6LSZH8SS500CM-Y 0.3 XS5W-T421-AMD-K 0.5 XS5W-T421-BMD-...

  • カタログ

    ... 1: Phase-R 3-phase 3-wire (3P3W2M) connection: Current input 1: Phase-R, Current input 2: Phase-T 3-phase 4-wire (3P4W) connection: Current input 1: Phase-R, current input 2: Phase-S, current input 3: Phase-T Special CT installation orientation ...

  • カタログ

    ...[N235-E1-04] K7DD Catalog Advanced Motor Condition Monitoring Device K 7DD Capture a wide variety of abnormalities affecting motor equipment to minimize unplanned downtime Implementing a new strategy of automated condition monitoring to maximize maintenance resources Manufacturing sites must respond to the rapidly changing times. OMRON is working to digitalize factories with the aim of ensuring highly mobile production that can react to such changes. We propose a new form of maintenance that watches all kinds of production facilities and equipment without relying on human senses. Developing a people-friendly style of Condition Based Maintenance Reactive maintenance has ...

  • カタログ

    ... function None Buffer 97 bytes Send wait time 0 to 99 ms Protocol CompoWay/F and Modbus RTU 5 K7GE-MG Nomenclature Front Section Main Unit K7GE-MGM Probe Unit K7GE-MG1 (A) (B) (K) (C) (J) (I) (D) (E) (H) Symbol (G) (N) (F) Name Operation (A) Alarm output indicator Displays the alarm judgment results of automatic measurement in three colors. Green: Normal, Yellow: Warning (Alarm 1 occurrence), Red: Critical (Alarm 2 occurrence) If the status is different across multiple channels, the display color is decided in the priority order of red (critical) > yellow (warning) > green (normal). (B)...

  • カタログ

    ...[N226-E1-04] K7GE Catalog Insulation resistance monitoring device K 7GE Continuous remote monitoring of insulation resistance on equipment to prevent unplanned downtime Preventing unexpected equipment stoppage and electric shock accidents due to "insulation degradation" Understanding the trend of insulation resistance degradation in equipment is ideal to prevent facilities stoppages and electrical shock accidents. However in reality, it is difficult to secure experienced maintenance personnel and make the time to visit the site and measure it manually. Conventional insulation resistance measurements requires an equipment shutdown, disconnection of power, and a skilled maintenance worker. OMRON is introducing a more efficient ...

  • カタログ

    .... When you use a flat wire, refer to the outline dimensional drawing of the relevant CT and use a CT with a larger diameter. However, use the CT within the range of its rated current. 5 K7TM Nomenclature Front Section (A) (...

  • カタログ

    ...[N229-E1-03] K7TM Catalog Heater Condition Monitoring Device K 7 TM Monitor Heater Condition with the K7TM To reduce unexpected downtown and wasteful costs due to heater burnout Heater equipment that operates at high temperatures is more likely to experience unplanned downtime due to heater burnout. Preventing burnout requires the heater's condition to be monitored, which was previously a time consuming and costly task, which can now be automated with the K7TM. Issues concerning heater burnout Downtime resulting from heater replacement and warm up is time consuming Temperature Time As the heater burns out, production fallout will ...

  • カタログ

    ...Sensor inputs 100 to 240 VAC 50/60 Hz 24 VAC 50/60 Hz or 24 VDC 85% to 110% of power supply voltage 5 VA max. 2 W max. (24 VDC), 4 VA max. (24 VAC) K8AK-TH11S Thermocouple: K, J, T, E; Platinum-resistance thermometer: Pt100, Pt1000 K8AK-TH12S Thermocouple: ...

  • カタログ

    ... occur if the input is connected to unused terminals and the Unit will not operate correctly. For the K8DT-AS3, the I1 terminal is not used. For the K8DT-AS2, the I3 terminal is not used. If using the OMRON K8AC-CT200L CT, connect to terminals ...

  • カタログ

    ... occur if the input is connected to unused terminals and the Unit will not operate correctly. For the K8DT-AW3, the I1 terminal is not used. For the K8DT-AW2, the I3 terminal is not used. If using the OMRON K8AC-CT200L CT, connect to terminals ...