全 96 件が検索されました。(81 - 96件を表示)
- マニュアル
... command 2. Description The specified axis will be moved for the specified distance for positioning after general input 1 or 2 is turned ON. Refer to the following examples. Example 1: Speed command 2 is not specified with the following format. G31 X100 ...
- マニュアル
...-s Protocolforcontrol‖ngaES100「「emperatureControllerviathePSB.Proceduresforwritingadlustmentparameters,readingoperationamounts,andw耐ng/readingoperatingparameters. Dig麓alPanelMeter ProtocolforcontrollingaDigitalPanelMeterviathePSB.Proceduresforw蘭ngcomparisonvaluesandreadingdisplayvaluesareset. V500〈1520BarCodeReader Protoco{forcontro川ngaBarCodeReaderviathePSB.Pr◎ceduresforcontrollingtheBarCodeReaderinremotemode,readingthedatathathasbeenreadbytheBarCodeReade陥andreading/w商ngoperatingParameters. 3Z4LLaserMicrometer Prot◎colforcontrollmgaLaserMicrometerviathePSB.Pr◎ceduresforcontro川ngtheLaserMcrometerinremotemode,readingmeasureddata,andwri肋g!readingoperatingparameters. ...
- マニュアル
... devices for which standard system protocols are provided are listed below. For details, refer to 5-7 Using Protocol Macros. Digital Controllers (E5@K, ES100@), Temperature Controllers (E5ZE, E5@J), Intelligent Signal Processors (K3T@), Bar Code Readers (V500/ V520), Laser Micrometers (3Z4L), Visual Inspection Units (...
- マニュアル
... set in the allocated words in the DM Area for every four inputs. The measurable data range is ±20 digits wider than the sensor input range. Setting °C Input 16-bit binary °F BCD F@@@ indicates minus sign. ...
- マニュアル
... the drives has a torque bigger than 200% we set a bit ;in an output variable (for PLC control) IF #MW0000>0; #OB0BA20=1; ENDIF; WED; JOINT; ;Pick and place sequence: ; - Go to 'pick piece' position MOVEL[J01]500 [J02]300 ...
- マニュアル
...and related sections before attempting any of the procedures or operations given. ix SECTION 1 Features OMRON’s unique system architecture has achieved real-time visual measurement capabilities. 3Z4SP-C23/-C23-US Visual Positioning Controller Video monitor Programmable Controller ...
- マニュアル
... read will not include decimals. Refer to the following examples: • For a Pt 100W input (–99.9° to 450.0°C), the lower limit is F999 and the upper limit is 4500. • For a K thermocouple input (–200 to 1,300°C), the lower limit is ...
- マニュアル
... to 240 VAC) F350-C41E IMP Unit Power Supply Unit Processes images. Supplies power to the entire system. KF300-FM2 MMI Unit Provides Memory Card functions and menu operations via a Video Monitor and Console. KF300-KP Console (Note: The ...
- マニュアル
... 120 VAC) K F300-P2E (200 to 240 VAC) Power Supply Unit Supplies power to the entire system. KF300-FM2 MMI Unit Provides Memory Card functions and menu operations via a Video Monitor and Console. KF300-KP Console (Note: The ...
- マニュアル
.... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 45 5-5 F200/F300 Camera Parameters . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 63 5-6 Connecting a Strobe Device . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 64 Index. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 67 Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 69 vii About this Manual: This manual describes the hardware for the F160 Vision Sensor and how to install the components, and it includes the sections described below. This is one of four manuals used to operate the F160. Refer to the following table for the contents of each manual. Manual Contents Cat. No. 1: Setup Manual Provides information on system hardware and installation. Be sure to read this manual first. 2: Conversational Menu Operation Manual Describes operation of the ...
- マニュアル
.... 3. If using Intelligent Lighting, select the model. 4. Select End. The settings will be registered and the System Settings Screen will return. CHECK If Other is selected under Camera, the Camera Settings (Detail) Screen will be displayed. The settings for ...
- マニュアル
.... 3. If using Intelligent Lighting, select the model. 4. Select End. The settings will be registered and the System Settings Screen will return. CHECK If Other is selected under Camera, the Camera Settings (Detail) Screen will be displayed. The settings for ...
- マニュアル
... shutter trigger pulse. Camera 0 tD Camera 1 ( : Shutter trigger pulse turns ON) Other Cameras The timing is synchronized. There is no displacement time. Can more than one internally synchronized Camera be connected? No. Only one internally synchronized Camera (...
- マニュアル
.... 3. If using Intelligent Lighting, select the model. 4. Select End. The settings will be registered and the System Settings Screen will return. CHECK If Other is selected under Camera, the Camera Settings (Detail) Screen will be displayed. The settings for ...
- マニュアル
.... 3. If using Intelligent Lighting, select the model. 4. Select End. The settings will be registered and the System Settings Screen will return. CHECK If Other is selected under Camera, the Camera Settings (Detail) Screen will be displayed. The settings for ...
... チャネル±10V または 4~20mA 12 ビット A/D コンバータボード黒の正面、上部、下部プレート、ねじ、2 カードガイド 3-4027A-00-0100-F200 上記と同じ、ただし黒の正面プレートのみ 3-4027A-00-0200-B200 16 チャネル±10V または 4~20mA 16 ビット A/D コンバータボード黒...