全 96 件が検索されました。(41 - 60件を表示)

  • マニュアル

    ...、位置決めします。 以下にいくつかの例を示しながら詳細を説明します。 (例1)速度指令2を指定しない場合 G31 X100 F200 (単位は、[mm]とします) 汎用入力1 X軸速度 200 速度制御 位置制御 (100mm移動) 時間 0 汎用入力1がONするまでは、200[mm/s]でX軸を...

  • マニュアル

    ...た。 アンプユニットと仕様上接続可能な形式・バージョンのセンサヘッドを接続してください。 Error-09 4-2 0x7FFF F200 • 画面表示に従って設定初期化を行ってください。 工場出荷設定初期化コマンドを通信ユニット経由で送ってください。 ZP シリ...

  • マニュアル

    ...H' 00000000 H' 00000000 H' 00000000 H' 00000000 H' 00000000 H' 00000000 H' 00000000 H' 00000000 H' 00000000 H' 00000000 H' 00000000 H' 00000000 H' 00000000 ( 対象 TC4/2 HFU 単位 F200 G3ZA3-CH1 演算勾配値 ~ ~ 0400 G3ZA1-CH1ソフトアップ時間 G3ZA1-CH2ソフトアップ時間 G3ZA1-CH3ソフトアップ時間 G3ZA1-CH4ソフトアップ時間 G3ZA1-CH5ソフトアップ時間 G3ZA1-CH6ソフトアップ...

  • マニュアル

    ...Fiber length (m) Band vs. Fiber Length The following equation expresses the baseband frequency characteristics f(L) in MHz for a given fiber length (L) in km. f(L) = 14.5×L–0.89 MHz (for 0.85 mm, NA=0.4, and spot size ...

  • マニュアル

    ...CT 0 overflow Loop 2 status data 0 Sensor error CT 0 overflow Note For four-digit BCD and platinum resistance thermometer data, the least significant digit = 0.1, and the most significant digit (F) = minus (–). For example, “...

  • マニュアル

    ...CTover・fbW O 0 RUN o O Coolingout-put HeaATtingout・put 04 03 02 01 0 LoOPlRUN Note SW2・1inNormalPosition Forfour-digitBCDandplatinumresistancethermometerdata,theleast significantdigit=O.1,andthemostsignificantdigit(F)=minus(一).Forexample, "...

  • マニュアル

    ...E5ZE Temperature Controller Reads D E5ZE Temperature Controller Writes E E5J Temperature Controllers F ES100 Digital Controllers Appendix Contents G K3T Intelligent Signal Processors H V500/V520 Bar Code Readers I 3Z4L Laser Micrometer J ...

  • マニュアル

    ... be specified. Specify the total number of words to which data is written. Example: Set C to CC07 and D to F002 to write the maximum count value of counter 1 in circular mode to words m+7 and m+8. Control Codes F100, ...

  • マニュアル

    ... command 2. Description The specified axis will be moved for the specified distance for positioning after general input 1 or 2 is turned ON. Refer to the following examples. Example 1: Speed command 2 is not specified with the following format. G31 X100 ...

  • マニュアル

    ... set in the allocated words in the DM Area for every four inputs. The measurable data range is ±20 digits wider than the sensor input range. Setting °C Input 16-bit binary °F BCD F@@@ indicates minus sign. ...

  • マニュアル

    ... Unit. Example Sensor input K: −200 to 1,300°C Select ON/OFF Control or PID Control Data storage/display format Binary (4-digit hexadecimal) 4-digit BCD FF38 to FFFF to 0514 (−200 to −1 to 1,300) F200 to 1300 (−200 to 1,300) A switch on the front of the Unit (pin 6 of the DIP switch) selects whether the Temperature Control Unit operates with ON/OFF control or PID control with 2 degrees of freedom. Note The setting on pin 6 sets the control method for all of the Unit’s control loops. The factory ...

  • マニュアル

    ... the drives has a torque bigger than 200% we set a bit ;in an output variable (for PLC control) IF #MW0000>0; #OB0BA20=1; ENDIF; WED; JOINT; ;Pick and place sequence: ; - Go to 'pick piece' position MOVEL[J01]500 [J02]300 ...

  • マニュアル

    ...(INT) Select (INT) UnitNo (INT) LoopNo (INT) SP When Input Type Switch Is Set to 4 Unit Set for Binary Data (Pin 3 of DIP Switch) –200 Unit Set for BCD Data (Pin 3 of DIP Switch) #F200 Related manuals 3-544 Temperature Control Unit Operation Manual (W396) 2-1-3 Input Specifications 3-7 Setting the Set Point (BOOL) ENO 3-16 ■ Variable Tables Input Variables Name EN Variable name EN Data type BOOL Default Range Model selection Select INT &2 &2, &4 Unit No. Loop No. Set point UnitNo LoopNo SP INT INT INT &0 &1 &0 &...

  • マニュアル

    ...off while setting data was being saved to the Amplifier Unit. Correction Initialize the settings according to the instructions on the display. • Execute the initialization command to restore the factory defaults via the Communication Unit. 0x7FFF ...

  • ..._8DO_24VDC_0_process_value_Ch8_7000_08 BOOL 9 6.EtherCAT Settings ■Input area (BL20 ECO Gateway to Controller) Device variable name Data type E001_Mapping_RxPDO_Device_Contro_Device_Control_Word_ UINT Meaning Not used (System reserved) ...

  • ... starting from “001”. For slave units with module configurations, the default device names are "M" followed by a sequential number starting from "1". ■E001: UR20-FBC-EC output area (Controller to u-remote) Data type Bit E001_Mapping_RxPDO_Device_Contro_Controlbit_0_...

  • ...らの連番」です。 ■E001:UR20-FBC-EC 出力エリア(コントローラ → u-remote) デバイス変数名 データ型 内容 Bit E001_Mapping_RxPDO_Device_Contro_Controlbit_0_F200_01 BOOL 0 Controlbit 0 E001_Mapping_RxPDO_Device_Contro_Controlbit_1_...

  • ...入力エリア(コントローラ←BL20 ECO ゲートウェイ) デバイス変数名 意味 データ型 E001_Mapping_RxPDO_Device_Contro_Device_Control_Word_ UINT 未使用 F200_01 (システム予約) E001_Mapping_TxPDO_Device_Status_Summarized_module_d BOOL iagnosis_F100_01 E001_Mapping_TxPDO_Device_Status_Diagnosis_message_av BOOL Diagnosis message available At least one module has a diagnostic message. The Diagnosis History Object contains a new message. ailable_F100_02 E001_Mapping_TxPDO_Device_Status_...

  • 生産終了品/推奨代替品

    ...替品 備考 位置決め用視覚認識装置用カメラ 3Z4SP-S1-A 1994年6月 生産終了 生産終了案内 視覚認識装置 カメラ F200-S 2002年9月 推奨代替品は生産終了 関連情報...

  • マニュアル

    ...の小数点位置に注意してください。 Ptセンサ入力(-99.9--450.0℃)の場合……下限:"F999"、上限:"4500" K熱電対入力(-200--1,300℃)の場合……下限:"F200"、上限:"1300" (7}測定値読み出し測定値(PV)とステータスデータの読み出しを行います。 ■コマンドフォーマット @ llユニットNo.RX×1011×1001...