全 84 件が検索されました。(81 - 84件を表示)

  • マニュアル

    ... only be written in whole bytes and 2 hexadecimal characters make up one byte. Up to 256 characters can be entered. Set the communication protocol of the Hand-held Reader Writer with its DIP switch to match the protocol of the host computer. 10 ...

  • マニュアル

    ...130 140 150 160 170 180 190 200 210 220 230 240 250 260 270 280 290 300 310 320 330 340 ’***** V670-CD1D SAMPLE PROGRAM ***** CLS OPEN “COM:E73NN” AS #1 ’ ’***** MAIN LOOP **** *LOOP LINE INPUT “Input TX Data : “, ITD$ TXD$=ITD$+”*”+CHR$(13) PRINT “[TX] : “;ITD$ PRINT #1,TXD$; GOSUB *RECEIVE PRINT “[RX] : “;REC$ GOTO *LOOP ’ ’***** RECEIVE DATA ***** *RECEIVE RXD$=” “ WHILE (LOC(#1)=0):WEND WHILE (INSTR(RXD$,”*”+CHR$(13))=0) RXD$=RXD$+INPUT$(1,#1) WEND REC$=LEFT$(RXD$,LEN(RXD$)-2) RETRUN ’ END ’Opens a RS-232C port. ’Inputs a command data. ’Sets a data string ...

  • マニュアル

    ...DR 6 Green SD CS 7 Red VCC RS 8 Black S.GND - 9 Shield F.GND Shield Cover 5VDC (Supplied from outside) 0V Example of BASIC program 100 CLS 110 CLOSE #1 120 OPEN "COM:N81NN" AS #1 130 BCDATA$="" 140 AA$=INPUT$(1,#1) 150 IF AA$=CHR$(&H03) GOTO 170 160 BCDATA$=BCDATA$+AA$:GOTO 140 170 PRINT "READ DATA=" ; BCDATA$ 180 GOTO 130 88 Signal name V500-R521B2/C2 User’s Manual V500-R521.book 89 ページ 2008年7月18日 金曜日 午後1時1分 Section 5...

  • マニュアル

    ... strings as character strings type exceeds 255 characters. Syntax error is occurred when you specify wrong formatting; typographical error of macro function's name, no comma or no spaces. Usage Cautions None. Example Rem Close the Console Window. shell "cmd.exe /C ...