全 80 件が検索されました。(61 - 80件を表示)
- マニュアル
... computer to read and display the 94 Section 1-9 Communications Functions data received from the PC while a host link read command is being executed to read data from the PC. 10 ’CQM1 SAMPLE PROGRAM FOR EXCEPTION 20 CLOSE 1 30 ...
- マニュアル
... to receive the data. This program allows the computer to read and display the data received from the PC while a host link read command is being executed to read data from the PC. 10 ’C200HS SAMPLE PROGRAM FOR EXCEPTION 20 CLOSE 1 30 ...
- マニュアル
...the data. This program allows the computer to read and display the data received from the ID Controller while a host link read command is being executed to read data from the ID Controller. 10 ’IDSC SAMPLE PROGRAM FOR EXCEPTION 20 CLOSE 1 30 ...
- マニュアル
...144 CLEAR CLEAR Initializes numeric and character variables and closes all ports. CLNG CLNG (numeric expression) Converts a value to a long integer. CLOSE CLOSE [#port number] Closes a port. Device control 145 ...
- マニュアル
...receive the data. This program allows the computer to read and display the data received from the PC while a Host Link read command is being executed to read data from the PC. 10 ’CQM1H SAMPLE PROGRAM FOR EXCEPTION 20 CLOSE 1 30 ...
- マニュアル
... to 07FFH, and the write data in two-character units, up to 256 characters. Be sure to correctly set the ID Controller communications format by setting its DIP switches to conform to the communications format with the host computer to which it is connected. ...
- マニュアル
...Downloads measurement parameters DATAUP Uploads measurement parameters FLIST Lists functions MENU Return to menu mode WAIT Pauses program for a certain duration AUTO Automatically assigns a line number to each program line CLEAR Clears all variables ...
- マニュアル
... 255, the system regards it as 255. Comments ––– Reference CIRCLE, LINE, POLYGON, PSET Sample Program The system will draw a rectangle whose diagonal points are (100, 50) and (200, 150) on the Paint window screen (OVL–2). 10 DISPLAY 14 20 ...
- マニュアル
... setting> 1100 GOSUB *MDAT
1110 GOSUB *COMM 1120 GOSUB *DISP 1130 GOSUB *QUIT 1140 END End 1150 ’************************************************ 1160 ’* * 1170 ’************************************************ 1180 *INIT 1190 ... - マニュアル
... *MAIN 1090 GOSUB *INIT
1100 GOSUB *MDAT 1110 GOSUB *COMM 1120 GOSUB *DISP 1130 GOSUB *QUIT 1140 IF FRG=0 THEN GOTO 1170 End judgment 1150 ... - マニュアル
... 2-digit HEX characters. The total character length of the write data must be 256 or less. Set the communication format of the ID Controller by using the DIP switches in accordance with the communication system of the host computer to be used. 10 ...
- マニュアル
... can only be written in whole bytes and 2 HEX characters make up one byte. Up to 256 characters can be entered. Set the communication protocol of the R/W Head with its DIP switch to match the protocol of the host computer. 10 ...
- マニュアル
... a circle. Graphic control Command 64 CLEAR Initializes variables. Memory management Command 65 CLNG Converts to a long integer. Calculation Function 65 CLOSE Closes an open file. File control Command 65 ...
- マニュアル
...9,600 bps Data length 8 bits Parity None Stop bits 1 Delimiter CR + LF ’*********************************************************************************** ’ (c)Copyright OMRON Co.1994 ’ All Rights Reserved ’ Sample Program ’Sample Program Using the Command Response Function ’*********************************************************************************** ...
- マニュアル
...(c)Copyright OMRON Co.1995 ’ All Rights Reserved ’ Sample Program ’––––––––––––––––––––––––––––––––––––––––––––––––––––––––––– ’Sample program for saving data. ’*********************************************************** BLKDATA = 128: BLKSIZE = 132 ACK$ = CHR$(&H6): NAK$ = CHR$(&H15): SOH$ = CHR$(&H1) EOT$ = CHR$(&H4): CAN$ = CHR$(&H18) DIM DAT$(BLKDATA) ...
- マニュアル
... default setting is 0.) (mode) 0 : All variables are initialized. 1: All variables except backup variables are initialized. When the mode is set to 1, CLEAR will initialize all variables that don’t start with characters specified by the VARBACK command. 72 ...
- マニュアル
... only be written in whole bytes and 2 hexadecimal characters make up one byte. Up to 256 characters can be entered. Set the communication protocol of the Hand-held Reader Writer with its DIP switch to match the protocol of the host computer. 10 ...
- マニュアル
...130 140 150 160 170 180 190 200 210 220 230 240 250 260 270 280 290 300 310 320 330 340 ’***** V670-CD1D SAMPLE PROGRAM ***** CLS OPEN “COM:E73NN” AS #1 ’ ’***** MAIN LOOP **** *LOOP LINE INPUT “Input TX Data : “, ITD$ TXD$=ITD$+”*”+CHR$(13) PRINT “[TX] : “;ITD$ PRINT #1,TXD$; GOSUB *RECEIVE PRINT “[RX] : “;REC$ GOTO *LOOP ’ ’***** RECEIVE DATA ***** *RECEIVE RXD$=” “ WHILE (LOC(#1)=0):WEND WHILE (INSTR(RXD$,”*”+CHR$(13))=0) RXD$=RXD$+INPUT$(1,#1) WEND REC$=LEFT$(RXD$,LEN(RXD$)-2) RETRUN ’ END ’Opens a RS-232C port. ’Inputs a command data. ’Sets a data string ...
- マニュアル
...DR 6 Green SD CS 7 Red VCC RS 8 Black S.GND - 9 Shield F.GND Shield Cover 5VDC (Supplied from outside) 0V Example of BASIC program 100 CLS 110 CLOSE #1 120 OPEN "COM:N81NN" AS #1 130 BCDATA$="" 140 AA$=INPUT$(1,#1) 150 IF AA$=CHR$(&H03) GOTO 170 160 BCDATA$=BCDATA$+AA$:GOTO 140 170 PRINT "READ DATA=" ; BCDATA$ 180 GOTO 130 88 Signal name V500-R521B2/C2 User’s Manual V500-R521.book 89 ページ 2008年7月18日 金曜日 午後1時1分 Section 5...
- マニュアル
... strings as character strings type exceeds 255 characters. Syntax error is occurred when you specify wrong formatting; typographical error of macro function's name, no comma or no spaces. Usage Cautions None. Example Rem Close the Console Window. shell "cmd.exe /C ...