全 2903 件が検索されました。(941 - 960件を表示)
- マニュアル
... mit Spannung oder mit anderen nicht dafür vorgesehenen Signalen. Andererseits würde der interne Schaltkreis des Zeitrelaiseinganges beschädigt. (14) Da der H3CR-H einen hochohmigen Eingangsschaltkreis hat, kann die Rückstellung durch Interferenzen, wegen induzierter Spannung, gestört weden. Um diese Störung zu vermeiden verdrahten Sie die Eingänge ...
- マニュアル
... to within the specified allowable range. (8) If a voltage that exceeds the rating is applied, internal components may be destroyed. (9) Wire all terminals correctly. (10) Do not wire the terminals which are not used. (11) Install and clearly label a switch or circuit breaker ...
- マニュアル
... to within the specified allowable range. (8) If a voltage that exceeds the rating is applied, internal components may be destroyed. (9) Wire all terminals correctly. (10) Do not wire the terminals which are not used. (11) Install and clearly label a switch or circuit breaker ...
- マニュアル
...[3616495-0A] H5CC-AWSD デジタルタイマ 取扱説明書(日/英語) SAFETY PRECAUTIONS CAUTION Do not allow pieces of metal, wire clippings, or fine metallic shavings or fillings from installation to enter the product. Doing ...
- マニュアル
...[3616492-6A] H5CC デジタルタイマ 取扱説明書(日/英語) Precautions for Safe Use 1) When mounting the Timer to a panel, tighten the two mounting screws alternately, a little at a time, so as to keep them at an equal tightness. If the panel screws are tightened unequally, water may enter the panel. indicator LEDs, LCD, and resin parts may deteriorate more quickly depending on the application environment, preventing normal indications. Periodic inspection and replacement are required. 21) The waterproof packing may deteriorate, shrink, or harden depending on the application...
- マニュアル
...CAUTION result property damage,or faulty operation. ● Graphic symbol ●Warning against electric shocks Notification of possible electric shocks under certain conditions. ●General warning Notification of general, unspecified prohibition items. ●Prohibition against disassembly Notification of disassembly of products, when doing ...
- マニュアル
...CAUTION could injury, property damage, or faulty operation. -1- Graphic symbol Warning against electric shock Notification of possible electric shock under certain conditions. General warning Notification of general, unspecified prohibition items. Prohibition against disassembly Notification of disassembly of products, when doing ...
- マニュアル
... supply as the AC power supply for the Counter. Using an inverter output with an output frequency of 50/60 Hz as the power supply may cause the Counter to produce smoke or become damaged by burning. • Use a switch, relay, or other device with contacts ...
- マニュアル
... supply as the AC power supply for the Counter. Using an inverter output with an output frequency of 50/60 Hz as the power supply may cause the Counter to produce smoke or become damaged by burning. • Use a switch, relay, or other device with contacts ...
- マニュアル
...[5639664-5C] H7CC-A□ 電子カウンタ 取扱説明書(日/英語) Precautions for Safe Use Precautions for Correct Use 1) When mounting the Counter to a panel, tighten the two mounting screws alternately, a little at a time, ...
- マニュアル
...(48) P3GA-11 (order separately) Back-connecting Socket 48 7.5 89.9 Panel-cutout Dimensions Diagram (Unit: mm) Panel cutouts are as shown below. (according to DIN43700) To allow easier operation, it is recommended that Adapters be mounted ...
- マニュアル
... dangers of high-voltage equipment. S Precautions on touching the terminals of the product even after power has been turned OFF. (These terminals are live even with the power turned OFF.) 5. Do not perform withstand voltage or other megameter tests on the product. Doing ...
- マニュアル
... AC Servomotors described in this manual are defined as looking at the end of the output shaft of the motor as follows: counterclockwise rotation is positive and clockwise rotation is negative. 7. Do not perform withstand-voltage or other megameter tests on the product. Doing ...
- マニュアル
... in place as specified before using the product. Consult your OMRON representative when using the product after a long period of storage. WARNING Always connect the frame ground terminals of the Servo Drive and the Servomotor to 100 or less. Not doing ...
- マニュアル
... manual contains information you need to know to correctly use the Servo Drive and peripheral equipment. Before using the Servo Drive, read this manual and gain a full understanding of the information provided herein. After you finished reading the manual, keep it in a convenient place ...
- マニュアル
... you need to know to correctly use the OMNUC G5 Series and peripheral equipment. Before using the OMNUC G5 Series, read through this manual and gain a full understanding of the information provided herein. After you finished reading the manual, keep it in a convenient place ...
- マニュアル
... protection Install the latest commercial-quality antivirus software on the computer connected to the control system and maintain to keep the software up-to-date. Security measures to prevent unauthorized access Take the following measures to prevent unauthorized access to our products. • Install physical controls ...
- マニュアル
... systems and facilities. Notice This manual contains information you need to know to use the DriveProgramming. Before using this product, read this manual and gain a full understanding of the information provided herein. After you finished reading this manual, keep it in a convenient place ...
- マニュアル
... correctly use the CompoNet Communications Unit (Model: 3G3AX-MX2-CRT-E/3G3AX-RX-CRT-E). Before using the CompoNet Communications Unit, read this manual and gain a full understanding of the information provided herein. After you finished reading this manual, keep it in a convenient place ...
- マニュアル
... there are differences, such as in dimensions and work envelopes, the different models will be covered separately. Figure 1-1. eCobra 800 Robot By adding a SmartController EX or a PLC, the eCobra series robots replace the previous sCobra and Cobra ePLC series robots, ...