全 387 件が検索されました。(61 - 80件を表示)

  • ...-BAT* CJ1W-CIF11* CJ1W-CIF21* CJ1W-CLK*/ -COR*/ -CRM*/ -DRM*/ -EIP*/-ETN*/ -FLN*/ -MCH*/ -NCF*/ -NC271*/-NC281*/ -NC471*/ -NC48*/ -NC88* CJ1W-CM* CJ1W-MAD* CJ1W-PA*/-PD* CJ1W-PRM*/ -PRT*/ -SCU* CJ1W-SP001* CJ1W-SPU*/ -SRM* CJ1W-...

  • サポート

    ...化の過程や摩擦の結果として耐用寿命の終末付近で発生するもので、時間の経過と共に急激に増加します。 図1のtb点を指すもので、tb点はPLC・ユニット毎に異なります。 3項にPLCの耐用年数の考え方を説明致します。 図1: 故障発生率 初...

  • サポート

    ...化の過程や摩擦の結果として耐用年数の終末付近で発生するもので、時間の経過と共に急激に増加します。 図1のtb点を指すもので、tb点はPT毎に異なります。 3項にPTの耐用年数の考え方を説明致します。 図1: 故障発生率 初期故障期...

  • カタログ

    ... 61F Controller’s NC contacts turn ON, the output contacts have already switched. Thus, only the continuous carry current needs to be considered for the load capacity of the 61F-AN, enabling application to the rated carry current of 3 A. Ta 61F ...

  • カタログ

    .... This state is held with a magnetic lock even if the power supply is turned OFF. • The above operation is repeated each time the power supply is turned ON. (Power Supply Pulse Response Method) Ta 61F Connections (Refer to connection diagram) ...

  • カタログ

    ... and is reset when current flows between the poles. Wiring is the same as for models with sequential operation. 3 61F-G@ Internal Circuit Diagrams The schematic diagrams shown below typify the internal connections of the various 61F models. The designations Ta, ...

  • カタログ

    ... and is reset when current flows between the poles. Wiring is the same as for models with sequential operation. 3 61F-G@ Internal Circuit Diagrams The schematic diagrams shown below typify the internal connections of the various 61F models. The designations Ta, ...

  • カタログ

    ...,000 operations min. Mechanical: 10,000,000 operations min. Weight GN models: 315 g; G1N, G2N, IN models: 410 g; G3N models: 625g; G4N models: 870 g Internal Circuit Diagrams Example: 61F-GN S2 Example: 61F-GNL S2 S0 S1 ...

  • カタログ

    ...,000 operations min. Mechanical: 10,000,000 operations min. Weight GN models: 315 g; G1N, G2N, IN models: 410 g; G3N models: 625g; G4N models: 870 g Internal Circuit Diagrams Example: 61F-GN S2 Example: 61F-GNL S2 S0 S1 ...

  • カタログ

    ...Note: To apply self-hold, short circuit between 5 and 6, and use 7 as E2. Power circuit Output circuit Control circuit 8 7 3 4 2 3 S0 S1 E3 E2 E1 Ta Tc Tb S0 S1 E3 E1 Ta1 Tc1 Tb1 Ta2 Tc2 Tb2 5 6 1 61F-LS-CP08-A 4 5 11 10 1 7 6 8 100 to 240 VAC Power circuit Power circuit Control circuit Control circuit 8 7 3 4 2 3 E1 Ta Tc ...

  • カタログ

    ... current is at DC micro-current level. Moreover, the Electrodes will corrode rapidly if the current is allowed to constantly flow between the Electrodes. Be careful with the electrode polarity and grounding when wiring. 1 61F-UHS/-HSL Internal Circuit Diagrams 61F-UHS ...

  • カタログ

    ... current is at DC micro-current level. Moreover, the Electrodes will corrode rapidly if the current is allowed to constantly flow between the Electrodes. Be careful with the electrode polarity and grounding when wiring. 1 61F-UHS/-HSL Internal Circuit Diagrams 61F-UHS ...

  • カタログ

    ...-CP08 61F-WL-CP11 100 to 240 VAC 100 to 240 VAC Power circuit Power circuit Control circuit Control circuit 1 7 3 4 2 3 S0 S1 E3 E1 Ta Tc Tb S0 S1 E3 E1 Ta1 Tc1 Tb1 Ta2 Tc2 Tb2 5 6 9 4 5 11 10 1 7 6 8 „Operating Principle When the two conductive cores of the Sensing Band are contacted by a liquid, a weak alternating current flows across the cores. This current is amplified to operate a relay. In practice, leakage will be detected if water drops are present between the ...

  • カタログ

    ...a 40-ms OFF-delay timer will start. E2C-AK4A 10 to 30 VDC Black NPN opencollector output OFF-delay operation terminal* 12 to 24 VDC Line 6 5 6 5 4 3 1 2 Tc Ta Tb 100 to 240 VAC Relay output Line 4 3 Shield Line Brown Black Blue Applicable Socket: P2CF-08 7 8 1 2 PNP 0 V 12 to NPN Output 24 VDC output 10 to 30 VDC NPN opencollector output 0V Note: Characteristics will change if the cable length changes. Do not cut or extend the cable. 10 E2C/E2C-H Load Connections...

  • カタログ

    .... T Incident light No incident light T T L-ON ON OFF D-ON T ON OFF Incident light No incident light L-ON ON OFF D-ON ON OFF Ta Tb Ta Tb A timer value can be set after pressing button when a timer menu (other threshold MODE display than “ Incident level Use Passing time(ms or μs) or longer to set [ ]. Send a workpiece past the Fiber Unit. Displaying the Passing Time and Difference in Incident Levels. ”) is displayed. button to set the time. UP/DOWN (1 to 9999 ms in 1 ms steps; the initial ...

  • カタログ

    ... (Ta) D-ON (Ta) Photoelectric Sensor main circuit ON OFF ON OFF ON OFF Refer to page 6 for information on Sensors with timers (T). Power Source 1 No polarity 2 3 Tb 4 Tc 5 Ta Contact output (Built-in Relay: G6C) DC SSR Output Models Model Timing chart Output circuit 24 to 240 VAC 12 to 240 VDC Power Source 1 No polarity E3JM-10S4(T)(-G)-NN(-US) E3JM-R4S4(T)(-G)(-US) E3JM-DS70S4(T)(-G)(-US) Incident light No incident light Indicator (red) * L-ON (Ta) D-ON (Ta) 2 ON OFF L/ON...

  • カタログ

    ...Incident light No incident light ON L-ON OFF ON D-ON OFF T T Incident light No incident light Ta ON L-ON OFF Ta ON D-ON OFF Tb Tb E3NX-CA Nomenclature Standard Models E3NX-CA11/CA41/CA6/CA8 NO/NC Button Used to set the external output polarity. When NO (normally open) is set, the output is ON when a workpiece is in the sensing area. When NC (normally closed) is set, the output is ON when a workpiece is not in the sensing area. NO/NC Indicator (Orange) Indicates the current NO/NC setting status....

  • カタログ

    ...Multi-sensing technology Flow rate Uses the "Thermal flow rate measurement algorithm". The sensor calculates first the flow velocity by measuring how fast the fluid cools the heated temperature measuring element Ta, and then the flow rate based on the pipe diameter. The temperature measuring element ...

  • カタログ

    ... the open-phase element, but the operating value of the overload element may vary. 3 K2CM Connections Voltage Reverse-phase Detection Models Manual Operation Low-voltage Circuit (Highcapacity Motor) Terminal Arrangement 200 VAC 50/60Hz R Ta Tc ...

  • カタログ

    ...24 VDC Protection IP40 IP65 (Oil-proof type) Ordering Information Plateau Head Indicators Degree of Protection: IP40 Flange Color: Black Type Plateau Head Indicator Flange Color: Metallic LED voltage Model 5 VDC M3U-...