全 1073 件が検索されました。(721 - 740件を表示)

  • マニュアル

    .... 98 Section 4-10 Batch Trend Screens • The trend data collection cycle and maximum save time in a Batch Trend Screen are shown in the following table. Item Collection cycle (See note.) Maximum save time Note Details 1 ...

  • マニュアル

    ... number of words, starting from the beginning word S at the remote node (node address M) is received at the words starting from the beginning word D at the local node. 15 Local node 0 Destination node number N S Command (...

  • マニュアル

    ... × hour or count × minute) Time Division width (See note.) Note The following table shows the divisions for the cumulative counter. 132 Section 5-4 Analog Input Units DRT2-AD2 Unit Hour Minute Divisions 3.6 ...

  • マニュアル

    ... to Bit Slaves using e-CON connectors, clamp terminals, or compact connectors are supplied power from the CompoNet communications power supply. No separate wiring is required for I/O power supply. Industry Standard Sensor e-CON Connectors (CRT1-V@D08S(-1)/ CRT1-@D@...

  • マニュアル

    ... within specified time When operation is started in hot start mode (ITEM018 = 0), a hot start is performed after recovering from a power interruption if the time that power is interrupted is a within the time specified in ITEM037 (Hot start enabled time: 0 to 3,600 ...

  • マニュアル

    ... Area becomes on. Analog input value Cumulated value (count hours or count minutes) 9 9-15 Monitoring the cumulated count Time Division width * These are the division widths for the cumulated count . Unit Division Hour 3.6 ...

  • マニュアル

    ...that is allocated to the STRING variable. • Upper and lower bytes are reversed. Example: The outputs will be as follows for a STRING array named s that has two elements (with the data quantity around elements is set to 4 bytes) when s[0] is “ab” and ...

  • マニュアル

    ...-blade screwdriver. Battery Charger socket Read/Write Head/Antenna connector Read/Write Head attachment hook For one-handed operation, attach the Read/Write Head here. Display LCD 20 characters x 2 lines Operation keys Read/Write Head Set V600–H06–...

  • マニュアル

    ... scene by pressing the left arrow or right arrow key.100 CLS 110 LOCATE 1, 1:PRINT ”LEVEL=” 120 LOCATE 1, 18:PRINT ”XG=” 130 LOCATE 1, 19:PRINT ”YG=” 140 S=0:CHANGE 0 150 K=KEYIN 160 IF K=4 THEN S=S+1:GOSUB 500 170 IF K=16 THEN S=...

  • マニュアル

    ...Sync system: HD/VD Input level: 2 to 5 Vp-p Input impedance: 75 Ω Image output VS: 1.0 Vp-p/75 Ω Resolution Horizontal: 570 lines min.; Vertical: 350 lines S/N ratio 56 dB Shutter speed 1/1000 s, 1/2000 ...

  • マニュアル

    ... (at 100 VDC, with internal surge absorber removed) Dielectric strength 1,000 VAC, 50/60 Hz between all DC external terminals and GR terminal (with internal surge absorber removed) Leakage current 10 mA max. Noise resistance 1500 Vp–p; pulse width: 0.1µ...

  • マニュアル

    ...+: 1.0 ppm Results of ICP Emission Spectral Analysis The V600-D23P66SP Data Carrier was soaked in concentrated hydrochloric acid (which can easily penetrate through PFA) at 80°C for 300 hours, then extracted substances were analyzed. Extracted Substances (Concentration) Si: 700 ng/ml, ...

  • マニュアル

    ... the built-in surge absorber removed) Dielectric strength 1,000 VAC, 50/60 Hz between all DC external terminals and GR terminal (with the built-in surge absorber removed) Leakage current 10 mA max. Noise resistance 1500 Vp–p; pulse width: 0.1µ...

  • マニュアル

    ... 100 VDC, with internal surge absorber removed) Dielectric strength 1,000 VAC, 50/60 Hz between all DC external terminals and GR terminal (with internal surge absorber removed) Leakage current 10 mA max. Noise resistance 1500 Vp–p; pulse width: 0.1µ...

  • マニュアル

    ... internal surge absorber removed.) Dielectric strength 1,000 VAC, 50/60 Hz between all DC external terminals and GR terminal (with internal surge absorber removed.) Leakage current 10 mA max. Noise resistance (common mode) 1500 Vp-p; pulse width: 0.1 µ...

  • マニュアル

    ... internal surge absorber removed.) Dielectric strength 1,000 VAC, 50/60 Hz between all DC external terminals and GR terminal (with internal surge absorber removed.) Leakage current 10 mA max. Noise resistance (common mode) 1500 Vp-p; pulse width: 0.1 µ...

  • マニュアル

    ...between all DC external terminals and GR terminal (at 100 VDC, with internal surge absorber removed) 1,000 VAC, 50/60 Hz between all DC external terminals and GR terminal (with internal surge absorber removed) 10 mA max. 1500 Vp–p; pulse width: 0.1µ...

  • マニュアル

    ...375 g Characteristics ■ Camera Characteristics Item Specification Picture element 1/3" Interline CCD (reading all pixels) Effective pixels 659 × 494 (H × V) Synchronization External sync. via horizontal sync signal Shutter speed F150-series: 1/100 ...

  • マニュアル

    ... in the order shown in the following diagram. 66 Section 4-1 Overview of RS-422 Communication Unit Example: Sending communications sequence 600 (with ASCII conversion) 15 08 07 00 Number of send data words S Node number ...

  • マニュアル

    ... I N G

    71 Section 4-3 Trigger Inputs and Output Format Settings Data for QR Code (Normal) Number 1 Settings data for QR Code (Normal) Image Adjust Digit(s) Shutter Speed 0: 1/100 s, 1: 1/500 s, 2: 1/2,000 s, 3: 1/10,000 s Digit 1 Filtering 0: OFF, 1: Weak Smoothing, 2: Strong Smoothing, 3: Enhance Edges Digit 2 3 Filtering Retry 0: OFF, 1: ON Digit 3 4 BGS Level Upper 001 to 255 (See note 1.) Limit Digits 4 to 6 5 BGS Level Lower 000 to 254 (...