全 1073 件が検索されました。(701 - 720件を表示)

  • マニュアル

    ... ASCII Unit (0 to F). 102 Section 6-5 IOWR/IORD Instruction Specifications CS1-series PCs 15 43 0 S: 0 0 0 Unit No. of the ASCII Unit (0 to F) 15 0 S+1: S: Rightmost 4 digits S+1 : Leftmost 4 digits No. of transfer words (0001 to 0080 Hex from CIO n+8) from the ASCII Unit to the CPU Unit. D: First destination word in CPU Unit's I/O memory from CIO n+8 and CIO n+9. Data Item Detail PC C200HX/HG/HE Operand D IR Area 1 IR 000 to ...

  • マニュアル

    ...D Word address (5th digit) D+1 Word address (1st digit) Word address (2nd digit) Word address (3rd digit) Word address (4th digit) RECV The beginning send word is determined by the contents of the destination node’s S and ...

  • マニュアル

    ...1211 87 0 − L PortspecifiCation 1:PortA 2:PortB Sendlreceivesequence No.OOOto999(BCD) S:Senddatastartingchannelnumber SetthestartingchannelattheCHareawheredatarequiredforsettingisstored. NeteWhennosenddataisfound,besuretoset#0000.Settingtheotherconstantor channelgeneratesanerror(ERflag25505isON),andthePMCRinstructionis notexecuted. SenddataofhowmanywordsarevalidatSandthefollowingisstoredinS. ActuallysenddataisstoredinS÷1andthefoilowing. No.ofsenddata S words ...

  • マニュアル

    ...由識 r晦継rr 奪端綱t ■ …8醐荘 、㌧_/∴"r}│_、ザ ⊥ 弍r r: ∴ ∵∵…;二1}∴∵ ) ■、A M'vや'A 峯竺⊥{ ■、ぐr/ ⊥ __こ 、、フ 、「潅纏緯醗一㌻l/l!∵ /i…}ザ○ 、"× _-、..s、、、、∨、、、1 ■一 、γ…w〃∵∵ … 一㌔∨ 、 ‥ r…/ノ ノニ ・ 」 一∴1■ ミ三{r 「 A ・ M白`♂"、、、A 』 ハいへ ヘノっへ ' こthooKR・ ' / / : E只「 ζ「ら1「\i泌舶R A■■一■}「一} ∴'適爾蔭言ご「1 , 〉 悶悶2' 、 淀遮Pωo駆 1 「'1.ADI)ER ヰ …/、 … 「...

  • マニュアル

    ... in the following example. Address Specification Address Contents FINS command sent Remote network address (1) Serial communications path network address Example A Remote node address (2) Unit No. for Host Link incremented by 1. ...

  • マニュアル

    ... Operation Manual or Programming Manual. Example Conditions Master node address: 63 Slave network address: 1 Slave node address: 2 Example: Using the CMND Instruction Command Words (S: First Command Word) Word Contents (Hex) Meaning S 28 01 ...

  • マニュアル

    ... timers are not defined using a timer number and timer numbers are not needed to access the Completion Flag and PV. The Completion Flag is bit 00 of D1, the PV is maintained in D2 and D2+1, and the SV is specified in S and ...

  • マニュアル

    ...Monitoring time during send/ receive processing Link word setting 60 Interrupt notificaYes tion for reception case number Receive wait, receive completion, or send completion can be monitored. Setting range: 0.01 to 0.99 s, 0.1 to 9.9 ...

  • マニュアル

    ... 03: 0 to 3 hex 0 (0 hex) Decimal point position (from right) for instantaneous value when 100% input --- Bit 04 to 07: 0 to 4 hex 0 (0 hex) Instantaneous value time unit (matching conversion period) 0: 1 ...

  • マニュアル

    ... at the local node) to remote node N. In return, “m” bytes of response data are stored at the local node beginning with D (the beginning word for storing response data). 15 Remote (source) node N Local node 0 S ••• (...

  • マニュアル

    ... to 3-5-4 Editing User Link Tables. Refresh period The refresh cycle for CPU Unit data. The cycle can be set to the system common operating cycle, 0.01 s, 0.02 s, 0.05 s, 0.10 s, 0.20 s, 0.50 s, 1.00 s, or 2.00 s (If the user link table is pasted in a block diagram to make software connections and the function block data is downloaded to the Loop Control Board with the Update User Link Table Refresh Cycle selection selected in the CX-Process Tool, the setting made here ...

  • マニュアル

    ...128 Master’s node number: 63 Slave’s network address: 1 Slave’s node number: 2 Section 6-3 Explicit Message Communications CMND(194) Operand Details [CMND S D C] • Command Words Word S S+1 S+2 S+3 S+4 S+5 Contents Function (Hex) 28 01 EXPLICIT MESSAGE SEND command code = 2801 (Hex) 02 1C Slave node number = 02 (Hex) READ BYTE DATA command service code = 1C (Hex) 00 2F Class ID = 002F (Hex) 00 01 Instance ID = 0001 (Hex) specifies data area 0A 00 Starting read address = 000A (Hex) specifies IR 010 Address L = 0A (Hex); ...

  • マニュアル

    ... 15 DM 6611 00 to 15 DM 6612 00 to 15 DM6645 00 to 15 DM6646 00 to 15 Function ABS resolution Rightmost 4 digits (the No. of input pulses for Leftmost 4 digits encoder's 1 revolution) Note: HCA12V1 Only Details 0000 0001 to 0000 8000 Hex Note: Set the resolution considering servo driver's "encoder dividing rate" and unit's "pulse input multiplication setting". Ex: “Driver: 1000, unit: with multiplication of 4”: FA0 (4000) Maximum ring counter value for high-speed counter 2 Note: HCP22V1/HCA22-V1 Only ABS offset value Note: HCA12V1 only As above. Rightmost ...

  • マニュアル

    ... Unit CPU Unit Interpretation1 Interpretation2 Command data Response No. of command bytes Response Response monitoring time ...... S+2 S+3 S+4 Command Destination node Local Master Unit CPU Unit S+1 Operands C: Control code S: 1st source word D: Destination information Execution L Execution ... Response data 1: For commands addressed to Master Unit 2: For commands addressed to CPU Unit Description IOWR transfers data from the words beginning at S to the specified Special I/ O Unit. The control code (C) specified parameters for the instruction as shown in the following illustration. C: Destination unit address (see ...

  • マニュアル

    ... size: 5 bytes Node address 1: OUT size: 4 byte, IN size: 3 bytes Node address 2: OUT size: 1 byte, IN size: 2 bytes 15 Allocation size setup table I 1 5 s I+1 4 3 s+1 I+2 1 2 s+2 : : s+3 OUT block 1 15 k 00 00 01 01 k+1 00 00 01 01 k+2 02 k+3 Not usable : k+4 00 Not usable 01 01 Not usable 01 02 k+5 l: First word of the allocation size setup table s: First word of OUT block 1...

  • マニュアル

    ...Ladder Symbols IR, SR, AR, DM, EM, TIM/CNT, LR, # MOVL(––) @MOVL(––) S S D D 000 000 D: Starting destination word Limitations IR, SR, AR, DM, EM, LR, # 000: Always “000” 000 S and S+1 must be in the same data area, as must D and D+1. DM 6144 to DM 6655 cannot be used for D. Note When using this instruction from the CX-Programmer, set bits 08 to 11 of DM 6600 in the Unit Setup Area to 1 to enable user-specified expansion instruction settings before uploading and downloading the program. On the CX-...

  • マニュアル

    ...Setting time (unit: 0.1 s) 0 to 999.9 s Binary mode TTIMX &0 to &65535 (decimal) or #0000 to #FFFF (hexadecimal) 0 to 6,553.5 s LONG TIMER (100 ms) Instruction name BCD mode Mnemonic S, S+1 (timer set values) TIML #00000000 to #99999999 (BCD) Setting time (unit: 0.1 s) 0 to 999.9 s Binary mode TIMLX &0 to &4294967295 (decimal) or #0000 to #FFFFFFFF (hexadecimal) 0 to 6,553.5 s MULTI-OUTPUT TIMER (100 ms) Instruction name Mnemonic S to S-7 (each timer set value) BCD mode MTIM #0000 to #9999 (...

  • マニュアル

    ... the new PV when changing the PV. If C is 0002 hex (i.e., when changing a PV), NV and NV+1 contain the new PV. Any values in NV and NV+1 are ignored when C is not 0002 hex. 0 15 S S+1 Lower word of new PV Upper word of new PV For Pulse Output or High-speed Counter Input: 0000 0000 to FFFF FFFF hex For Interrupt Input in Counter Mode: 0000 0000 to 0000 FFFF hex Operand Specifications Area CIO Area Work Area Holding Bit Area Auxiliary Bit Area Timer Area Counter Area...

  • マニュアル

    ... is continued before operation is started) is possible CX-Process Tool or FINS command. Standard: Operation of all function blocks is executed at the same operation cycle preset to ITEM 004 in the System Common block. Settable operation cycles: 0.1 s, 0.2 s, 0.5 ...

  • マニュアル

    ... number of words, starting from the beginning word S at the remote node (node address M) is received at the words starting from the beginning word D at the local node. 15 Local node 0 Destination node number N S Command (...