全 44873 件が検索されました。(6601 - 6620件を表示)
- マニュアル
...設定したときは筐体の単回転感度ボリウムの示す位置に基づく感度と実際に反映されている感度は異なります。 *(a)から(d)に記載されている他、本カタログ等記載の商品は自動車 (二輪車含む。 以下同じ) 向けではありません。 自動車に搭...
- マニュアル
... "1 ∼ 9" で表示し、 10 月は "X"、11 月は "Y"、12 月は "Z" で表示する。 YY:製造年、西暦2位数字で表示する。 例えば、 2025 年は”25”。 A :工場 ID、例えば OMS は「M」です。 1 茶 DC12∼24V 安定表示灯(緑) 3 透過形の投光器コネクタピン番号 1 茶 光電 DC12∼24V ②は空端子 ④は空端子 スイ...
- マニュアル
...旋钮和动作切换开关, 所以外形有所不同。 NO.789,Jinji Road, China(Shanghai)Pilot Free Trade Zone 201206 The following notice applies only to products that carry the CE mark: Notice: This is a class A product. In residential areas it may cause radio interference, in which case the user may be required to take adequate measures to reduce interference. © OMRON Corporation 2005-2025 All Rights Reserved. 证明标签 ●警告表示的意思 Precautions on Safety 灵敏度调节旋钮** 动作...
- マニュアル
...作切替スイッチ** (3)中国の場合本製品は、GB/T 7247.1-2024(IEC60825-1:2014)に定める Class1に分類されます。 Precautions on Safety Meaning of Signal Words Indicates a potentially hazardous situation which, if not avoided, will result in minor or moderate injury, WARNING or may result in serious injury or death. Additionally there may be significant property damage. 動作表示灯* (4)カナダで使用する場合本製品は、IEC60825-1:2014に...
- マニュアル
...: Importer in EU: Omron Corporation, Omron Europe B.V. Shiokoji Horikawa, Shimogyo-ku, Wegalaan 67-69 Kyoto 600-8530 JAPAN 2132 JD Hoofddorp, The Netherlands The following notice applies only to products that carry the CE mark. Notice: In ...
- マニュアル
... installing and operating the product. Before operating the product,read the sheet thoroughly to acquire sufficient knowledge of the product.For your convenience,keep the sheet at your disposal. The following notice applies only to products that carry the CE mark: Notice: This is ...
- マニュアル
...[5654869-0A] E3Z-LS□□ 光電センサ 取扱説明書(日/英/伊/独/仏/西/韓語) 使用上の注意 ■定格性能 * 5 6 5 4 8 6 9 - 0 A * © OMRON Corporation 2002-2010 All Rights Reserved. 安全上のご注意 ●警告表示の意味正しい取扱いをしなければ、この危険のために、時に軽傷・中程度の傷害を負ったり、ある...
- マニュアル
...致一机能:连接V成成 NPN PNP 型检 模式 换 设定距离范围 BGS 检 The following notice applies only to products that carry the CE mark: Notice: This is a class A product. In residential areas it may cause radio interference, in which case the user may be required to take adequate measures to reduce interference. * 2 1 3 8 7 5 6 - 2 B * © OMRON Corporation 2003 All Rights Reserved. 距离范围 FGS 源(发 波长取电源电压消费电流控...
- マニュアル
...(PBT)、 材質操作部およびレンズカバー部:変性ポリアリレート設定距離範囲 The following notice applies only to products that carry the CE mark: Notice: This is a class A product. In residential areas it may cause radio interference, in which case the user may be required to take adequate measures to reduce interference. * 6 9 9 7 3 1 2 - 9 D * © OMRON Corporation 2003-2010 All Rights Reserved. ■外形寸法図 動作表示灯...
- マニュアル
... L load is used. (8)Water resistance Though this is type IP67, do not use in the water, rain or outdoors. (9)Do not use the product in ambient atmosphere or environment exceeding the rating. ⑥ Plug in or out the connector after surely turning off ...
- マニュアル
...Representative in EU: Manufacturer: Omron Corporation, Omron Europe B.V. Shiokoji Horikawa, Shimogyo-ku, Wegalaan 67-69 Kyoto 600-8530 JAPAN 2132 JD Hoofddorp, The Netherlands The following notice applies only to products that carry the CE mark: Notice: In ...
- マニュアル
...Manufacturer: Omron Europe B.V. Omron Corporation, Wegalaan 67-69 Shiokoji Horikawa, Shimogyo-ku, 2132 JD Hoofddorp, Kyoto 600-8530 JAPAN The Netherlands Ayabe Factory 3-2 Narutani, Nakayama-cho, Ayabe-shi, Kyoto 623-0105 JAPAN Notice: In ...
- マニュアル
...ません。 ただし、次に掲げる用途であっても当社の意図した商品用途の場合や特別の合意がある場合は除きます。 (a) 高い安全性が必要とされる用途 (例:原子力制御設備、燃焼設備、航空・宇宙設備、鉄道設備、昇降設備、娯楽設備、医用機器、安全装...
- マニュアル
...Omron Europe B.V. Wegalaan 67-69 2132 JD Hoofddorp, The Netherlands Manufacturer: Omron Corporation, Shiokoji Horikawa, Shimogyo-ku, Kyoto 600-8530 JAPAN Ayabe Factory 3-2 Narutani, Nakayama-cho, Ayabe-shi, Kyoto 623-0105 JAPAN Notice: In ...
- マニュアル
...Precautions for Safe Use ⑤Excessive force (hitting by hammer, etc.) should not b Thank you for selecting an OMRON product. This sheet primarily describes precautions required in installing and operating the product. • ...
- マニュアル
...择额定•性能有一定余地的产品,同时应当考虑各种安全对策,即使发生故障,也能将危险降低到最小程度的安全回路等。 a)屋外的用途、潜在化学污染或受到电气妨害的用途、或者在商品目录、使用说明书等中没有记载的条件及环境下使用。 b)原...
- マニュアル
...れていません。 ●製品に関するお問い合わせ先お客様相談室 FAX 500m/s2 (約50G) X,Y,Z 各方向 3回 約120g (1セット) *(a)から(d)に記載されている他、本カタログ等記載の商品は自動車 (二輪車含む。 以下同じ) 向けではありません。 自動車に搭載する用途...
- マニュアル
...[E429-E1-12] E3NW-ECT EtherCAT® Digital Sensor Communication Unit Operation Manual E3NW-ECT EtherCAT Digital Sensor Communication Unit ® Operation Manual E429-E1-12 © OMRON, 2013 All rights reserved. No part of this publication may be reproduced, stored in ...
- マニュアル
... 4 èÕ4 Section 5 Introduction Application Considerations (Please read first) Introduction Introduction Terms and Conditions Agreement Warranty, Limitations of Liability ■ Warranties ● Exclusive Warranty Omron’s exclusive warranty is that the Products will be free from defects in materials and workmanship for ...
- マニュアル
...-E1-11] E3NW-CCL CC-Link Digital Sensor Communications Unit User's Manual E3NW-CCL CC-Link Digital Sensor Communications Unit User’s Manual Cat. No. E431-E1-11 NOTICE (1) No part of this publication may be reproduced, stored in ...