全 1430 件が検索されました。(561 - 580件を表示)
- マニュアル
... heat source • Water flooding or oil splashes • Direct sunlight • Dust or corrosive gases (especially, sulfuric or ammonia gas) • Rapid temperature changes • Condensation or icing due to high humidity • Strong vibration or mechanical shock (2) Do not block heat dissipation from the product, i....
- マニュアル
.... Page 5-23: Changed the description at the top of the page. Page 5-23: Added a table for “Disabled”, changed the titles to “Overflow” and “Input error”, and changed the description for Output under Overflow. Page 5-24: Changed the seven segment displays for step ...
- マニュアル
... user’s attention. Page 5-83: Text added after table. Page 6-9: Middle rows of table reversed. Pages A-2: Changed “XAD” to “XVA” and “XVA” to “XAD” in left column. Page A-3: Changed column division within table under Event inputs, i....
- マニュアル
... Protocol (CompoWay/F Communications) The host computer sends a command frame, and the K3HB sends a response frame based on the content of the command frame. One response frame is sent in response to one command frame. 1-2 d an mm ...
- マニュアル
...Troubleshooting Describes how to check and possible countermeasures for errors. Appendices Provides specifications and settings lists. XII Settings Data Notation The letters of the alphabet in settings data are displayed as shown below. a b c d ...
- マニュアル
... low power radio station is operating close to it. (2) If in case this product causes radio interference with an RFID premises radio station, immediately change the product's frequency or stop radio emission, and contact OMRON representative for actions to take to prevent cross talk (...
- マニュアル
... limited to, embedding and/or using Omron Products in their parts/components, electronic substrates, devices, equipment or systems manufactured by customers. (5) Fitness: (a) fitness for a particular purpose, (b) performance, (c) non-infringement of third-party intellectual property, (d) compliance with laws and regulations and (...
- マニュアル
... limited to, embedding and/or using Omron Products in their parts/components, electronic substrates, devices, equipment or systems manufactured by customers. (5) Fitness: (a) fitness for a particular purpose, (b) performance, (c) non-infringement of third-party intellectual property, (d) compliance with laws and regulations and (...
- マニュアル
... special CT, be sure to use the insulated wires at temperatures below 65°C that have rated minimum 600 V and at least basic insulation. When clamping with conductive materials like busbar etc., use the special CT after ensuring equal to or more than basic insulation ...
- マニュアル
... with the torque in the range of 0.5 to 0.6 N•m. Also confirm if the terminal screw is tighten appropriately. ●To prevent malfunctions caused by noise, ground the NA Unit correctly. ●Do not use any battery if strong impact is applied to it (...
- マニュアル
... server, make the settings of the DHCP server as described below. Otherwise, controlled devices may perform unexpected operations. • IP address assignment method: Static assignment • Lease period: Unlimited Precautions for Safe Use • The CPU Unit performs I/O refresh even while the program is stopped (i....
- マニュアル
... will not operate correctly if it uses corrupted data. • Always turn OFF the power supply before you attempt any of the following. a) Mounting or removing the Units b) Assembling the Units c) Setting rotary switches d) Connecting cables or wiring the system ...
- マニュアル
.... Installation • Do not block the intake or exhaust openings. Malfunction, operation stop, or equipment damage may result. • Do not allow foreign objects to enter the Amplifier. • Do not operate or store in the following locations: a) b) c) d) ...
- マニュアル
...。 なお、長い電極棒を使用するときには、接触防止のためにセパレータを使用してください。 割シズは高さをかえてE 1 、E 2 、E 3 の 位 置でそれぞれの 電 線 に取 付けます。 これが液 体と導 線との 接 触 面 になり、それぞれが短、中 、長 電 極とな...
- マニュアル
... on the Servo Drive and Servomotor. Internal elements may be damaged. Carefully perform the wiring and assembling. Injury may result. Wear the protective equipment when installing or removing the main circuit connector, main circuit connector A, main circuit connector B, main circuit connector ...
- マニュアル
...みます。 (5)「適合性等」 : 「お客様用途」での「当社商品」の (a) 適合性、 (b) 動作、 (c) 第三者の知的財産の非侵害、 (d) 法令の遵守および (e) 各種規格の遵守 2. 記載事項のご注意 「カタログ等」の記載内容については次の点をご理解ください。 (1)定格値および性...
- マニュアル
...-CX1DBF R88A-CX1DEBF*1 200 VAC 3,000-r/min Servomotors 200 W, 400 W, 750 W 200 VAC 3,000-r/min Servomotors 1 kW R88A-CX1DSF *1. R88A-CX1EBF is an extension cable. This cable can be used when extending an integrated cable whether it has a brake wire or not. To extend the R88A-CX1CF integrated cable, use R88A-CX1BEBF. 43 AC Servomotors/Servo Drives 1S-series Instruction Manual External Dimensions ...
- マニュアル
...みます。 (5)「適合性等」 : 「お客様用途」での「当社商品」の (a) 適合性、 (b) 動作、 (c) 第三者の知的財産の非侵害、 (d) 法令の遵守および (e) 各種規格の遵守 2. 記載事項のご注意 「カタログ等」の記載内容については次の点をご理解ください。 (1)定格値および性...
- マニュアル
...みます。 • 「適合性等」 :「お客様用途」での「当社商品」の (a) 適合性、(b) 動作、(c) 第三者の知的財産の非侵害、(d) 法令の遵守および (e) 各種規格の遵守 記載事項のご注意 「カタログ等」の記載内容については次の点をご理解ください。 • 定格値および性能値...
- マニュアル
...-B03 S82Y-FSG-B04 S82Y-FSG-B05 S82Y-FSG-B07 使用取付穴 Mounting hole for use Type A Type B a/d A/B a/d A/B a/b D/F d/e A/D a/b A/E a/b A/E a/d A/F a/d A/F A/B/D/E(※) E/G/M/Q a/b A/B a/b A/B e/f A/D D/E...