全 31668 件が検索されました。(481 - 500件を表示)
- マニュアル
...-E CQM1H-PRO01-E LCD display Mode switch FUN SFT A ST OR H AA LD AC OUT N M 7 0 . −IR TR J *EM WR/LR K AR HR EM DM P CH *DM Q CONT # R 6 T DEL MON 2 3 Y TEXT ! CLR VRFY NOT B C CHG W INS TN AND G H AC OUT N M 7 E F 4 6 0 6 D 2 DR IR . −IR TR J *EM WR/...
- マニュアル
...C-mode Commands The following table lists the C-mode (Host Link) commands. For details, refer to SECTION 4 C-mode Commands. Type I/O memory reading 2 Header code RR Name CIO AREA READ RL LR AREA READ RH HR AREA READ RC TIMER/COUNTER PV READ RG RD TIMER/COUNTER STATUS READ DM AREA READ RJ AR AREA READ RE EM AREA READ Function Reads the specified number of words beginning with the designated CIO word. Reads the specified number of words beginning with the designated ...
- マニュアル
... for the sequence can be set automatically. Using the interrupt function, high-response processing can be achieved. 4th operand in PMCR instruction (3rd operand for C200HX/HG/HE) Designate word+ z word CIO@@@ WR@@@@ (note 1) ...
- マニュアル
...7 SFT NOT OR CNT OUT TIM EM 9 EXT 8 E 4 F 5 B 1 C 2 A 0 TR DM * EM AR LR HR CH DM * 6 D 3 Programming Console Initial Data Settings 1. Specify the Special I/O Unit DM Area settings. Refer to Allocations in DM Area on page 394 for further details. SYSMAC CJ1G-CPU44 PROGRAMMABLE CONTROLLER RUN ERR/ALM INH PRPHL COMM OD261 0 8 0 8 I II 1 2 3 4 5 6 7 9 10 11 12 13 14 15 1 2 3 4 5 6 7 9 10 ...
- マニュアル
...C200H I/O Link Units Communications Specifications Item I/O points Specification Input: 512 points max. (32 words) Output: 512 points max. (32 words) Memory areas that can C200HX/HG/HE: be allocated CIO, DM, HR, AR, ...
- マニュアル
... on the Serial Communications Board. TXD(––) or RXD(––) instructions Bar–code reader 1:1 Data Link System Printer If two PCs are linked one-to-one by connecting them together through their RS-232C ports, they can share up to 64 words of ...
- マニュアル
... 0050 to CIO 0099, CIO 0350 to CIO 0399 SYSMAC BUS Area: CIO 3000 to CIO 3049 CIO 0247 to CIO 0250 and A442 PLC Link Words Optical I/O Unit and I/O Terminal Area Link Relay Area (LR) Work/ Internal I/O area Work Area (WR) Temporary Relay Area Holding Relay Area(HR) Auxiliary Relay Area (AR) DM Area EM Area Timer Area Counter Area CX-Simulator Not allocated actually even if the unit is set. Only Serial Communications Units and Network Communications Units are allocated. Not allocated actually even if the unit is set. I/O ...
- マニュアル
...: 1 CIO: 32 Wds, DM: 64 Wds Node 1 Node 2 Node 3 Node 2 Node 4 When using a data link that combines C-series SYSMAC LINK Units, CSseries SYSMAC LINK Units, and CVM1/CV-series SYSMAC LINK Units, LR 00 to ...
- マニュアル
... the use of communications programs on the PLC (CPU Unit) or IBM PC/AT or compatible computer. Data written in the send area of the local node will be automatically sent to the receive area of other nodes. The I/O area (CIO area), link area (...
- マニュアル
... input words and 32 output words) can be allocated to the DeviceNet Master’s I/O. The Master’s I/O can be allocated to the following data areas. IR 000 to IR 049 IR 200 to IR 227 DM 0000 to DM 2047 LR 00 to ...
- マニュアル
... DM Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . LR Area. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Difference between I/O Refreshing in Customizable Counter Units and That in Other Special I/O Units . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 5 Unit Setup Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5-1 Unit Setup Area. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 60 63 67 71 72 77 78 vii TABLE OF CONTENTS SECTION 6 I/O Memory. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6-1 6-2 6-3 6-4 Overview . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Details . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SR Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . AR Area . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 85 86 89 93 98 SECTION 7 Special Functions . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 119 7-1 7-2 7-3 7-4 7-5 7-6 7-7 7-8 7-9 7-10 7-11 7-12 7-13 7-14...
- マニュアル
... words) words x 1) 1,024 pts (32 input/32 output words) CQM1-DRT21 32 pts (1 input/1 output word) CS1W-DRM21(-V1) CJ1W-DRM21 C200HW-DRM21 CIO, WR, DM, EM, HR CQM1-DRT21 CIO CIO, DM, EM, AR, LR, T/C 5 Section 1-1 Overview of DeviceNet Message Communications Function [ CMND ... ] Master Master Special Slave Item Communications Instructions Master CS Series CJ Series CVM1, CV Series CS1W-DRM21(-V1) CJ1W-DRM21 DVM1-DRM21-V1 SEND(192) SEND(192) SEND(192) RECV(193) RECV(193) RECV(193) FINS commands CMND(194) CMND(194) CMND(194) CS Series,...
- マニュアル
...x 1) input/100 output words) 1,024 pts (32 input/32 output words) CQM1-DRT21 32 pts (1 input/1 output word) CS1W-DRM21(-V1) CJ1W-DRM21 C200HW-DRT21 CIO, WR, DM, EM, HR CIO, DM, EM, AR, LR, T/C CQM1-DRT21 CIO CS1W-DRM21(-V1) 7 Overview of DeviceNet Section 1-1 Message Communications Master Master RS-232C Interface Unit Communications Instructions Master CS Series CJ Series CVM1, CV Series CS Series, C200HX/HG/HE C200HS Item Max. No. of nodes per Master for message communications using FINS commands Max. No. of nodes per Master for message...
- マニュアル
... be used. 86 Range CIO Area DM Area Section 4-8 Manual I/O Allocations • C200HW-DRM21-V1 PLC model C200HS C200HE-CPU11 Data area IR/SR Area Range 000 to 511 HR Area LR Area HR 00 to HR 99 LR 00 to LR 63 DM Area IR/SR Area DM 0000 to DM 5999 000 to 511 HR Area ...
- マニュアル
...Automatic setting can be used to create simple data links. • Using a Programming Device (such as a Programming Console), set the automatic data link mode in the DM parameter area of the startup node. • Area 1 can be selected from bit areas (i.e., IR, CIO, and ...
- マニュアル
... AR 27 AR 0000 to AR 2715 These bits serve specific functions such as flags and control bits. TR Area 8 bits --- TR 0 to TR 7 These bits are used to temporarily store ON/OFF status at program branches. ...
- マニュアル
... data links can be created to automatically transfer large amounts of data as listed below. Item Number of send words per node Number of send and receive words per node Specifications 508 words max. (254 words max. in the CIO/...
- マニュアル
... blocks, Memory Units, expansion cables, and other items with locking devices are properly locked into place. Improper locking may result in malfunction. • Double-check all wiring and switch settings before turning ON the power supply. Incorrect wiring may result in burning. • Disconnect the ...
- マニュアル
...Command mode DIO1 to DIO8 UNL TA LA Data mode A B C ... Delimiter DAV ATN UNL: Unlisten command TA: Talker address LA: Listener address 8 A, B, C ...: Data Delimiter: CR + LR, CR, etc. (selectable) Section 1-4 Comparison with other OMRON Units’ GP-IB Functions 1,2,3... 1. The Controller sets the ATN line to “L” and sends the UNL command. This command inactivates the connected GP-IB devices. 2. The Controller sends the TA (Talker address) and LA (Listener address). Two or more Listener addresses can be specified. This step determines the new Talker and Listener(...
- マニュアル
... certain usage conditions. It may not be possible to use a Master Unit in some locations. Contact your OMRON representative before attempting to use a Master Unit on a ship. 7-1 Applicable Shipping Standards The Master Units conform to the following standards: ...