全 2268 件が検索されました。(401 - 420件を表示)

  • マニュアル

    ...D-H” is used to indicate information that is the same for the E5CD-H and E5ED-H Digital Controllers. Meanings of Abbreviations The following abbreviations are used in parameter names, figures, and other descriptions. These abbreviations mean the following: Symbol PV ...

  • マニュアル

    ...Description The command is too long. Non-volatile memory error • Error Occurred Response code 1001 2203 2-3-8 Operation Command • • • • • • • Communications Writing AT Execute/Cancel Software Reset Auto/Manual Switch ...

  • マニュアル

    .../O Extended Speed and Acceleration Control Extended Speed and Torque Control Extended Control I/O Extended Control I/O and Multi function I/O Monitor Special I/O Flexible Format Outline Types of Remote I/O that support general ...

  • マニュアル

    ...-15 Error Codes ..........................................................................................................................3-19 Section 4 V+ Process Manager Module 4-1 pm.ace.blt.cam .......................................................................................................................4-3 4-2 pm.ace.blt.ltch........................................................................................................................4-4 4-3 pm.ace.blt.pos........................................................................................................................4-5 4-4 pm.ace.blt....

  • マニュアル

    .../14 LIM TE 29 -57V Do ctr no cu no ic t dis 9/1 新能 ITE CH LiF Kg dc Do t or t sh co 34 源股 D NO da oc nn lea no sp IP3 eP /[1 Ke d t ea ma k or ec O4 份有 LO P1 GY 3 it ep to ex rin ge bu t, Ba Sin if liqu the fire po g the 6S 限公 rns dis mo gle tte as or se ob ]M 司 We vin id un ex to jec un . Se se ry /-...

  • マニュアル

    ...8.2. ASCII コード表 10 進数 16 進数 文字 2 進数 10 進数 16 進数 文字 0000000 0 0 NUL 0100000 32 20 SP 0000001 1 1 SOH 0100001 33 21 ! 0000010 2 2 STX 0100010 34 22 " 0000011 3 3 ETX 0100011 35 23 # 0000100 4 4 EOT 0100100 36 24 $ 0000101 5 5 ENQ 0100101 37 25 % 0000110 6 6 ACK 0100110 38 26 & 0000111 7 7 BEL 0100111 39 27 ' 0001000 8 8 BS 0101000 40 28 ( 0001001 9 9 HT 0101001 41 29 ) 0001010 10 A...

  • マニュアル

    ...左から 5 ∼ 8 文字分の ASCII コード R 形式を 12 文字の左詰め表記としたときの左から 9 ∼ 12 文字分の ASCII コード (sp)は空白文字(スペース) R ソフトバージョン (例)H’00000100 → Ver.1.0.0 R ステータス情報 「コントローラステータス読出(0601) 」参照 R バッファ...

  • マニュアル

    ...リフ 0 : T1 1 : T2 2 : T3 3 : T4 R/W 1200 2400 形式 1(KM-N) R 1201 2402 形式 2(3-FL) R 1202 2404 形式 3(K(sp)(sp)(sp)) R 共通 1203 2406 ソフトバージョン(例 .100) R 1204 2408 ステータス情報 R 1205 240A バッファサイズ(230 固定) R 通信詳細仕様 95 KM-N3-FLK_UsersManual_jpn.book 96 ページ 2024年1月17日 水...

  • マニュアル

    ...frame based on the content of the command frame. One response frame is sent in response to one command frame. 1-2 d an mm e Co fram d an mm e Co fram K3HB Re sp fra ons me e Host computer Re sp fra ons me e CompoWay/F Communications Communications Method Communications Method Section 1-1 After a receiving a response from the Digital Indicator, have the host computer wait at least 50 ms before sending the next command. When writing multiple sets of setting data in a row, such as when writing to the variable area ...

  • マニュアル

    ...× Averaging times avg-n × Auto-zero time A at. za × Auto-zero time B at. zb × Power interruption memory memo Comparative set value display svd. sp Display refresh period d. ref Display color selection color Display value selection disp Automatic display return ret Position meter type pos-t Position meter upper limit pos-h Position meter type ≠ OFF Position meter lower limit pos-l Position meter type ≠ OFF Prescaling bank ps. bnk Bank selection ≠ OFF Prescale * AX (*: 0-7) pso. ax Bank selection ≠ OFF; * is the value between 0 and 7 set for the comparative set...

  • マニュアル

    .... R 2402 1201 Model 2 (2-FL) The model is shown in ASCII code, with characters 5 to 8 starting on the left when the display is 12 characters aligned to the left. R 2404 1202 Model 3 (K (sp)(sp)(sp)) The model is shown in ASCII code, with characters 9 to 12 starting on the left when the display is 12 characters aligned to the left. (...

  • マニュアル

    ... settings 110E 221C Current tariff 0 : T1 1 : T2 2 : T3 3 : T4 1200 2400 Model 1 (KM-N) R 1201 2402 Model 2 (3-FL) R 1202 2404 Model 3 (K (sp)(sp)(sp)) R 1203 2406 Software version (Ex.: 100) R 1204 2408 Status information R 1205 240A Buffer size (230 fixed) R 99 7. Troubleshooting Troubleshooting 7.1 Warnings Warnings come as errors and alarms. The types of errors and alarms are described below. Warning type Error Description Display Action to take Setting value error Internal memory corrupted Measured value error Internal memory corrupted Calibration value...

  • マニュアル

    ...Model FH-3/FH-3- OMRON 0.3 megapixel digital camera Model FZ-SC/S 0.3 megapixel compact digital camera Model FZ-SFC/SF 0.3 megapixel compact digital camera, Model FZ-SPC/SP pen type 0.3 megapixel high-speed camera Model FZ-SHC/SH 0.3 megapixel high-speed CMOS camera Model FH-SC/SM 2 megapixel digital camera Model FZ-SC2M/S2M 2 megapixel high-speed CMOS camera Model FH-SC02/SM02 4 megapixel high-speed CMOS camera Model FH-SC04/SM04 5 megapixel digital camera Model FZ-...

  • マニュアル

    ...Model FH-3/FH-3- OMRON 0.3 megapixel digital camera Model FZ-SC/S 0.3 megapixel compact digital camera Model FZ-SFC/SF 0.3 megapixel compact digital camera, Model FZ-SPC/SP pen type 0.3 megapixel high-speed camera Model FZ-SHC/SH 0.3 megapixel high-speed CMOS camera Model FH-SC/SM 2 megapixel digital camera Model FZ-SC2M/S2M 2 megapixel high-speed CMOS camera Model FH-SC02/SM02 4 megapixel high-speed CMOS camera Model FH-SC04/SM04 5 megapixel digital camera Model FZ-...

  • マニュアル

    ...) IOSP(187) None None None None None IORS(188) None IODP(189) READ(190) None None WRIT(191) None MSG(195) MSG(46) TOUT SA(210) None SA(784) SP(211) SR(212) SF(213) SE(214) None None None SE(785) SOFF(215) CSP(221) None CSP(510) CSPN(222) CSPN(511) CNR(236) CNR(545) PID(270) PID(190) RD2(280) None WR2(281) None TST(350) TST(350) TSTN(351) TSTN(351) Operand The data type of the 2nd operand is changed from BCD to BIN. For a constant, the # mark is converted to & mark. To ...

  • マニュアル

    ...) IOSP(187) None None None None None IORS(188) None IODP(189) READ(190) None None WRIT(191) None MSG(195) MSG(46) TOUT SA(210) None SA(784) SP(211) SR(212) SF(213) SE(214) None None None SE(785) SOFF(215) CJP(221) None CJP(510) CJPN(222) CJPN(511) CNR(236) CNR(545) PID(270) PID(190) RD2(280) None WR2(281) None TST(350) TST(350) TSTN(351) TSTN(351) Operand The data type of the 2nd operand is changed from BCD to BIN. For a constant, the # mark is converted to & mark. To ...

  • マニュアル

    ... variable names are displayed in the list. Select the desired variable name to register it. 35 The following variables are entered in the example in this Guide:  PTIn_Run: Input of sample program execution from the Programmable Terminal  PTIn_...

  • マニュアル

    ...CJ2M-CPU3[] FH-1050/3050 FH-1050/3050-[]0 FH-SC12/SM12 FH-SC04/SM04 FH-SC02/SM02 FH-SC/SM FZ-SC5M2/S5M2 FZ-SC2M/S2M FZ-SC/S FZ-SHC/SH FZ-SFC/SF FZ-SPC/SP FZ-SQ010F/SQ050F FZ-SQ100F/SQ100N Precautions for Correct Use As applicable devices above, the devices with the models and versions listed in Section 5.2. are actually used in this document to describe the procedure for connecting devices and checking the connection. You cannot use devices with versions lower than the versions listed in Section 5.2. To use the ...

  • マニュアル

    ...0.3 Megapixel High-Speed Camera 0.3 Megapixel Small Digital Camera 0.3 Megapixel Small Digital Pen-Shaped Camera Intelligent Compact Camera FZ-SC5M2/S5M2 FZ-SC2M/S2M FZ-SC/S FZ-SHC/SH FZ-SFC/SF FZ-SPC/...

  • マニュアル

    ... CMOS Camera 4 Megapixel High-Speed CMOS Camera 5 Megapixel Digital Camera Intelligent Camera Intelligent Compact Camera Auto-Focus Camera NJ501-[][][][] NJ301-[][][][] FH-1[][][]/ FH-1[][][]-[][] FH-3[][][]/FH-3[][][]-[][] FZ-SC/S FZ-SFC/SF FZ-SPC/...