全 2268 件が検索されました。(341 - 360件を表示)

  • マニュアル

    ... adjust the beam (e) mutual interference prevention function When 11.Output Mode is Differential output modes, (a), (b), (c) and (d) cannot be used. On/Off-delay Timer Power tuning adjustment ON button. (L100 to 1. Initial value: L100) d ...

  • マニュアル

    ...い。 *2 解除すると、 [ 0rst ] %ff を表示します。 実行によりしきい値も連動します。 しきい値の下限は-1999です。 d sp std d sp per d sp p-b d sp bar (e) 相互干渉防止機能の (d) 光軸調整したい場合投光周期設定設定状態を知りたい場合 (e) 11. 出力モードで微...

  • マニュアル

    ... indicators • SUB1 to 4: Auxiliary outputs 1 to 4 indicators • OUT1 to 2: Control outputs 1 to 2 indicators Lit for other than 0% output for linear current output. • TUNE: Lit during AT (auto-tuning). • FSP: Lit when the Fixed ...

  • マニュアル

    ...1) 13 PV变化率报警 15 16 17 ON OFF ON OFF 12 14 ON OFF 绝对值下限 绝对值下限待机序列ON SP绝对值上限 SP绝对值下限 MV绝对值上限 MV绝对值下限 SP X SP X SP L H ON OFF 5 7 L H ON OFF ON OFF 10 or-r M in-h 100 M 比例缩放上限(仅限设定模拟量输入时) ·HOLD:...

  • マニュアル

    ... indicators • SUB1 to 4: Auxiliary outputs 1 to 4 indicators • OUT1 to 2: Control outputs 1 to 2 indicators Lit for other than 0% output for linear current output. • TUNE: Lit during AT (auto-tuning). • FSP: Lit when the Fixed ...

  • マニュアル

    ...ON OFF 9 Absolute value lower limit ON OFF 10 Absolute value upper limit standby sequence ON ON OFF 11 Absolute value lower limit standby sequence ON ON OFF 12 L H SP X SP X SP L H SP L H SP X SP X SP X 0 X 0 X 0 X 0 Vary with "L", "H" values ON OFF in-h 100 Scaling Upper Limit (only when setting analog input) *6 Scaling Lower Limit (only when setting analog input) *6 ON OFF in-l 0 *6 dp 0 Decimal Point (only when setting analog input) *6 d-...

  • マニュアル

    ...变化率报警 0 比例缩放下限(仅限设定模拟量输入时) ∗6 dp 0 d-u c ∗6 °C= c °F= f ∗6 1300 ∗6 SP上限 ON OFF ON OFF L H SP X -200 ∗6 SP下限 cntl onof PID·ON/OFF 使用ON/OFF控制时= onof 使用2路PID控制时= pid ∗6 标准或加热/冷却标准控制时= stnd 加热冷却控制时= h-c ∗6 stnd ...

  • マニュアル

    ...dati di stato. Codice (H'03) che indica la fine del testo. Carattere di controllo blocco Metodo di controllo errore usato dal FINS-mini. Ogni byte dal No. nodo mediante ETX ha un valore XOR (esclusivo Numero di ingressi 4 punti max. ...

  • マニュアル

    ... value lower limit ON OFF 10 Absolute value upper limit standby sequence ON ON OFF 11 Absolute value lower limit standby sequence ON ON OFF 12 LBA (only for alarm 1) ptrn X SP X SP L H SP L H X cp *6 c-cp ...

  • マニュアル

    ...ブア SID No. ドレス 0 0 MRC SRC 0 0 5 0 3 ノード サブア No. ドレス 1 入力点数 最大4点マルチSP、バンク選択(-Hタイプのみ)、RUN/STOP、AUTO/MANUAL、 機能プログラムリセット/スタート、正逆反転、SPモード切替、100%AT実行/中止、 40%AT実行/中止、設定変更許可/禁止、通...

  • マニュアル

    ... not exceed the allowable operating temperature given in the specifications, especially when two or more Controllers are mounted. Front Panel Part Names and Functions (1) (3) Displays the process value (PV) or parameter. (2) Display No. 2 Displays the set point (...

  • マニュアル

    ..., correct the wiring and cycle the power supply. Alarms (Alarms are output from auxiliary outputs.) Setting *1 Alarm type 0 No alarm function 1 Deviation upper/lower limit 2 Deviation upper limit Alarm output function Output off ...

  • マニュアル

    ... setting 0 analog input) M °C= c d-u Temperature °F= f Unit M c-cp 20 M orev or-r M alt1 1300 alh1 sl-l -200 4-20 SP Lower Limit trst Step Time/Rate of Rise Programming M off Deviation upper/lower limit Deviation upper limit Deviation upper/lower range ON OFF Deviation upper/lower limit standby sequence ON 6 Deviation upper limit standby sequence ON Deviation lower limit standby sequence ON ...

  • マニュアル

    ... lower limit standby sequence ON 12 LBA (only for alarm 1) 13 PV Change Rate Alarm 5 ON OFF ON OFF ON OFF ON OFF ON OFF ON OFF 14 SP absolute value upper limit ON OFF 15 SP absolute value lower limit ON OFF 16 MV absolute value upper limit ON OFF 17 MV absolute value lower limit ON OFF L H ...

  • マニュアル

    ...OFF Absolute value lower limit ON OFF 10 Absolute value upper limit standby sequence ON Absolute value lower limit standby sequence ON ON OFF LBA (only for alarm 1) 13 PV Change Rate Alarm X SP X SP L H ...

  • マニュアル

    ...Deviation upper limit Deviation lower limit *1 4 Deviation upper/lower range *1 5 Deviation upper/lower limit standby sequence ON 6 7 Deviation upper limit standby sequence ON Deviation lower limit standby sequence ON ...

  • マニュアル

    ...OFF ON OFF 9 Absolute value lower limit Absolute value upper limit standby sequence ON Absolute value lower limit standby sequence ON ON OFF LBA (only for alarm 1) 13 PV Change Rate Alarm 14 SP absolute value upper limit ON OFF ON OFF 15 ...

  • マニュアル

    ...Absolute value lower limit ON OFF 10 Absolute value upper limit standby sequence ON Absolute value lower limit standby sequence ON ON OFF 12 LBA (only for alarm 1) 13 PV Change Rate Alarm X SP X SP L H ...

  • マニュアル

    ... lower limit ON OFF 10 Absolute value upper limit standby sequence ON ON OFF 11 12 13 Absolute value lower limit standby sequence ON LBA (only for alarm 1) PV Change Rate Alarm 14 SP absolute value upper limit ON OFF 15 ...

  • マニュアル

    ...alh2 0 0 6FDOLQJ/RZHU/LPLW RQO\ZKHQVHWWLQJDQDORJLQSXW 0.0 0.0 Hold down for at least VHFRQGV Decimal Point RQO\ZKHQVHWWLQJDQDORJLQSXW bank 7HPSHUDWXUH8QLW ƒ& c ƒ) f &VWDQGVIRU&HOVLXV)IRU)DKUHQKHLW 0 sp...