全 367 件が検索されました。(321 - 340件を表示)

  • マニュアル

    ... 0000. • Status: Contains 0000. Note The decimal point position has to be managed by the user since the Digital Panel Meter’s decimal point position is not transferred in SYSWAY (X format) communications. Status (Offset: +3, +6, and +9) The read data area’...

  • マニュアル

    ... each time the instruction is executed. • The bytes of source data shown below will be sent in the following order. If most significant bytes first is specified (0): 12345678.. If least significant bytes first is specified (1): 21436587.. S S+1 S+2 ...

  • マニュアル

    ...-type Pulse Input Unit CS1W-PPS01 This function counts the number of pulses per time unit and converts the number to an instantaneous value (pulses/time unit). Any of the following time 17 Section 1-2 Features and Functions units can be selected: 1 ...

  • マニュアル

    ... SYSMAC WAY. (SYSMAC WAY) 34 PLC CS S i Series Usage Special high-speed communications protocol for Programming Devices Standard protocol for general-purpose host computers Cable connection Connect to the PLC’s peripheral o ...

  • マニュアル

    ...045). (An FCS check error or frame error occurred 3 times in a row. A response was not returned after sending data to the Controller for a ES100X Controller Terminal (Block Model 045). (Response was not returned for 5 ...

  • マニュアル

    ... number: 63 Slave’s network address: 1 Slave’s node number: 2 Section 6-3 Explicit Message Communications CMND(194) Operand Details [CMND S D C] • Command Words Word S S+1 S+2 S+3 S+4 S+5 Contents Function (Hex) 28 01 EXPLICIT MESSAGE SEND command code = 2801 (Hex) 02 1C Slave node number = 02 (Hex) READ BYTE DATA command service code = 1C (Hex) 00 2F Class ID = 002F (Hex) 00 01 Instance ID = 0001 (Hex) specifies data area 0A 00 Starting read address = 000A (Hex) specifies IR 010 Address L = 0A (Hex); Address H = 00 (...

  • マニュアル

    ...S D D Local node S 1st response word Remote Master Unit CPU Unit Interpretation1 Interpretation2 Command data Response No. of command bytes Response Response monitoring time ...... S+2 S+3 S+4 Command Destination node Local Master Unit CPU Unit S+1 Operands C: Control code S: 1st source word D: Destination information Execution L Execution ... Response data 1: For commands addressed to Master Unit 2: For commands addressed to CPU Unit Description IOWR transfers data from the words beginning at S to the specified Special I/ O Unit. The control code (C) specified parameters for the instruction as ...

  • マニュアル

    ...Node address 2: OUT size: 1 byte, IN size: 2 bytes 15 Allocation size setup table I 1 5 s I+1 4 3 s+1 I+2 1 2 s+2 : : s+3 OUT block 1 15 k 00 00 01 01 k+1 00 00 01 01 k+2 02 k+3 Not usable : k+4 00 Not usable 01 01 Not usable 01 02 k+5 l: First word of the allocation size setup table s: First word of OUT block 1 k: First word of IN block 1 Note 00 IN block 1 00 Not usable :...

  • マニュアル

    ... and executes that program. OK OK OK OK OK OK OK OK MACRO MCRO/ @MCRO 099 Calls the subroutine with the specified subroutine number and executes that program using the input parameters in S to S+3 and the output parameters in D to D+3. OK OK OK OK OK OK OK OK SUBROUTINE ENTRY SBN 092 Indicates the beginning of the subroutine program with the specified subroutine number. OK OK OK OK OK OK OK OK SUBROUTINE RETURN RET 093 Indicates the end of a subroutine program. OK OK OK OK OK OK OK OK GLOBAL SUB- ...

  • マニュアル

    ... down differentiation. • Use the MSKS(690) instruction to enable the interrupt inputs in counter mode. Use control data (N) settings 6 to 9 to specify interrupt inputs IN0 to IN3. Set S=2 to start a decrementing counter and enable the interrupts. Set ...

  • マニュアル

    ...&RQWDLQV ‡ 'LVSOD\YDOXHVWDWXV &RQWDLQV Note The decimal point position has to be managed by the user since the Digital Panel Meter’s decimal point position is not transferred in SYSWAY (X format) communications. Status (Offset: +3, +6, and +9) The read data area’...

  • マニュアル

    ... and Other Software Relevant ITEMs in the System Common Block (block model 000) ITEM type Parameter ITEM 050 Data contents HMI EM bank number 051 Input HMI function's operation cycle (s) 1 (0.1 s), 2 (0.2 ...

  • マニュアル

    ...address automatically. When necessary, check the status of the Mail Send Function by checking the Send Mail Status words (m and m+17 of the DM Area words allocated to the Ethernet Unit as a CPU Bus Unit) from the ladder program. The send condition'...

  • マニュアル

    ...(Block Model 045). (An FCS check error or frame error occurred 3 times in a row. A response was not returned after sending data to the Controller for a ES100X Controller Terminal (Block Model 045). (Response was not returned for 5 ...

  • マニュアル

    ...2.2 µs Example: CS1H-CPU63H Input variables with a 1-word data type (INT): 3 Output variables with a 1-word data type (INT): 2 Total instruction processing time in function block definition section: 10 µs Execution time for 1 instance = 6.8 µ...

  • マニュアル

    ... intervals whether or not the connected device is turned ON. Keep this in mind when measuring total ON times for inputs of less than 1 s. ■ Measuring an ON Time of 0.5 s As shown in Figure A, the actual ON time is 1.5 ...

  • マニュアル

    ... (block model 000) ITEM type ITEM Data contents Data range Default Parameter 050 HMI EM bank number 0 to C (Hexadecimal) 0 051 HMI function's operation cycle (s) 1 (0.1 s), 2 (0.2 s), 3 (0.5 s), 4 (1 s), or 5 (2 s) Note: Always stop operation before changing this ITEM. 1 to 5 4 (1 s) 056 Reception stop switch 0: Normal; 1: Stop reception 0 or 1 0 057 Transmission stop switch 0: Normal; 1: Stop transmission 0 or 1 0 059 HMI function disable switch 0: Used; 1: Not used 0 ...

  • マニュアル

    .... 5 to 8.4 Hz with 3.5 mm single amplitude and 8.4 to 150 Hz with 9.8 m/s² for 10 times each in X, Y and Z directions Shock resistance (during operation) Conforms to IEC 60068-2-27. 147 m/s², 3 times each in X, Y and Z directions Material finish Applicable for model-ID NYM£££-££1££ *1 Nickel plated conforms to ASTM B733-15, SC2 Degree of protection Front of product: IP65 *3 Pollution degree 2 or less: Conforms to JIS B3502 and IEC 61131-2 *1. *2. *3. 4-18 Refer to ...

  • マニュアル

    ... directions. Conforms to IEC 60068-2-6. • For a Panel PC with one or more HDD storage devices the Panel PC must be installed in a vibration free environment. *3 Shock resistance (during operation) Conforms to IEC 60068-2-27. 147 m/...

  • マニュアル

    ... variables 8 4 10 Total size of variables 600 bytes 200 bytes 1,000 bytes Calculate the variable access time as shown below. [(600 + 200 + 1,000) bytes × 0.0006 s] + [(8 + 4 + 10) variables × 0.100 s] + 3...