全 7847 件が検索されました。(2761 - 2780件を表示)
- マニュアル
...Terminal (which consists of an NX-series EtherCAT Coupler Unit and NX Units), and information on hardware, setup, and functions to set up, control, and monitor NX Units through EtherCAT. NA-series Programmable Terminal Hardware User’s Manual V117 NA5-□...
- マニュアル
...NX-series EtherCAT Coupler Unit and NX Manual NX-series EtherCAT Coupler Application Units), and information on hardware, setup, and functions to set up, control, and monitor NX Units through EtherCAT. NA-series Programmable V117 Terminal Hardware User’s NA5-□...
- マニュアル
... NX1P are displayed in the I/O Map. 2. Double-click an I/O port to enter a variable name. Set variable names for input/output terminals as shown below. Variable names for input terminals Variable names for output terminals Terminal No. R/...
- マニュアル
... table I/O points 10 points 14 points 20 points 30 points 40 points 60 points CP1E-E CP1E-N Normal-type 66×90×85 86×90×85 86×90×85 130×90×85 150×90×85 195×90×85 Dimensions (W x H x D) CP1E-ES CP1E-NS(1) Renewal-type 86×90×79 86×90×79 130×90×79 150×90×79 195×90×79 CP2E 86×90×80 86×90×80 130×90×80 150×90×80 195×90×80 2.2. Mounting The DIN track and screw hole dimensions are the same as for the CP1E. I/O points 10 points 14 points 20 points 30 points 40 points 60 points 100 mm Mounting hole pitch ...
- マニュアル
.... To write the configured data to the control module, the PC and the remote I/O converter must be properly connected. Installing R7CON ① Start Windows. ② Download the Configurator Software from the website of MG Co., Ltd. Institute (https://www.mgco.jp/download_...
- マニュアル
... 14 points or more. Dimension comparison table I/O points CP1L-L/M 66×90×85 86×90×85 86×90×85 130×90×85 150×90×85 195×90×85 10 points 14 points 20 points 30 points 40 points 60 points Dimensions (W x H x D) (mm) CP1L-EL/EM 130×90×85 130×90×85 150×90×85 - CP2E 86×90×80 86×90×80 130×90×80 150×90×80 195×90×80 2.2. Mounting The DIN track and screw hole dimensions are the same as for the CP2E except CP1L-EL20. I/O points CP1L-L/M 56±0.5 76±0.5 76±0.5 120±0.5 140±0.5 185±...
- マニュアル
... that case, use the equivalent procedures described in this guide by referring to the Sysmac Studio Version 1 Operation Manual (Cat. No. W504). Precautions for Correct Use Turn ON the terminating resistance switch on the Serial Communications Unit and connect 120 Ω (1/2 ...
- マニュアル
... message setting screen> ●Detection of normal message and error message This protocol macro data detects a normal message or an error message based on the response code of the receive message. ●Settings of RV PRO_R receive message (normal message)
++”00”+&(... - マニュアル
...#ss Conduction Time first byte at error #16#tt Conduction Time second byte at error #16#uu Conduction Time third byte at Operation Log error (Operation Code: : : Conduction #16#vv Operation code 10 Time) #16#...
- マニュアル
... types are used for the Smart Camera. ■Definition of the data type to access the signals (Union) This data type is used to access the control signals and status signals. Data type name Base type U_EIPFlag UNION F BOOL[32] ...
- マニュアル
... describes the settings of the receive message. Additional Information Refer to 3-4 Communication Message Attributes of the CX-Protocol Operation Manual (Cat. No. W344) for details on receive message settings. [Receive message setting screen] ●Setting of receive message RV_RDCODE
(... - マニュアル
... describes the settings of the receive message. Additional Information Refer to 3-4 Communication Message Attributes of the CX-Protocol Operation Manual (Cat. No. W344) for details on receive message settings. [Receive message setting screen] ●Setting of receive message RV_RDCODE
(... - マニュアル
... describes the settings of the receive message. Additional Information Refer to 3-4 Communication Message Attributes of the CX-Protocol Operation Manual (Cat. No. W344) for details on receive message settings. [Receive message setting screen] ●Setting of receive message RV_RDCODE
(... - マニュアル
... describes the settings of the receive message. Additional Information Refer to 3-4 Communication Message Attributes of the CX-Protocol Operation Manual (Cat. No. W344) for details on receive message settings. [Receive message setting screen] ●Setting of receive message RV_RDCODE
(... - マニュアル
... the tag data links of Destination Device. ■Definition of the data type to access the signals (Unions) This data type is used to access the control signals and status signals. Data type name Data type U_EIPFlag UNION F BOOL[32] ...
- マニュアル
...EIP002_Status_IN [15] to [0] 15 14 13 12 11 10 9 Resv Resv Resv Resv Resv Resv Resv 8 7 6 5 4 3 2 1 0 RF_W SYS_ RF_E CMD_ NOR READ FRIC ERR BUSY AR ERR RR ERR M Y Precautions for Correct Use If the data size of tag data links for Destination Device is an odd-numbered byte, use BYTE type to define, do not use BOOL type. Additional Information With Sysmac Studio, two methods can be used to specify an array for a data type. After specifying, (1) is converted to (...
- マニュアル
...Command Data : D10019 ■Details on input area Address D10100 Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0 RF_W SYS_ RF_E CMD_ NOR READ Resv Resv Resv Resv Resv Resv Resv FRIC ERR BUSY AR ERR RR ERR M Y D10101 Error Code D10102 Response Information 1 D10103 Response Information 2 D10104 : Response Data D10119 Additional Information For the allocation of tag data links of RFID Reader/Writer, refer to Memory Assignments in EtherNet/IP Communications Protocol in Section 5. Host Communications Specifications of the V680S Series User’s Manual (...
- マニュアル
.... ・Error message: Receive messages with 2 characters beginning with E ・Normal message: Receive messages except for the above (A receive message is identified using a receive matrix.) : All the other messages except for the above ●RV_VR receive message setting (Normal message)
(... - マニュアル
... data types are used for tag data links to communicate with Sensor Controller. ■Defining a data type for signal access (Union) Data type to access control signals and status signals Data type name Data type U_EIPFlag UNION F BOOL[32] ...
- マニュアル
...+ 2 SDA- 3 SDB+ 4 FG 5 Terminal block Terminating resistance Terminal Signal RS-485 No. name interface 13 B(+) 14 A(-) Terminal block *Connect 120 Ω (1/2 W) terminating resistance between B(+) and A(-) of the Digital Temperature Controller that is connected at the end of the network. Additional Information For information on the connector configurations and pin assignments of the other models, refer to their respective manuals. 10 7.Serial Communications Connection Procedure 7. Serial Communications Connection Procedure This section describes the procedures for connecting the PLC to the Digital Temperature Controller via serial communications. The ...