全 2741 件が検索されました。(2481 - 2500件を表示)
- マニュアル
... included with the CPU Unit or an equivalent connector to connect to the DeviceNet transmission line. 5. PC Status Indicators The following indicators show the operating status of the PC. Indicator PWR (green) RUN (green) ERR/ALM (red) ...
- マニュアル
... PC. Connector Pin Assignments CJ/CS/CQM1H Signal 9 SG 8 NC 7 NC 6 NC 5 CTS 4 RTS 3 RXD 2 TXD 1 NC (On Simple Communications Unit) FG Pin 1 SD Simple Comm. Unit Cable connections and Signal directions Signal Pin --- 1 2 ...
- マニュアル
.... When constructing an intranet, communication failure may occur due to cable disconnection or the influence of unauthorized network equipment. Take adequate measures, such as restricting physical access to network devices, by means such as locking the installation area. When using a device equipped with the ...
- マニュアル
... mm (W × H × D) Conform to general specifications for the SYSMAC CJ Series. 14 Section 1-4 Specifications 1-4-2 Dimensions CS1W-ETN21 ETN21 100M ERH TCP FTP HOST RUN ERC SD RD LNK UNIT NO. 0 1 ×161 ×160 130 NODE NO. 0 100BASE-TX 10BASE-T 35 101 (Unit: mm) CJ1W-ETN21 Back Front • Unit Version 1.5 or Later ETN21 65 31 2.7 2.7 31 • Unit Version 1.4 or Earlier ETN21 ERC ...
- マニュアル
...Weight Dimensions 200 g max. 35 × 130 × 101 mm (W × H × D) 11 Section 1-4 Specifications 1-4-2 Dimensions CS1D-ETN21D ETN21D 100M ERH TCP RUN ERC SD RD LNK DPL UNIT NO. 0 1 ×161 ×160 130 NODE NO. 0 100BASE-TX 10BASE-T 35 101 (Unit: mm) 1-4-3 Software Configuration The software supported by the Ethernet Unit runs in the layers shown in the following diagram. The components that form the various layers are defined below the diagram. CS-series CPU Unit CS-series CPU Unit FINS communication service 7....
- マニュアル
...given below. Connector Pin Arrangement The pin arrangement for the CPU Unit connector is shown below. Pin number 1 2 3 4 5 6 7 8 9 Metal cap Signal abbreviation FG SD (TXD) RD (RXD) RS (RTS) CS (CTS) 5V DR (DSR) ER (DTR) SG (0V) FG CS-series Pin Arrangement Signal direction --Output Input Output Input --Input Output ----- CJ-series Pin Arrangement 5 1 1 5 9 6 Signal name Frame ground Send data Receive data Request to send Clear to send Power supply Data set ready Data terminal ready Signal ground Frame ground 6 9 13 Connecting ...
- マニュアル
...164 174 188 78 Terminating resistance selector switch RS422 63 Approx. 140 10 dia. Appendix B Link Adapter Specifications Internal Structure RS-232C Pin Name 1 FG 2 SD 3 RD 4 RS 5 CS 6 DR 7 SG 8 CD 20 ER ● CTS (CS) Selector Set to 0 V to have the clear-to-send (CTS) signal always ON. Set to external to receive an external CTS signal. ● Terminating Resistance Selector When set to ON, connects the builtin terminating resistance (220 Ω); when set to OFF, disconnects it. ● Power Supply Connection RS-422 OR/ Switching circuit External CTS Selector 0V...
- マニュアル
...Functions is also allocated in the CPU Bus Unit System Setup Area. 4 Section 1-2 Specifications Dimensions (Same for All Units) Front Side Version 1.4 or Lower Version 1.5 or Higher 2.7 2.7 SD RD LNK TCP FTP HOST EF012 ABCD SW SETTING BATTERY EF01 ABCD EF01 2345 1 x16 ERC ...
- マニュアル
... by yourself. • When constructing network infrastructure, communication failure may occur due to cable disconnection or the influence of unauthorized network equipment. • Take adequate measures, such as restricting physical access to network devices, by means such as locking the installation area. • When using devices equipped with an ...
- マニュアル
... Windows, Visual Basic and Visual Studio are either registered trademarks or trademarks of Microsoft Corporation in the USA and other countries. • EtherCAT® is registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany. • ODVA, CIP, CompoNet, DeviceNet, and EtherNet/IP are trademarks of ODVA. • The ...
- マニュアル
..., Visual Basic, and Microsoft Edge are either registered trademarks or trademarks of Microsoft Corporation in the United States and other countries. • EtherCAT® is registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany. • ODVA, CIP, CompoNet, DeviceNet, and EtherNet/IP are trademarks of ODVA. • The ...
- マニュアル
..., Windows, Excel, and Visual Basic are either registered trademarks or trademarks of Microsoft Corporation in the United States and other countries. • EtherCAT® is registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany. • ODVA, CIP, CompoNet, DeviceNet, and EtherNet/IP are trademarks of ODVA. • The ...
- マニュアル
... Basic, and Microsoft Edge are either registered trademarks or trademarks of Microsoft Corporation in the United States and other countries. • EtherCAT® is registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany. • ODVA, CIP, CompoNet, DeviceNet, and EtherNet/IP are trademarks of ODVA. • The ...
- マニュアル
... Windows, Visual Basic and Visual Studio are either registered trademarks or trademarks of Microsoft Corporation in the USA and other countries. • EtherCAT® is registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany. • ODVA, CIP, CompoNet, DeviceNet, and EtherNet/IP are trademarks of ODVA. • The ...
- マニュアル
... Windows, Visual Basic and Visual Studio are either registered trademarks or trademarks of Microsoft Corporation in the USA and other countries. • EtherCAT® is registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany. • ODVA, CIP, CompoNet, DeviceNet, and EtherNet/IP are trademarks of ODVA. • The ...
- マニュアル
... mode 54321 Secondary internal circuit Antenna terminal (ANT1) Serial Master Station Secondary internal circuit Serial Master Station D-sub, 9-pin, Female End at WT30 Pin No. Signal I/O direction ----1 2 RD Output 3 ...
- マニュアル
...Conform to EIA RS-232C Section 2-1 E5ZD-4jjj-E/-6jjj-E Hardware • Signal connections: Signal name Symbol Direction Pin Field ground FG NA 1 Signal ground SG NA 7 Send data SD Output 2 Receive data RD Input 3 Send request RS Output 4 Send enable CS Input 5 Data set ready DR Input 6 Data terminal ready ER Output 20 As shown below 13 1 25 14 RS-232C Pin Assignments • Connection diagram: As shown below You cannot connect the host computer directly to more than one E5ZD Unit via the RS-232C connectors. Host computer RS-...
- マニュアル
...-V is used. Signal g name Signal direction Abbr. Input Pin no. Output Safety ground or earth ground GR --- --- 1 Signal ground or common return line SG --- --- 7 Send data SD --- Required 2 Receive data RD Required --- 3 Request send RS --- Required 4 Can send CS Required --- 5 Data terminal ready ER --- Required (20) ID Controller Host computer GR FG SG SG ...
- マニュアル
... below shows the pin assignment for the RS-232C connector on the rear panel of the Visual Controller. Pin number Old JIS code New JIS code Pin connection 1 2 Pin name GND --- Connector top view TXD SD Transmitted Data 3 RXD RD Received Data 4 RTS RS Request to Send 5 CTS CS Clear to Send 6 DSR DR Data Set Ready 7 GND SG Signal Ground 8 NC NC Protective Ground 9 (+14V) 10 (–14V) 20 DTR ER Data Terminal Ready Note Pin 9 and Pin 10 are used exclusively for the power supply of the Keyboard...
- マニュアル
... EIA RS-232C. Communications Signals 1 13 25 14 Signal Abbreviation Signal direction Pin no. Frame ground (safety ground) FG ––– 1 Signal ground or common return SG ––– 7 Send data SD Output 2 Receive data RD Input 3 Request to send RS Output 4 Clear to send CS Input 5 Data set ready DR Input 6 Data terminal ready ER Output 20 Connection Diagram The following diagram shows how the E5AX is connected to the host computer using the RS-232C. Host computer RS-232C Abbreviation E5AX RS-232C Pin no. Pin Abbrevino. ation 1 1 FG SG 7...