全 2741 件が検索されました。(2461 - 2480件を表示)
- マニュアル
...lADRS O 1 1` Bitl5 ⇒ Command execution Bito n:Firstailocatedword athroughd:Arbitraryda槍 ADRS:Unitaddresswheredataisl◎cated. READDATA:DatareadfromUnit, _一一:Variable Monitoring (CommandCode:3) Readsthe4-digithexadecimal"readdata"fromthespecifiedaddressinthe High-speedCounterUnit.Thespecifiedaddressis2-digithexadecimal:00to ...
- マニュアル
...億躍窪馳患 」 △Cauti。 n WiringDiagrams lBMPC/ATComputer Femaie9-pin RS-232Cconnector AlwaysconnecttheCV500-CIFOItothecomputerbeforecomectlngittothe CPU.ElementsinsidetheCPUmaybedamagedifthecableisconnectedtothe CPUfirst. AnadapterisrequiredtoconnecttheCV500-CIFOIcabletoacomputer.Wire theadapterasshownbelow. IBMPS/2Computer Female25-pln Computer CV500・CIFO1 3 ...
- マニュアル
...-V1 Master Unit for CS-series, C200HX/C200HG/C200HE-(Z)E, and C200HS PLCs Section 4-1 Indicators The following table shows the meaning of the indicators. Indicator RUN (green) Status ON Meaning The Unit is operating normally. OFF ...
- マニュアル
...these specifications can be connected. Connector Pin Assignments Pin assignments for the RS-232C port are given in the following table. Pin 1 6 9 5 Abbreviation Name Direction 1 FG Field ground --- 2 SD...
- マニュアル
...-point Transmission distance 15 m max. Interface Complies with EIA RS-232C Connector Pin Assignment Connectors Specification Pin No. Signal name Abbreviation Signal direction 1 Safety ground FG – 2 Send data ...
- マニュアル
... match the external device interface. C200H-ASC11/21 1 C200H-ASC31 6 9 9 6 5 5 Pin 1 Symbol Name Direction Frame ground Comments 1 FG - 2 SD Send data Output 3 RD Receive data Input 4 RTS Request to send Output 5 CTS Clear to send Input 6 - Not used - Only for terminal port of C200H-ASC31. 5V 5V output Output Other ports 7 DSR Data set ready Input 8 DTR Data terminal ready Output 9 SG Signal ground - Hood FG Frame ground - RS-232C Interface Specifications Item Specifications Electrical characteristics Conform to EIA RS-232C Synchronization...
- マニュアル
... CJ-series PLCs, one for the C200HX/HG/HE PLC, and one for CQM1H-series PLCs. Item Model Specifications CJ1W-CLK23 CJ1W-CLK21-V1 CS1W-CLK23 CS1W-CLK21-V1 External appearance C200HW-CLK21 CLK21 RUN ERC INS ...
- マニュアル
...-sub connector (female) IBM PC/AT or compatible Connect as shown below. Connector for the personal computer IBM PC/AT Computer Female 25-pin CV500-CIF01 Female 25-pin RS-232C Connector Computer 2 SD 3 ...
- マニュアル
... for the personal computer 24 Connecting the Teaching Box Section 3-2 Wire the following. RS-232C MC Unit side (20 pins) Personal computer side (9 pins) 1 Connector hood 2 RD 2 3 SD 3 7 RS 4 8 CS 5 5 SG 6 6 DR 7 4 ER Connector hood 8 9 10 11 12 Shielded wires (see note) 13 14 15 16 17 18 19 20 Note Connect the shielded line to the FG (pin 1) at the computer, and to the connector hood at the MC Unit. 3-2 Connecting the Teaching Box The procedure ...
- マニュアル
... I/O Unit 39 Unit Components Section 2-2 2-2-7 Communications Adapter Components CPM1-CIF01 RS-232C Adapter 1. Mode Setting Switch 3. RS-232C port RS-232C Port Pin Allocation FG 1 6 DCD SD 2 7 DSR RD 3 8 DTR RTS 4 2. Connector 1, 2, 3... 9 SG CTS 5 1. Mode Setting Switch Set this switch to “HOST” when using a Host Link system to connect to a personal computer. Set this switch to “NT” when connecting to a Programmable Terminal or PC for 1:1 PC Link. 2. Connector Connects to ...
- マニュアル
.... Indicator PWR (Green) ( ) Display ERC (Red) ON OFF ON OFF ON Flashing OFF ON OFF ON OFF ON COMM (Yellow) OFF Flashing RUN ((Green)) ERR ((Red)) SD ((Yellow)) RD ((Yellow)) OFF 16 2-2 Status Power is being supplied. Power is not being supplied. In RUN mode or MONITOR mode In PROGRAM mode or fatal error has occurred. Fatal error has occurred. Non-fatal error has occurred. Normal operation CompoBus/S data is being sent. Data is not being sent. CompoBus/S data is being received. Data is not being received. A CompoBus/S communications error has occurred. Normal ...
- マニュアル
...tOve1⊂1・.\ 題F㎞!St。 P ・:一目Remote!Loca■ :一目Execute/OartC6i、/ ㌧翻Movet。 ㎞e口 :圏s。 `』‥・・ゼ\ 羅刹 .、端子拠L畦.,,,.ゴ・・*・・ }.・ TerptSrt,.'ChaCtictrocleW −L愈臨,Ad』≧.Date 》 `SD(Dt)-1 'SDΦ2)1 SDΦ3)1 ...
- マニュアル
... 25-pin Connector Adapter required for 9-pin connector. Section Formatting Floppy Disks 2-2 2-1-4 Preparing the Connecting Cable Personal Computer with D-sub 9-pin RS-232C Connector PCU or CPU Unit Personal computer ...
- マニュアル
...35 15 101 (16.5 including cover) (Unit: mm) 130 CS1W-ETN11 35 101 (Unit: mm) 9 Section 1-6 Software Configuration CJ1W-ETN11 65 2.7 31 ETN11 RUN ERC SD RD ERH TCP FTP EF012 6789 345 ABCD EF012 6789 345 TS UNIT No. NODE No. x161 ABCD EF012 6789 345 ABCD 90 x160 2.7 ETHERNET 1-6 (Unit: mm) Software Configuration The software supported by the Ethernet Unit runs in the layers shown in the following diagram. The components that form the various layers are defined below the diagram. Memory Card/ EM File Memory CS/CJ-...
- マニュアル
... Units RS-232C Connector Pin Arrangement (Same for Ports 1 and 2) Pin No. Symbol Signal name Signal direction RS-232C Unit ↔ External devices 1 2 --RD Not used Receive data --← 3 4 SD --- Send data Not used → --- 5 6 SG --- Signal ground Not used ----- 7 8 RS CS Request send (See note.) Can send (See note.) → ← 9 --- Not used --- Note The CS signal is always checked. Data will not be output if CS is not connected. Short-circuit the RS-CS signals when they are not used. A connection example using applicable connectors and recommended cables is provided ...
- マニュアル
... a Programming Device (including Programming Consoles), host computer, or standard external device. 12. RS-232C Port Connects the PC to a Programming Device (excluding Programming Consoles), host computer, Programmable Terminal, or standard external device. RS-232C Port Pin Allocation FG 1 ...
- マニュアル
...RS-232C cable Wiring Connect the Units with the cables wired as shown below. CQM1H CQM1H or another C–series PC Signal Abb. Pin No. Pin No. Signal Abb. FG Hood Hood FG SD 2 2 SD RD 3 3 RD RTS 4 4 RTS CTS 5 5 CTS – 6 6 – – 7 7 – – 8 8 – SG 9 9 SG Recommended Cables UL2464 AWG28x5P IFS-RVV-SB (UL-approved, Fujikura Ltd.) AWG28x5P IFVV-SB (not UL standard) (not UL-approved, Fujikura Ltd.) UL2464-SB (MA) 5Px28AWG (7/0.127) (UL-approved, Hitachi Cable, Ltd.) CO-MA-VV-SB 5Px28AWG (7/0....
- マニュアル
..., does not cover baud rates above 19.2 Kbps. Refer to the manual for the device being connected to confirm support. Connector Pin Layout Pin No. Note Abbreviation Signal name I/O 1 (See note 1.) 2 FG SD...
- マニュアル
... inclusion) Orange Lit Not lit Unit is part of Network. Unit is not part of Network. M/S (polling node) Orange Lit Not lit Unit is polling node. Unit is not part of Network or is polled node. SD (send) Orange Lit Not lit Unit is sending data. Unit is not sending data. RD (receive) Orange Lit Unit is receiving data. LNK (data link) Orange Not lit Lit Unit is not receiving data Unit is part of active data link. Flashing Data link error has occurred. Rapid flash- Data link table communications cycle time is too short. ing Not ...
- マニュアル
... interface error, EEPROM error, unit number error, I/O table not set, duplex communications setting error, or duplex settings incomplete INS (network participation) Yellow Not lit Lit No error. Unit is participating (inserted) in the network. Not lit ...