全 2741 件が検索されました。(2441 - 2460件を表示)
- マニュアル
... 9-pin RS-232C interface and the ID Controller has a 25-pin RS-232C interface.) The following diagram shows the pin assignments and cable connections. Pin Signal Setting Communications Parameters Signal Pin 1 FG FG 1 2 ...
- マニュアル
...Transmissionspeedisseiectableupto9600baud. 19 ---------------------[End of Page 8427]--------------------- 庇伽o戒Sεr吻εU漉オ Section2Pt6 ThetWoserialportsOntherearoftheUnithavepinassignmentSaSde● scribedinthefollowingtable.●『hisinforrnationcanbeusedtobuildacabie betWeentheNetWorkServiceUnitandaserialdevicesuchasamodem. PmNo. SlgnalAbbr. SlgnalNamg SlgnalDlrgctlon Notgs 7 SG C◎mmonReturnLine Bilateral (PlnlisFG) 2 ...
- マニュアル
...-232Cgnterface WhenusinganopticalfibercableorRS-422cable,severalHostLinkUnits canbecomectedtoonehostcomputer.WhenRS-232Ccablesareused, however,theconnectionmustbemadeonaone-to-onebasis,oraLink AdaptermustbeusedtoconverttoRS-422cableoropticalfiberoable.(See AppendixBSpecifica施ηsortheL加kAdaptermanualsfordetails).Thetable belowgivestheproperconnectionsforanRS-232Cinterface. 官Signal Symbol PinNo. FrameGround FG 1 SlgnalGround SG 7 SendData ...
- マニュアル
...-RS-232C standards. Signal directions are oriented from the point of view of the ASCII Unit. Pin No. 1 13 1 13 108 14 Symbol Name Direction 1 FG Frame ground 2 SD Send data Output 3 RD Receive data Input 4 RTS Request to send Output 5 CTS Clear to send Input 6 DSR Data send ready Input 7 SG Signal ground 8 to 19 --- Not used 20 DTR Data terminal ready 21 to 25 --- Not used 25 14 25 Output Appendix B Specifications Connections to Peripheral Devices ASCII Unit FG 1 Printer 1 FG SG 7 7...
- マニュアル
...STOOOO一 ACOOO1 TNOOOO ST◎001●一 ACOOO2 Whenastepbecomesactive,itwillnormallyremainactiveforatleastoneexecutioncycleeveniithetransitionconditionismetforactivestatustom◎veto thenextstep.Ifyouwisり,however,youcanuseanactionqualifier(AQ}topre・ ventexecutionduringthefirStexecutiOnCycle. NoteWhenactivestatusistransferredfromonesteptoanother,thestepthatbecomesinactiveisreset,Le.,theactionsassociatedwiththatsteparereset.Ifyou wishyoucanaddtheoptionalAQsymbolH(forhold)tocertainAQs(N,P,L,D, andR>topreventoutputsortimersfrombeingresetafterexecutionofanaction iscomplete.lnadditjon,S-groupAQs(S,SL,...
- マニュアル
...Tool Bus Connections IBM PC/AT Computer Female 9-pin RS-232C connector IBM PS/2 Computer Female 25-pin RS-232C connector Female 25-pin Female 25-pin Computer CV500-CIF01 Computer CV500-CIF01 3 SD 2 SD 1 FG 1 FG 2 RD 3 RD 2 ...
- マニュアル
...isks(*紳*)」tisnotpossibletoenterdatainblankspaces.Movethecursortoa blankIineandpresstheFgkeytodisplayasterisksinthespacestopermitdata tobewri廿en.ThecursorcanonlybemovedtothetopblankIine。 WrltlngA◎ 1,2,3..。 1.MovethecursortotheAQcolumnwheretheasterisks(****)aredisplayed andpresstheEnterKey.TheAQtablewilibedisplayedattheIeftofthe screen. 2.SelecttherequiredAQwiththecursorandpresstheEnterKey.↑heAQ tablewilldisappearandtheselectedAQwillbedisplayedatthecursorp◎sト tion.ThecursorwillmOvetOtheSVcolumn. orPresstheEscKeyorShift+EscKeystocanceltheAQinput,ThishidestheAQ tableandlocksthecursorintheactionblock. WritingSV AnSVmustbeinputwhenoneofthefollowingAQiswritten:D,DH,LLH,...
- マニュアル
... on the Backplane. 26 Section 3-1 Remote I/O Master Units Indicators CV500-RM221 (Wired) CV500-RM211 (Optical) RUN RUN Indicator RUN Color Green ERC ERT ERC ERH ERL ERH SD CD SD CD T/R TS T/R TS Indication Operating status T/R Orange Data transfer status TS Orange Test status ...
- マニュアル
...Viewed from the PC. Maximum cable length: 15 m Host interface pin Signal No. Connector hood Frame ground Symbol FG Direction of signal --- 9 Signal ground SG (GND) --- 2 Send data SD (TXD) Output 3 Receive data RD (RXD) Input 4 Request to send RS (RTS) Output 5 Clear to send CS (CTS) Input 1 6 9 5 Connection Method The following diagram shows the connections between the host computer and the PC. When RS-232C cable is used, a host computer can be connected to only one PC. Female 25-pin RS-232C connector Male 9-pin Computer Recommended ...
- マニュアル
... Interfaces Pin Configuration Port 1 and Port 2 are RS-232C interfaces and are configured as follows: 1 6 9 5 Pin No. Signal symbol Signal name Signal flow 1 FG Frame ground --- 2 SD (TXD) Send data Output 3 RD (RXD) Receive data Input 4 RS (RTS) Request to send Output 5 CS (CTS) Clear to send Input 6 --- Unused --- 7 DR (DSR) Data set ready Input 8 ER (DTR) Data terminal ready Output 9 SG Signal ground --- Connector washer FG Frame ground --- Applicable Connector Plug: XM2A-0901 (OMRON) Hood: XM2S-0911 (OMRON) or equivalent One plug and ...
- マニュアル
... n) FD Label E Label F Label G FF FG SF SG FE FB Fuzzy output n Label D FC FA 0 0 SA SB SC SD SE FFF Output data If all of the fuzzy outputs are zero, the divisor in the equation above will also be zero, the division will not be performed and the Error Flag (bit 15) and No Corresponding Output Flag (bit 04) for that output will be turned ON. Refer to 3-3-2 Output Data for details on the output data format. Maximum Value Method 8 The maximum value method uses the ...
- マニュアル
...[W212-E1-02] CV500-SLK11/SLK21 SYSMAC LINK System System Manual SYSMAC CV-series SYSMAC LINK System System Manual Revised July 1998 SLK11 SLK21 RUN ERC P/S ERH RUN ERC ERH INS SD TS M/S RD LNK INS SD TS M/S RD LNK P/S SL1 SL2 SL No. 6182 OMRON Corporation Read and Understand this Manual Please read and understand this manual before using the product. Please consult your OMRON representative if you have any questions or comments. Warranty and Limitations of Liability WARRANTY OMRON's exclusive warranty is that the products are free from ...
- マニュアル
...(JA∈) L。 。 。 ±1。 。 mm 45 ---------------------[End of Page 690]--------------------- Piinters Connections 5-2-3◎peration 7,2,3_ 46 Section5-2 ThefollowingdiagramshowstheconnectjonofsignalsbetweenthePrinterlnterfaceUnitandtheprinter. 1 FG FG 1 コ\ 2 ...
- マニュアル
... can be connected. Connector Pin Assignments Pin assignments for the RS-232C port are given in the following table. Pin 1 6 9 5 38 Abbreviation Name Direction 1 FG Field ground --- 2 SD (TXD) Send data Output 3 RD (RXD) Receive data Input 4 RS (RTS) Request to send Output 5 CS (CTS) Clear to send Input 6 --- Not used. --- 7 --- Not used. --- 8 --- Not used. --- 9 SG Signal ground --- Connector fitting FG Field ground --- Wiring and Connections Section 2-5 Connections The connections between the CQM1 and a personal computer are illustrated below as an example. CQM1...
- マニュアル
... other external device for wire details for it. The connections between the C200HS and a personal computer are illustrated below as an example. C200HS Personal computer Signal Pin No. Pin No. Signal FG 1 1 – ...
- マニュアル
...these specifications can be connected. Connector Pin Assignments Pin assignments for the RS-232C port are given in the following table. Pin 1 6 9 5 Abbreviation Name Direction 1 FG Field ground --- 2 SD...
- マニュアル
...Status ON Normal operation. OFF Operation stopped. ON Node number not between 1 and 126. A hardware (internal memory or communications unit) error has occurred. OFF Unit normal. ON A PC error has occurred. Flashing ...
- マニュアル
...一一 」 o怜㍊悟況品間o ● 45 r-"'・●〔 Appr◎x.140 9ntemalC◎耐iguration RS・232C 』 1 2 3 4 5 6 7 8 20 FG SD RD 陪 CS DR SG CD ER "脳≡〔 = OV Change・ over 宇 CTS ch8nge ・◎ve「OV 'C剖comector 8● Tran6 ロ mlS叡On Recepti◎n 1 0 No 9 5 6 1 3 7 SDA SDB RDA ROB SG FG ■…, Ti㎜i「冶6{}n陶sisto「S ぐ5V 、 、24V 喝 ; 1 ;N2 200VAC M 100∨A H PowersupPty 撰]隠==蒜 " ---------------------[End of Page 1501]--------------------- 。 函。...
- マニュアル
...---------------------[End of Page 6500]--------------------- 、 、 、、 ー ー ド匡 RS-232C/RSL4221nteZzceBoardS SeCtien362 ThetollowingtableShowsthepinallocatientortheRS・232C{ntertaceBO'ard's conneCt◎rl,・ Pin SignaI Sゆalname ρoD●sign8tlon f FG Framegro顕d "一 2 ...
- マニュアル
... be connected. Connector Pin Assignments Pin assignments for the RS-232C port are given in the following table. Pin 1 6 9 5 Personal Computer Abbreviation Name Direction 1 FG Field ground --- 2 SD (TXD) Send data Output 3 RD (RXD) Receive data Input 4 RS (RTS) Request to send Output 5 CS (CTS) Clear to send Input 6 --- Not used. --- 7 --- Not used. --- 8 --- Not used. --- 9 SG Signal ground --- Connector fitting FG Field ground --- The connections between the ID Controller and a personal computer are illustrated below as an example. ID Controller Personal Computer Signal Pin No....