全 2741 件が検索されました。(2541 - 2560件を表示)
- マニュアル
...supply device Omron Corporation PC 24VDC Recommended: OMRON S8VS-03024 2D code reader V400-F050/250/350 Special round connector DOS/V PC D-sub, 9-pin Name Pin No. Name - 1 SD RD 2 RD SD 3 +24V ER 4 GND SG 5 TRIG DR 6 RESET RS 7 RUN CS 8 OK/NG - 9 ERROR Shield wire Connector cover BUSY +24 V (Brown) 0 V (Blue) Not used with RS-232C communication. TRIG (Pink) RESET (Orange) RUN (Green) OK/NG (Black) ERROR (Gray) BUSY (Yellow) (View of mating section) 60 V400-F050/250/350 User’s Manual Section ...
- マニュアル
.... RS-232C cable for connecting a personal computer Use a cable with the following pin layout, 10 Personal computer side (PC/AT compatible) (Note 1) 1 2 3 4 5 Fitting section 1 6 7 Signal name NC SD (TXD) RD (RXD) RS (RTS) CS (CTS) NC NC NC SG (GND) NC FG Pin No. 1 2 3 4 5 6 7 8 9 10 Shell 8 9 Pin No. 1 2 3 4 5 6 7 8 9 Signal name NC RD (RXD) ...
- マニュアル
...combinations may cause malfunction or damage. • Do not turn the power OFF in the following instances. Doing so will damage data that is in the process of being saved. - While data is being saved on the Controller - While data is being saved on the ...
- マニュアル
....18 VERGET (or VR) Backup/Restore Commands Command name Description Page BGRLOAD (or GL) This command uploads bank group data to the Controller from an external device. p.19 This command uploads bank group data to the Controller from an ...
- マニュアル
...V500-R521B2/C2 User’s Manual 7 V500-R521.book 8 ページ 2008年7月18日 金曜日 午後1時1分 Introduction Introduction 3. Wiring • Extension length of the RS-232C line (SD, RD, SG) should be up to 15 m. • For trigger and power line, use a cable with 0.3 mm2 or more and extension length should be up to 5 m. • Wiring should avoid approaching to a high-power heavy electric current wire. • Check the polarity of terminals and be careful of faulty wiring. • Avoid reverse connection of power ...
- マニュアル
...combinations may cause malfunction or damage. • Do not turn the power OFF in the following instances. Doing so will damage data that is in the process of being saved. - While data is being saved on the Controller - While data is being saved on the ...
- マニュアル
... (or PW) VERGET (or VR) Backup/Restore Commands Command name Description Page BGRLOAD (or GL) This command uploads bank group data to the Controller from an external device. p.25 This command uploads bank group data to the Controller from an ...
- マニュアル
... and Connection Pin arrangement (Pin alignment) Connector part (DIN: 8P plug) Made by Hosiden Corporation TCP1394-715267 (Type A) Connection with upper equipment p.31, p.32 Wire color Pin No. Signal name Function Reader Green 1 ...
- マニュアル
... combinations may cause malfunction or damage. • Do not turn the power OFF in the following instances. Doing so will damage data that is in the process of being saved. - While data is being saved in internal memory - While data is being saved on the ...
- マニュアル
... if it matches the configured settings. Measurement • The overall judgement of all inspection items are output using OR logic. Overall judgement output • Measurement data and image data can be logged in memory in the Sensor or Logging FQ Short Manual in an ...
- マニュアル
... intranet, communication failure may occur due to cable disconnection or the influence of unauthorized network equipment. Take adequate measures, such as restricting physical access to network devices, by means such as locking the installation area. When using a device equipped with the USB flash drive or ...
- マニュアル
... 9-pin D-SUB female connector. The pins are arranged as follows. 㪌 㪐㪏 㪋㪊 㪎 㪉 㪍 㪈 Pin No. Signal name Function 1 FG (GND) Protective frame ground 2 SD (TXD) Transmission data 3 RD (RXD) Reception data 4 RS (RTS) Request to send 5 CS (CTS) Clear to send 6 NC Not connected 7 NC Not connected 8 NC Not connected 9 SG (GND) Signal ground Use a compatible connector. Recommended Model Manufacturer Model Plug OMRON Corporation XM2A-0901 Hood OMRON Corporation XM2S-0911 Z5FP Setup Manual 35 SECTION 3 Connecting External Devices Wiring...
- マニュアル
...When constructing an intranet, communication failure may occur due to cable disconnection or the influence of unauthorized network equipment. Take adequate measures, such as restricting physical access to network devices, by means such as locking the installation area. When using a device equipped with the ...
- マニュアル
...rear face of the controller. Form: D-sub, 15-pin, female 1 8 Application RS-232C RS-422A Pin No. 1 2 3 4 5 6 7* Terminal name RD (RXD) SD (TXD) SG (GND) 8 9 10 11 12 13 14 15 RDB (+) RDA () SDB (+) SDA () 9 15 Function (Not used) Enters data from the external device. Outputs data from the controller. (Not used) (Not used) (Not used) A signal ground. Connects the SG (GND) terminal on the external device. (Not used) Enters data from the external device. Enters ...
- マニュアル
... (female) 1 8 Applicatio n RS-232C RS-422A 8-4 9 15 Pin No. Terminal name Function 1 2 3 4 5 6 7 RD (RXD) SD (TXD) SG (GND) 8 9 10 11 12 13 14 15 RDB () RDA () SDB ( SDA ( (Not used) Enters data from the external device. Outputs data from the controller. (Not used) (Not used) (Not used) A signal ground. Connects the SG (GND) terminal on the external device. (Not used) Enters data from the external device. Enters data from ...
- マニュアル
...rear face of the controller. Form: D-sub, 15-pin, female 1 8 Application RS-232C RS-422A Pin No. 1 2 3 4 5 6 7* Terminal name RD (RXD) SD (TXD) SG (GND) 8 9 10 11 12 13 14 15 RDB (+) RDA () SDB (+) SDA () 9 15 Function (Not used) Enters data from the external device. Outputs data from the controller. (Not used) (Not used) (Not used) A signal ground. Connects the SG (GND) terminal on the external device. (Not used) Enters data from the external device. Enters ...
- マニュアル
... (female) 1 8 Applicatio n RS-232C RS-422A 8-4 9 15 Pin No. Terminal name Function 1 2 3 4 5 6 7 RD (RXD) SD (TXD) SG (GND) 8 9 10 11 12 13 14 15 RDB () RDA () SDB ( SDA ( (Not used) Enters data from the external device. Outputs data from the controller. (Not used) (Not used) (Not used) A signal ground. Connects the SG (GND) terminal on the external device. (Not used) Enters data from the external device. Enters data from ...
- マニュアル
... within a specified length. If it isn't, safety function may not work properly, resulting in danger. E F3SG-RR User’s Manual ix Introduction Settings Some settings of functions or the setting recovery function configurable with the configuration software, ...
- マニュアル
... this function to retrieve ambient light level information. Making any changes to the function is not possible. (When the F3SG-R is in the cascade connection, ambient light level of each segment can be retrieved.) Refer to Safety Light Curtain Configuration Tool for Model F3SG (...
- マニュアル
...ファイバ長を表 し ています。 100K は 1Km の こ と です。 AC アダプタ : Z3P-AC / 電源プラグコード Z3P-DC ④ ② ■仕様電源電圧 ② SD 2 RD 3 RS 4 CS 5 ER 20 DR 6 SG 7 +12V 9 ③ ⑤ ① POWER LED (緑) 形 Z3R の電源を供給する と 点灯 し ます。 ② RUN LED (緑) 相手側の形 Z3R に電源が供給 さ れ、 両者の間に...