全 50423 件が検索されました。(221 - 240件を表示)

  • マニュアル

    ...z 1 0 1 1 B VT ESC K k { 1 1 0 0 C FF FS , L l 1 1 0 1 D CR GS - M m 1 1 1 0 E S0 RS . N n 1 1 1 1 F SI US Even parity A-2 b7 ? O _ } o DEL E5C-T Digital Temperature Controllers Programmable Type Communications Manual (H186) A Appendices A-2 Troubleshooting Before Requesting Repairs If communications are not functioning properly, check the items in the following table before requesting repairs. If normal operation cannot be restored even after checking everything, return the ...

  • マニュアル

    ... settings for the other parameters. • • • • • • • • Operate Communication Setting: Selected. Protocol: Dedicated Protocol Parity: Even Stop Bit: 2Bit Transmission Speed: 38,400 H/W Type: RS-485 Sum Check: Selected. Transmission Control Procedure: Form4 (With ...

  • マニュアル

    ... settings for the other parameters. • • • • • • • • Operate Communication Setting: Selected. Protocol: Dedicated Protocol Parity: Even Stop Bit: 2Bit Transmission Speed: 38,400 H/W Type: RS-485 Sum Check: Selected. Transmission Control Procedure: Form4 (With ...

  • マニュアル

    ... be reset by the interference of induced voltage. To prevent such trouble, wire the lead as short as possible and avoid laying wires in parallel with power lines. In case the induced voltage exceeds 30% of the rated voltage (10% for DC type), connect a ...

  • マニュアル

    ... not be reset by the interference of induced voltage. To prevent such trouble, wire the lead as short as possible and avoid laying wires in parallel with power lines. (25) In case the induced voltage exceeds 30% of the rated voltage (10% for DC type), connect a ...

  • マニュアル

    ... be reset by the interference of induced voltage. To prevent such trouble, wire the lead as short as possible and avoid laying wires in parallel with power lines. (23) In case the induced voltage exceeds 30% of the rated voltage (10% for DC type), connect a ...

  • マニュアル

    ...ficiently before use. 16) Do not wire the terminals that are not used. 17) If there is a transformer or other device with a large inductance component on the power supply line, the inductance will cause a reverse voltage. If that occurs, insert a ...

  • マニュアル

    ...ficiently before use. 16) Do not wire the terminals that are not used. 17) If there is a transformer or other device with a large inductance component on the power supply line, the inductance will cause a reverse voltage. If that occurs, insert a ...

  • マニュアル

    ... time. Fuji Electric Co., ERB44-06 or equivalent Select varistor voltage as follows: 24-VDC system varistor: 39 V 100-VDC system varistor: 200 V 100-VAC system varistor: 270 V 200-VAC system varistor: 470 V Okaya Electric Industrial Co. ...

  • マニュアル

    ... when electricity is conducted through the conductors that will not result in cracking or damage to an extent that would affect the functionality of the sheath. Broken shield strands may occur. Encoder Cables Model Minimum bending radius (R) R88A-CRGA...

  • マニュアル

    ... Flexible Cables R88A-CAKA@@@BR-E • OMNUC G5 Series Servo Drive R88D-KT • OMNUC G5-series Servomotor Feedback Signals 100 VAC 200 VAC 400 VAC Peripheral Devices Encoder Cables ● Flexible Cables • 750 W or less: R88A-CRKA@@@...

  • マニュアル

    ...bit 7 bit 6 bit 5 bit 4 bit 3 bit 2 bit 1 bit 0 n 0 CI8 CI7 CI6 CI5 CI4 CI3 RV FW 1 CO2 CO1 CR CO5 CO4 CO3 RS EXT n+1 n+2 Rotation Speed Reference (Low byte) Rotation Speed Reference (High byte) 4 Torque Reference (Low byte) 5 Torque Reference (High byte) 6 Torque Compensation Bias (Low byte) 7 Torque Compensation Bias (High byte) 4 4-3-3 Extended Control I/O (101/151/153) n+3 2 3  Output Bit/Data Details Name Description FW Forward/Stop 0: Stop 1: Forward...

  • マニュアル

    ... with sufficient allowance for the return circuits, and bundle them with lines of the same signal level. • For long I/O lines, wire the input and output signal lines separately. • Use twisted-pair wires for pilot lamps (and particularly lamps with filaments). • Use countermeasures, such as ...

  • マニュアル

    ... on "dlun". WRITE (dlun) $in.string The following example returns any error generated during the write operation example above to the "error" variable. error = IOSTAT(dlun) Reading from a Disk The following example reads from the open file on "dlun" up to the first ...

  • マニュアル

    ...wide. /In Format values as decimal integers in fields n spaces wide. /On Format values as octal integers in fields n spaces wide. The following specifiers can be used to insert special characters in the string. /Cn Include the characters carriage return (...

  • マニュアル

    ... on "dlun". WRITE (dlun) $in.string The following example returns any error generated during the write operation example above to the "error" variable. error = IOSTAT(dlun) Reading from a Disk The following example reads from the open file on "dlun" up to the first ...

  • マニュアル

    ...Z930) NX-SOD[] XS5W-T[] - AC Servo Drives R88D-1SN[] 1S-series AC Servomotors and AC Servo Motors R88M-1[] Servo Drives User’s Manual (with Power cables R88A-CA[] Built-in EtherCAT Encoder Cables R88A-...

  • マニュアル

    ... W K05030H/T□ CAKAS, CAKASR, 100 W K10030L/S□ CAKAS CAKASR CAKAB CAKABR 200 W K20030L/S□ 3,000 CRKAC CRKACR 50 W K05030H/T□ r/min *2 *2 100 W K10030H/T□ CAKAS, CAKASR, 200 V CAKAS CAKASR CAKAB CAKABR 200 W K20030H/T□ 400 W K40030H/T□ *1. □ represents an optional specification for the motor.  represents a 3-digit cable length (005 for 5 m). *2. When you ...

  • マニュアル

    ...[] --- Cable 15 AC Servo Drive R88D-1SN[]-51 AC Servomotors/Servo Drives 1S-series AC Servomotor R88M-1[] with Built-in EtherCAT Communications Power cables R88A-CA[] and SS1/SLS Safety Sub-Functions Encoder Cables R88A-...

  • マニュアル

    ...XS5W-T[] Manual name --- AC Servo Drive R88D-1SN[]-51 1S-series AC Servomotors/Servo AC Servomotor R88M-1[] Drives with Built-in EtherCAT Power Cable R88A-CA[] Communications and SS1/SLS Safety Encoder Cable R88A-...