全 50423 件が検索されました。(181 - 200件を表示)
- カタログ
...Outputs extracted character strings and combined two character strings, which is usually done by a PC or PLC. Logic Tool Example: Overall judgment excluding Presence/Absence Compares a human-readable character string read by OCR with data contained in the code read by ...
- カタログ
... USA and other countries. Other company names and product names in this document are the trademarks or registered trademarks of their respective companies. 28 Dimensions (Unit: mm) Sensor Integrated Sensor Narrow View FQ2-S@@@10F-@@@ FQ2-CH@@@10F-M FQ-...
- カタログ
... Signals G5 Series Drives with Built-in EtherCAT Communications R88D-KN@@-ECT Encoder Cables • Non-Flexible Cables 750W or less R88A-CRK@@@@C • 1.0kW or more R88A-CRKC@@@N • Flexible Cables • 750W or less R88A-CRK@@@@...
- カタログ
... influence of inductive voltage, the wires connected to the H3CR-H must be as short as possible and should not be installed alongside power lines. If the H3CR-H is influenced by inductive voltage that is 30% or more of the rated voltage, connect a ...
- カタログ
... inductive voltage. To eliminate inductive voltage, the wires connected to the Timer must be as short as possible and should not be installed parallel to power lines. If the Timer is influenced by inductive voltage that is 30% or more of the rated voltage, connect a ...
- カタログ
...A2 • The power supply circuits for H3DT-series Timers use switching mode. Therefore, if there is a transformer or other device with a large inductance component on the power supply line, the inductance will cause a reverse voltage. If that occurs, insert a ...
- カタログ
...Life-test Curve (Reference Values) 30% Measurement time Time 3 H3FA Connections Block Diagrams Note: All diagrams are views from the top. H3FA-A, H3FA-B, H3FA-SA, H3FA-SB When the input voltage is applied, the ...
- カタログ
... The input for the H7E@-NFV-@ is a high-impedance circuit and so influence from an induced voltage may result in malfunction. Therefore, when the input signal wiring is longer than 10 m (line capacitance of 120 pF/m, at room temperature), it is recommended that a ...
- カタログ
.... Refer to Mounting Brackets on E39-L/E39-S/E39-R on your OMRON website for details. Reflector (A Reflector is required for each Retro-reflective Sensor: A Reflector is not provided with the Sensor. Be sure to order a Reflector.) Oil-resistant Reflector E3ZM-...
- カタログ
...PYF-14-PU PYF-08-PU PYF-08-PU-L* PYF-14-PU-L* Appearance *A release lever is not included. PTF-PU-Applicable Models General-purpose Relays SSRs Temperature Controllers Applicable models LY2 LY2-CR LY4 G3H/G3HD /G9H E5L-A E5L-C No. of poles 2 2 4 1 - - Socket model PTF-08-PU PTF-08-PU-L* PTF-14-PU-L* PTF-08-PU PTF-14-PU-L* PTF-14-PU-L* Appearance *A release lever is not included. P2RF-PU-Applicable Models Applicable models General-purpose Relays SSRs Liquid Leakage Sensor...
- カタログ
...観 *リリースレバーは装備されていません 形PTF-PU対応機種一般リレー適合機種 SSR 温度調節器 形LY2□ 形LY2□-CR 形LY4□ 形G3H/G3HD /形G9H 形E5L-A □ 形E5L-C □ 極数 2 2 4 1 - - ソケット形式 形PTF-08-PU 形PTF-08-PU-L* 形PTF-14-PU-L* 形PTF-08-PU 形PTF-14-PU-L* 形PTF-14-PU-L* 外観 *...
- カタログ
...G3F/G3FD Series H3Y Series H3YN Series Timers No. of poles Model *1 MY2@ MY2IN(S) 2 PYF-08-PU MY4@ MY4H MYQ4@ MY4@(S) MY2K 4 PYF-14-PU MY2Z(N)-CR 2 PYF-08-PU-L *2 1 PYF-08-PU H3Y(N)-2-B 2 PYF-08-PU-L H3Y(N)-4-B 4 PYF-14-PU-L G3FM G3F G3FD *1. The PYF-@@-PU-L Sockets do not have release levers. *2. Use with the hold-down clip (Y92H-3). PTF Series Socket Applicable model (typical example) No. of poles LY2@ General Purpose Relays LY Series...
- カタログ
...R88A-CAKA@@@B • Flexible Cables R88A-CAKA@@@BR Motor power signals EtherCAT Communications Feedback Signals Encoder Cables 750W or less R88A-CRK@@@@C • 1.0kW or more R88A-CRKC@@@N • Flexible Cables • 750W or less R88A-CRK@@@@...
- カタログ
....g., contactor or valve) that generates an arc when the circuit is broken, the NC (NO) contact may turn ON before the NO (NC) contact has opened (turned OFF). • When using both NO and NC outputs at the same time, incorporate an arc suppressor (use the ...
- カタログ
....g., contactor or valve) that generates an arc when the circuit is broken, the NC (NO) contact may turn ON before the NO (NC) contact has opened (turned OFF). • When using both NO and NC outputs at the same time, incorporate an arc suppressor (use the ...
- カタログ
...n) conc oncept ept pt fo forr the the specif spe cifica icatio tions ns of pro produc ducts ts use used d in in cont control ol paanels willl cr creat eatee new new val v ue to o our cu custo stomer mer'ss con contro troll pane panels. ls. Combin Com bining ing mu multi ltiple ple pr produ oducts cts th that at sha share the he Va Value lue De Desig sign sig n conc conc oncept ept wi willll fur furthe therr incr increas ease the val value ue provid pro vided vid ed ...
- カタログ
... is the time required for communication between the Antenna and the RF Tag. Response receipt time: This is the time required for returning a response from the Controller to the host device. It varies depending on the communications speed and format. • For an ordinary command ...
- カタログ
...Series for MY, LY , G2R-S Relays and G7SA Relays with Forcibly Guided Contacts Applicable model (typical example) Size W×H×D (mm) 2 PYF-08-PU MY4 4 PYF-14-PU LY2 2 PTF-08-PU LY2-CR 2 PTF-08-PU-L LY4 4 PTF-14-PU-L 43.4×90×52.1 1 PTF-08-PU 24.8×90×70.1 G2R-1-S 1 P2RF-05-PU G2R-2-S 2 P2RF-08-PU H3Y(N)-2-B 2 PYF-08-PU-L H3Y(N)-4-B 4 PYF-14-PU-L H3RN-1-B 1 P2RF-05-PU H3RN-2-B...
- カタログ
...,800, 9,600 (default) 19,200, 38,400, 57,600, or 115,200 bps Data bit length *1 7 bits or 8 bits (default) Parity check *1 None (default), Even, or Odd Stop bit length Data delimiter 1 bit When receiving ...
- カタログ
...0 5 0 10 500 1000 1500 2000 2500 3000 Travel distance Sampling: 4 ms Error (Pm) 13.5 Pm Previous OMRON models Moving resolution when measuring SUS 5 Previous OMRON models Cr Glass 10 Pmp-p 5 0 5 10 15 0 20 40 Travel distance (mm) SUS 10 ...