全 2436 件が検索されました。(2101 - 2120件を表示)
- マニュアル
... set the local IP address as follows: Set the local IP address in the CPU Bus Unit System Setup when making other settings in the CPU Bus Unit System Setup (i.e., the default settings are not used). The settings are made with CX-Programmer. ...
- マニュアル
...0 0 0 0 0 0 1 1 0 1 2 : : : : 1 1 1 1 1 1 1 1 0 1 1 0 61 62 1 1 1 1 1 1 63 0: OFF, 1: ON Note 1. Refer to Appendix A Node Address Settings Table for a complete table of DIP switch settings. 2. The Slave won’t be able to participate in communications if the same node address is used for the Master or another Slave node (node address duplication error). Baud Rate Setting Pins 7 and 8 are used to set the baud rate as shown in ...
- マニュアル
...#2 #1 32 outputs 4-point 16 inputs Analog Output Unit Output area Input area CIO 355 32 output bits for Unit #0 CIO 356 CIO 57 CIO 58 CIO 59 CIO 60 CIO 61 CIO 360 Unused CIO 63 CIO 64 CIO 65 CIO 66 (See note 1.) CIO 361 CIO 362 4 analog outputs for Unit #1 16 output bits for Unit #2 I/O Unit interface status for node number 05 CIO 357 16 input bits for Unit #2 CIO 358 16 input bits for Unit #3 CIO 359 Unused 4 analog outputs for Unit #1...
- マニュアル
...Power Capacity A CVM1D PC consumes up to 200 VA per Rack. Power consumption varies with the system configuration (refer to 3-6-10 Current Consumption). When power is applied, a surge current five times the steady-state current will flow to the PC. ...
- マニュアル
.... (030) MOV *D00100 A090 Indirect address Word D00099 D00100 D00101 Content 4C59 0324 F35A D00324 D00325 D00326 5555 2506 D541 Indicates D00324. 5555 moved to A0090. 61 Section 3-10 Index and Data Registers (IR and DR) If the content of *DM addresses is defined as binary in the PC Setup, the number indicates a internal I/O memory address. The range of possible binary numbers, $0000 to $FFFF, allows all memory areas, including EM, to be indirectly addressed. If, in this case, the content of D00100 is $0324, then *D00100 indicates internal I/O memory address $0324, which ...
- マニュアル
... limit SR 244 to SR 247 Method(s) to read counter PV Incrementing counter Decrementing counter 2 kHz Contains counter PV. Read SR 244 to SR 247. Execute PRV(62). (Counter PV) Method to change counter PV Execute INI(...
- マニュアル
... kHz Contains counter PV. Same as CPM2C. Same as CPM2C. Method(s) to read counter PV Read SR 244 to SR 247. Same as CPM2C. Execute PRV(62). Method to change counter PV One-shot mode Execute INI(61). Same as CPM2C. 1 kHz Contains counter PV–1. Read SR 244 to SR 247. (Counter PV – 1) Not supported. Yes Same as CPM2C. Same as CPM2C. Scheduled interrupt mode Yes Same as CPM2C. Same as CPM2C. Item Setting the quick-response function PC Setup INT(89) (Mask) INT(89) (Read mask) Not supported (ignored) Reads mask status. INT(89) (...
- マニュアル
... Units can also be connected. If an Expansion I/O Block is used, a maximum of 16 Units can be connected. (See 1-2-1 Basic Configuration.) Note 1. The CQM1H is mounted to DIN Track. 2. Only the CQM1H-CPU51/...
- マニュアル
...PT 7 Section 1-3 Specifications 1-3 Specifications 1-3-1 Serial Communications Board Device name Model number Serial Communications Board CQM1H-SCB41 Classification Supporting CPU Units CQM1H-series Inner Board CQM1H-CPU51/...
- マニュアル
...14 13 12 11 10 +3 32 31 30 29 28 27 26 25 24 23 22 21 20 19 18 17 +4 48 47 46 45 44 43 42 41 40 39 38 37 36 35 34 33 +5 Note - - 62 61 60 59 58 57 56 55 54 53 52 51 50 49 Even if the local node is disconnected from the network, only the bit corresponding to the local node is turned OFF (i.e., the entire status area participating in the network is not turned OFF). While the local node is disconnected, the bits corresponding to ...
- マニュアル
.... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 61 SECTION 2 Individual Unit Descriptions for CS Series . . . . . . . . . . . . . . . 67 2-1 CS1W-PTS01-V1 Isolated-type Thermocouple Input Unit . . . . . . . . . . . . . . . . . . . . . . . . . . . . 68 2-2 CS1W-PTS11 Isolated-type Thermocouple Input Unit . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 80 2-3 CS1W-PTS51 Isolated-type Thermocouple Input Unit . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 97 2-4 CS1W-PTS55 Isolated-type Thermocouple Input Unit . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 109 2-5 CS1W-PTS02 Isolated-type Resistance Thermometer Input Unit (Pt100 or JPt100). . . . . . . . . 121 2-6 CS1W-PTS03 Isolated-type Resistance Thermometer Input Unit (Ni508.4) . . . . . . . . . . . . . . . 132 2-7 CS1W-PTS12 Isolated-type Resistance Thermometer Input Unit (Pt100, JPt100, Pt50, Ni508.4) 142 2-8 CS1W-PTS52 Isolated-...
- マニュアル
.... . . . 60 3-2-2 CS1 and CS1-H PLCs . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 61 3-2-3 CS1D PLCs . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 62 Optical Wiring . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 63 3-3-1 Optical Fiber Cable Connections for H-PCF Cable. . . . . . . . . . . . . 63 3-3-2 Optical Fiber Cable Connections for GI Cable . . . . . . . . . . . . . . . . 65 3-3-3 Backup Power Supply Wiring . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 67 3-3-4 Connecting Optical Fiber Cable to Connectors for H-PCF Cable . . 68 3-3-5 Connecting Optical Fiber Cable to Connectors for GI Cable . . . . . 70 3-3-6 Connecting Backup Power Supply Cables. . . . . . . . . . . . . . . . . . . . 73 47 Section 3-1 Component Names and Functions 3-1 Component Names and ...
- マニュアル
... 00001 IR 00002 00 PLC Setup setting (DM 6642 bits 08 to15) 01 02, 03, or 04 Used as normal inputs. Used as high-speed Used as inputs for synchrocounter inputs. nized pulse control. Used as a normal input. ...
- マニュアル
... Box for the Project Workspace level. When an LCU or LCB element is selected, function block group, or function block is selected Function Block Reference Displays the reference help for the selected function block. When a function block is selected ...
- マニュアル
... the collection cycle (approximately 10 s for realtime trends and 60 s for historical trends) plus the screen refresh cycle (a few seconds). If another screen is switched to, the changes will be reflected in the screen as soon as it is returned to. ...
- マニュアル
... Relay Units and 2 PCU Connecting Cables are required. • When using in combination with the CS1W-NC213/NC233 (2-axis control), 2 Servo Drive Connecting Cables are required. • When using in combination with the CS1W-NC413/NC433 (4-axis control), 4 Servo Drive Connecting Cables are required. ...
- マニュアル
...INT(89) (Mask) INT(89) (Read mask) INT(89) (Clear) Minimum pulse width Count mode CPM2C-S Incrementing counter Decrementing counter 2 kHz Contains counter PV. Read SR 244 to SR 247. Execute PRV(62). Execute INI(...
- マニュアル
... pins 40 pins XW2B-40G4 XW2D-40C6 Size Miniature Standard Standard Miniature The recommended size for cable wires is AWG 24 to 26 (0.2 to 0.13 mm2). Use a cable with an outer diameter of less than 1.61...
- マニュアル
...1 1 1 1 1 1 1 Pin 1 0 1 0 1 Node address 0 1 2 3 : : 0 1 0 1 60 61 62 63 The Master Unit is shipped with the node address set to 0. Since the DIP switch is located on the back of the Master, the Master must be removed from the PLC in order to change the node address setting. Be sure to set the node addresses before assembling the Network. 35 Section 2-1 Master Unit for CVM1 and CV-series PLCs Pins 7 and 8 are reserved for system use. Leave ...
- マニュアル
.... . . . . . . . . . . . . . . . . . . . 55 SECTION 3 Allocated CIO and DM Words . . . . . . . . . . . . . . . . . . . . 61 3-1 Overview of Word Allocations . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 62 3-2 Allocated CIO Area Words . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 64 3-3 Allocated DM Area Words . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 84 SECTION 4 Remote I/O Master Communications . . . . . . . . . . . . . . . 95 4-1 Master Remote I/O Communications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 96 4-2 Scan List . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 103 4-3 Fixed Allocations . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 105 4-4 User-set Allocations . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 111 4-5 Starting and Stopping Remote I/O Communications . . . . . . . . . . . . . . . . . . . . . . . 120 4-6 Example of Ladder Programming for Remote I/O Communications . . . . . . . . . . . 121 4-7 Errors that May Occur in Remote I/O Communications . . . . . . . . . . . . . . . . . . . . 122 vii TABLE OF ...