全 177 件が検索されました。(141 - 160件を表示)
- マニュアル
...用可能にする(F7) ······························································4-25 バンク切替方法の選択(F8) ··································································4-26 4.8.7 4.9 バンクコピーする(F9)·········································································· 4-27 E24 検出有効/無効(...
- マニュアル
...示部 L HH ADJL ADJH BANK 公差表示部 ZERO ESC キー機能名表示部 F1 F2 F3 F4 F5 F6 F7 F8 F9 F10 ファンクションキー SHIFT ≪ 12.345 67.891 DISP HH 第1章 ↓ ▲ 0 H リモート/ローカル=リモートニュウリョクレンジタイミングホールド&トリガエンザンシキスケーリングバン...
- マニュアル
... Switch Backlight Check Comm. Check Move the bar cursor to the item you want to check, and then press the Enter Key. Function Key Check F1 F2 F3 F4 F5 F6 F7 F8 F9 F10 F11 F12 F13 F14 F15 F16 F17 F18 F19 F20 F21 F22 F23 F24 F25 F26 F27 F28 F29 F30 F31 F32 F33 F34 F35 F36 F37 F38 F39 F40 F41 F42 F43 F44 F45 F46 F47 F48 F49 F50 F51 F52 F53 F54 F55 F56 F57 F58 F59 F60 F61 F62 F63 F64 The operation of the function keys can be checked if ...
- マニュアル
...』units. 110 F8 lnitialScreen(ln.Scり Setsthescreennumberofthefirstscreentobedisplayed(theinitialscreen)whentheProgrammableτbrminalispowereduporreset. F9 TitbChange{TITLE) Changesa川et川ethathasprevbuslybeenset. 98 臼0 NextFunctions(NEXT) Usetochangethefunctionsa‖ocatedtothefunctionkeys. … NEXτF1 TbolSe賃hgs(T.OOLS) Accessesthe「「bolSettingsmenu. 15 NEXT,...
- マニュアル
... notify area must be set as described below before selecting the screen number. To read the screen data from other file, press the [F5] (Read) function key. 114 Creating and Transmitting Screen Data Section 4-1 Host link/NT link/C200H direct communication ' Press [...
- マニュアル
... file in the “Screen List” screen. To read the screen data from other file, press the [F5] (Read) function key. When using host link/NT link/C200H direct communication, set the direct connection information before selecting the screen number. ⇒ While in the “Screen List” screen, press the [...
- マニュアル
.... . SECTION 5 Creating Marks, Images, and Library Data Reading BMP files Image files (BMP format) created using packages such as Microsoft Windows (TM) Paintbrush can be read as data. xvi Menu Tree Main Menu * This comprises the function keys F1 through ...
- マニュアル
...status notify area must be set by referring to the sections specified below. To read the screen data from other file, press the [F5] (Read) function key. 116 Creating and Transmitting Screen Data Section 4-1 While in the “Scr list” screen, press the [...
- マニュアル
... graph area, resulting in the graph no longer being visible when the + range color is set to black. i ii NTH25/25C Programmable Terminal Operation Manual Produced May 1999 + -F7 POWER F8 F1 F9 F2 F10 F3 F11 F4 F5 F6 iii iv OMRON Product References All OMRON products are capitalized in this manual. The word “Unit” is also capitalized when it refers to an OMRON product, regardless of whether or not it appears in the proper name of the product. The abbreviation “Ch,” which appears in some displays and on some OMRON products, often means “word” and is ...
- マニュアル
...The NSH5 is an NSH5-series Hand-held Programmable Terminal that provides both a touch panel and safety switches. ET RESET RE S SET RE RUN F6 F1 F7 F2 F8 F3 F9 F4 F10 F5 Touch panel NSH5 Safety switches Touch Panel The touch panel is the same as the one for NS5-series Programmable Terminals with touch panels. Connecting to an OMRON PLC by RS-232C or RS422A does not require a program. Function switches are also provided. Safety Switches An emergency stop switch and an enabling switch are provided. Be sure to externally connect them to safety ...
- マニュアル
...Specification Minimum requirement RAM capacity 640K bytes Free work disk capacity 4 MB (can be a combination of hard disk and work disk) Floppy disk drive 5.25” or 3.5” drive Keyboard Home, Esc, Ctrl, PgUp, PgDn, Backspace, F1 to ...
- マニュアル
...F3 Selectoverviewmode Displaysalarge-scaleviewofalargerrangeoftheSFCprogramandmonitorsthePCoρerationstatus. F4 Sebctρrogramviewmode Displaysthe'sρecifiedtransitionoradioninladder・diagramformandmonitorsthePCoperationstatus. FIo Clearerror ClearserrorsinthePCfromthe◎omputer Shift+F7 SelectRUNmode. SetsthePCinRUNmode. Sh廿t+F8 Se{ectMONITORmode. SetsthePCinMOMTORmode. Sh廿t+F9 SelectDEBUGrnode. SetsthePCinDEBUGmode. Sh流◆...
- マニュアル
...)θれヨηd ApPlicableohlytoOU℃ instructions 加sfτucfわη8πadd佑ss一 」qρθ陥rldSMft+FIO OUTNOτKEEP(011), Shlft+FIOCR CR DIFU(013),DIFD(014), SET(016),RSET(017), Advancedirlstruction: CMP(020),and 'ηsfπ∫dわηSh流+...
- マニュアル
.... Create the I/O table. 18 Section 2-2 Host Link Unit Settings and Parameters 5. Select “CPU Bus Setting.” The following menu will be displayed. 6. Select “CPU Bus Unit System Setup.” The following screen will appear. 7. Press ...
- マニュアル
...,N,1.Alsosettheprinterfor}6 inchpaperdelivery,80characters川ne,andno-paperdetection,anddisable 1"perforations. 2.AttachthePrinterlnterfaceUnittotheGPCandsecureitbytighten│ngthe screw.ltiSnOtneCessarytosettheDIPSwitCheSonthePrinterlnte【寸ace Unit. ThePrinterlnteriaceUnitandprintercanbeusedevenw袖outaSystem MemoryCassetteinsta‖edintheGPC. 3.ConnectthePrinterlntertaceUnitandprinterwiththeappr◎priateconnect・ ingcable(e、g.,SCY-CN201). ---------------------[End of Page 691]--------------------- ...
- マニュアル
... completed or not. When the power is turned on, this mode is automatically selected. The following illustrations show changes in the speed in the stop mode and the pass mode when the continuous operation commands are given as shown below. Example: N010 G01 X100 ...
- マニュアル
...N007 N008 N009 P800 G27 G01 G01 G01 G01 G01 G27 G26 G73 XY XY X10 X20 Y20 X10 Y10 XY XY Y100 M10 Y10 F10 M20 M30 Block N000 declares the program number and axes being used. P006: N001 Sets the workpiece origin offset to (X100, Y100). Changing the Interpolation Acceleration Time Section 9-6 P006: N002 Calls subprogram P800. P800: N001 Returns to the workpiece origin. The workpiece coordinate system is selected at this time. M code M10 is output and the Unit waits for the M code reset. P800: N002 through N006 The subprogram’s series of ...
- マニュアル
...BACKSPACE DELETEcharactertoleftofinseltion DELETE DELETEscontentsofcelI F6 Movestonextpaneclockwise AIT F6 MovestoapPUca樋on'snextopenn皿−documentwindOW ALT+SHIFT F6 Movesthroughthenon-documentwindowsinreverseorder CTRL F6 Movestopdocumenttobottomofstack CTRL+SHIFT F6 Movesbottomdocumenttotopofstack SHIFT F6 Movestopreviouspaneclockwise ...
- マニュアル
...DELETEcharactertoIeftofinsertiorl 「▼T-w DELETE Deletescontentsofce正1 F6 Movestonextpaneclockwise ALT F6 .・-MovestoapPlica60n'snextopennon-documentwindOW AILT+SHIFT F6 Movesthroughthenon-documentwindowsinreverseorder −CTRL F6 Movestopdocumenttobottomofstack CTRL+SHIFT F6 Movesbottomdocumenttotopofstack SHnヨT一 F6 Movestopreviouspaneclockwise ...
- マニュアル
... the same as the default CX-Programmer. Menu Function View project workspace [View] | [Window] | [Workspace] Shortcut keys [Ctrl]+[F11], [Alt]+[1] View Output window [View] | [Window] | [Output] [Ctrl]+[F12] , [Alt]+[2] View Watch window [View] | [Window] | [Watch] [Ctrl]+[...