全 344 件が検索されました。(141 - 160件を表示)

  • マニュアル

    ...Model S3200-COCF2011 S3200-COCF2511 Replacement model S3200-COCF2071 S3200-COCF2571 Optical Fiber Cables with Connectors (Indoor Use Only) The following Optical Fiber Cables are available with Connectors (lap/polished type) already attached. Note Specifications Optical Fiber Cable Connectors: ...

  • マニュアル

    ...*1 Data Comparison Value 00 – Data Comparison Value 31 Y Y cA 00-31 10 x M*2 Captured Count Value N Y cC 02 2 Rate History Log File Data N Y cF 01 2 x R*3 Counter Value Y Y cC 01 2 (Re) Configure Unit Y N 0D 01 1 Clear Error(s) Y N EC 00 1 c = Counter Number (1 or 2) *1 M = Number of Ranges, 1 ≤ M ≤ 21 *2 M = Number of Comparison Values, 1 ≤ M ≤ 12 *3 R = Pulse Rate value, 1 ≤ R ≤ 64 121 Section 4-5 Supported IOWR/...

  • マニュアル

    ...E” “0” “P” “T” 06 “A” “*” F2 “I” 02 07 “G” “R” “M” “t” 02 “V” “2” “C” “R” “*” 13 “*” 30 “D” 01 CF “O” 13 “O” ““ “I” “T” 13 “B” “E” “*” 01 “*” 79 13 00 02 “R” 09 “D” “U” “D” “Y” 07 “R” “V” “*” “*” “*” 13 07 13 01 “Y” “O” “E” “N” 13 “P” “U” “E” 13 “*” 13 06 “S” 07 06 13 “M” “L” “i” 07 “E” “N” “V” 02 “*” 08 “C” “Y” “R” 02 03 “R” 13 “t” “D” 13 “I” 13 “*” “*” “S” “0” “S” “E” 01 “P” “O” 15 ““ “E” 0A “T” 03 “*” 13 “E” “...

  • マニュアル

    ...About TIMER and COUNTER Data Types (STRING) StrX (STRING) StrX D100 Describe the TIMER and COUNTER type variables as shown below. 1) How to describe the TIMER type variables in the structured text. Timer completion flag: TIMER_type_variable_name....

  • マニュアル

    ...: 30 max., Virtual axes: 2 max., Special motion control language CJ1W-MCH71 25 words 0 to F 3 Units/Rack 0.60 --- 210 g max. SYSMAC SPU Unit (Highspeed Storage and Processing Unit) One CF card type I/II slot (used with OMRON HMC-EF Memory Card), one Ethernet port CJ1W-SPU01V2*10 0.56 --- 180 g max. *9 Not used. 0 to F 16 Units*3 *1 Some CJ-series CPU Bus Units are allocated words in the CPU Bus Unit Setup Area. The system must be designed so that the number of words allocated ...

  • マニュアル

    ...AR T C DM @DM *DM OK OK OK OK OK OK OK OK OK Constants OK Registers DR IR Indirect using IR OK --- OK CF --- Pulse TR bits bits --- --- --- CP1E/CP2E CPU Unit Instructions Reference Manual(W483) 2 Instructions Item Contents Flags Name Function Label Notation and Layout of Instruction Descriptions The flags table indicates the status of the condition flags immediately after execution of the instruction. Any flags that are not listed are not affected by the instruction. “OFF” indicates that a flag is turned OFF immediately after execution of the instruction regardless of the results of executing ...

  • マニュアル

    ...received. 2A Group 2 only server general failure This error code may only be reported by DeviceNet group 2 only servers with 4K or less code space and only in place of Service not supported, Attribute not supported and Attribute not settable. 2B-...

  • マニュアル

    ... (W553) 3 Hardware 3-6 CFast Card, Battery Slot (Optional) 3-6 CFast Card, Battery Slot (Optional) Depending on the product configuration an optional CFast Card slot and/or an optional Battery are located at the rear side of the base layer. as ...

  • マニュアル

    ... (W555) 3 Hardware 3-6 CFast Card, Battery Slot (Optional) 3-6 CFast Card, Battery Slot (Optional) Depending on the product configuration an optional CFast Card slot and/or an optional Battery are located at the rear side of the base layer. as ...

  • マニュアル

    ...3-6 CFast Card Slot (Optional) Depending on the product configuration an optional CFast Card slot is located at the rear side of the base layer. The CFast Card slot accepts CFast Cards that comply with the CFast 2.0 specification. t as ...

  • マニュアル

    ...-6 CFast Card Slot (Optional) Depending on the product configuration an optional CFast Card slot is located at the rear side of the base layer. The CFast Card slot accepts CFast Cards that comply with the CFast 2.0 specification. 3 t as ...

  • マニュアル

    ... was received. 2A Group 2 only server general failure This error code is reported only by group 2 only servers with 4K or less of code space and only in place of Service not supported, Attribute not supported, or Attribute not settable. 2B-...

  • マニュアル

    ... member was received. 2A Group 2 only server general failure This error code is reported only by group 2 only servers with 4K or less of code space and only in place of Service not supported, Attribute not supported, or Attribute not settable. 2B-...

  • マニュアル

    ... 5-31 for connection details. NY-series NYE Industrial Panel PC Hardware User's Manual (W634) 3-9 3 Hardware 3-5 CFast Card Slot The CFast Card slot is the storage device for the OS and related software. t as ...

  • マニュアル

    ...RUN RUN ZFV ZS-DSU User’s Manual 1-11 Section 1 Part Names and Functions Part Names and Functions Section 1 FEATURES The following describes the names and functions of parts on the Data Storage Unit. (1) ...

  • マニュアル

    ...TR SP PARAMETER SET SP PARAMETER SET OPERATION MODE CHANGE MO - - OPERATION CONDITION SET SE - - RESPONSE RESEND RR - - CONTROLLER CONTROL CC CONTROLLER CONTROL CC READ ERROR INFORMATION CF READ ERROR INFORMATION ...

  • マニュアル

    ... current/voltage switch on the base of the Interface Unit is set to the side Section 2 UPGRADING THE SYSTEM that has no tab (default). Side with no tab 2. Set the Air Particle Sensor Amplifier Unit to the RUN mode. CNT/...

  • マニュアル

    ...ZG2-DSU User’s Manual Part Names and Functions (1) (2) (3) 1 (4) BEFORE USE (5) (10) (6) (7) (9) (8) (11) (12) (14) (13) Name Function (1) CF power LED Displays the status of the power supplied to the Memory Card. This LED turns ON when power is ON, and turns OFF when power is OFF. (2) ...

  • マニュアル

    ... Format The output CSV file format can be changed according to the external device. Item Symbol Field separator None, comma (default), tab, space, or semicolon Decimal symbol None, point (default), or comma Record separator None, comma, tab, space, or CR or ...

  • マニュアル

    ... Format The output CSV file format can be changed according to the external device. Item Symbol Field separator None, comma (default), tab, space, or semicolon Decimal symbol None, point (default), or comma Record separator None, comma, tab, space, or CR or ...