全 167 件が検索されました。(101 - 120件を表示)

  • マニュアル

    ....1% X X A A U1-33 ACR(d) Output Monitor’s the current control output value for the motor’s excitation current. 10 V: 100% 0.1% X X A A U1-34 OPE Detected Displays the first constant number for which an ...

  • マニュアル

    ... 16 (0001 and 0010 Hex). The number of registers of the DSR message multiplied by two does not coincide with the number of bytes of the attached data. The write data is not within the permissible range. The data set is illegal and causes an ...

  • マニュアル

    ... 16 (0001 and 0010 Hex). The number of registers of the DSR message multiplied by two does not coincide with the number of bytes of the attached data. The write data is not within the permissible range. The data set is illegal and causes an ...

  • マニュアル

    ... been performed, turn the power supply OFF and ON again. Check and correct the register number. Note 1. When a communications error occurs, the function code MSB will be returned as “1.” Note 2. A “constant restriction” is a restriction on ...

  • マニュアル

    ...ACR (d) excitation current. Output 0.1 % No No A 60H - A A A 61H Software U1-28 No. (CPU) (Manufacturer’s CPU software No.) (Cannot be output.) CPU ID OPE fault parameter U1-34 OPE Detected PID input U1-36 volume PID Input PID output U1-37 volume PID Output PID command U1-38 PID Setpoint RS-422A/ 485 Communications Error U1-39 Transmit Err Shows the first parameter number where an ...

  • マニュアル

    ...: Register Number 0022 Hex Bit 0 1 to 2 3 4 5 to 15 ● Content During data write (1: during write) Not used. Upper/lower limit error (1: error): setting range exceeded Integration error (1: error): same as ...

  • マニュアル

    ... control 10 V: 100% U1-33 output value for the motor (−10 to 10 V possible) ACR (d) excitation current. Output 0.1 % No No A A 60H Shows the first parameter number where an OPE fault (Cannot be output.) was detected. - A A A A 61H Shows the number of PG pulses times 4 for the move(Cannot be output.) ment range when stopped at zero. 1 No No No A 62H Display Description Output voltMonitors the Inverter interage refernal voltage reference for ence (Vd) U1-27 motor excitation current Voltage Ref control. (Vd) Software U1-28 No. (...

  • マニュアル

    ... of Parts Names of Parts Inside the Front Cover 1 Main circuit terminal block (input side) Communications connector Overview 8k8k8k8 Do not touch these! (ELECTRICAL HAZARD: For factory maintenance only) Relay output terminal block S7 485 ...

  • マニュアル

    ...-485 Communication/Operator Selector> Select the mode according to the option connected to the communications connector. The 3G3AX-OP01 supplied with the Inverter can be used regardless of the switch condition. Symbol Name Status RS-485 communication/ operator selector 485 485/...

  • マニュアル

    ...) 22: F/R (3-wire forward/reverse) 23: PID (PID enabled/disabled) 24: PIDC (PID integral reset) 26: CAS (control gain switching) 27: UP (UP/DWN function accelerated) 28: DWN (UP/DWN function decelerated) 29: UDC (UP/DWN function data clear) 31: ...

  • マニュアル

    ...21: STP (3-wire stop) 22: F/R (3-wire forward/reverse) 23: PID (PID disabled) 24: PIDC (PID integral reset) 27: UP (UP/DWN function accelerated) 18 (RS) 28: DWN (UP/DWN function decelerated) 29: UDC (UP/DWN function data clear) 31: ...

  • マニュアル

    ... start) 21: STP (3-wire stop) 22: F/R (3-wire forward/reverse) 23: PID (PID disabled) 24: PIDC (PID integral reset) 27: UP (UP/DWN function accelerated) 28: DWN (UP/DWN function decelerated) 29: UDC (UP/DWN function data clear) 31: ...

  • マニュアル

    ...Code Function name Remote operation accelerated - - DWN Remote operation decelerated RS Reset 29 UDC Remote data clear JG Jogging 30 - DB Braking with external direct current 31 OPE Forced operator function 2CH 2-step acceleration/deceleration 32 SF1 Multi-step speed setting bit 1 FRS Stopping of free running 33 SF2 Multi-step speed setting bit 2 EXT External abnormality 34 SF3 Multi-step speed setting bit 3 USP Prevention of power restoration restarting 35 SF4 Multi-step speed setting bit 4 CS Commercial switch 36 SF5 Multi-step speed setting bit 5 SFT Soft-lock 37 SF6 Multi-step ...

  • マニュアル

    ...3-wire forward/reverse 23 PID PID enabled/disabled PID PID disabled 24 PIDC 27 UP 28 DWN 29 UDC UP/DWN function data clear UDC Remote operation data clear 31 OPE forced operator OPE Forced operator function 50 ADD frequency addition ADD Set frequency A145 addition PID integral reset PIDC UP/DWN function UP accelerated UP/DWN function DWN decelerated 21 PTC thermistor thermal protection PID integral reset Remote operation accelerated Remote operation decelerated 51 F-TM forced terminal block F-TM 52 RDY ready function ATR 53 SP-SET special 2nd function KHC 64 EMR emergency shutoff - 255...

  • マニュアル

    ...一 . 1月 『− A+8 1鮎 A-B W .一 1〃一占 K∼(A+B〕 1喘 (1-B!A)x100 1棚一1 B/Ax100 b口 ▼一.■ Ope「atingPa「ameter2(Previ。 usAverageVa如eC・mparis。 n) 欝繊灘㌔鱗撫 Concept・fP・evl・USAVe白9・V・1・eC・mp訂{。 。 n 「Number。 f・mθas町mg叩eγatbns [nρutv・lu. DrSplay8dvalue lC。 叩…dwlthp,。 s,猷,創ue 1 V1 V1-Vt胃0 C1=V1 2 V2 V2-C1 C2パ尼{C'+V2)日々{V1+V・)1 3一 −V3...

  • マニュアル

    ... K8AC is called the “variable area. ”The PV is read and various setting data are read and written using the variable area of K8AC. Operation commands and reding of machine attributes do not use the variable area. K8AC Microcomputer n ratio ...

  • マニュアル

    ...一一ーー IN 」 ◎ W》 1│ 3-9K 一ーし │ − Note110Ndelayti田eandOFFdelayti田earefiguresofhardNare anddonotindicatedealingtiロeofthepositioner. Note210N/OFFdelayti●esofprogra田inputandcorrectionvalue inputare6μSTYPrespectively. DetailsofBsection(transistoroutput) lCapacity lCircuit Max....

  • マニュアル

    ...Extended Operation Settings No.1 Set the operation parameter for when G500/ G501 P1 command is issued. CNC Coordinate System Extended Operation Settings No.2 Set the operation parameter for when G500/ G501 P2 command is issued. Default Refer to _sCNC_COORD_...

  • マニュアル

    ...1"ミ 5・6 ---------------------[End of Page 2308]--------------------- 、5-L2.(i21:r-JBI的なニモニヅク→フロー図変換の例 ■シートNa2 《・ニモニック表示》'… '"二 "一…' sTEPLABEL MNEMoNI'じ oPE'R'ANb ;グループ0 20GN(10)000 21LBLOOO8 ;停止断線 220UT@SOL1 ;自動モードフラグON 23AND@LS1 24WAIT ;停止断線解除 ;インターロvク1START.'.11-. 250UTNOT@SOL1 260UT@SOL3' ;アラーム点灯フ...

  • マニュアル

    ...を正しく行ってください。 表示内容は各センサモジュールのティーチングの方法を参照ください。 ・表示灯の検出(OPE)表示は、検出物体が検出距離以内に近づくと点灯し、検出状態を示します。 表示灯の安定(STAB)表示は、検出物体が検出距離の...