全 2903 件が検索されました。(1081 - 1100件を表示)
- マニュアル
... the touch points to move on the touch panel. Calibrate the touch panel periodically. ●A touch position detection error of approximately 20 pixels may occur due to the precision of the touch panel. Always take this into account when positioning objects on the panel ...
- マニュアル
... damage. Caution Indicates a potentially hazardous situation which, if not avoided, may result in minor or moderate injury, or property damage. Safety Precautions WARNING Do not touch any of the terminals or terminal blocks while the power is being supplied. Doing ...
- マニュアル
...ZKHQWKH\DUHVKLSSHGEHIRUH\RXWXUQ21WKHSRZHUVXSSO\,IWKHOD EHOVDUHQRWUHPRYHGKHDWZLOODFFXPXODWHDQGPDOIXQFWLRQVPD\RFFXU z %HIRUH\RXFRQQHFWDFRPSXWHUWRWKH&388QLWGLVFRQQHFWWKHSRZHU VXSSO\SOXJRIWKHFRPSXWHUIURPWKH$&RXWOHW$OVRLIWKHFRPSXWHUKDV DQ)*WHUPLQDOPDNHWKHFRQQHFWLRQVVRWKDWWKH)*WHUPLQDOKDVWKH VDPHHOHFWULFDOSRWHQWLDODVWKH*5WHUPLQDORQWKH3RZHU6XSSO\8QLW $GLIIHUHQFHLQHOHFWULFSRWHQWLDOEHWZHHQWKHFRPSXWHUDQG&RQWUROOHU PD\FDXVHIDLOXUHRUPDOIXQFWLRQ z ,IWKHH[WHUQDOSRZHUVXSSO\WRDQ2XWSXW8QLWRUVODYHKDVSRODULW\FRQ QHFWLWZLWKWKHFRUUHFWSRODULW\,IWKHSRODULW\LVUHYHUVHGFXUUHQWPD\ IORZLQWKHUHYHUVHGLUHFWLRQDQGGDPDJHWKHFRQQHFWHGGHYLFHVUHJDUG OHVVRIWKHRSHUDWLRQRIWKH&RQWUROOHU 3RZHU6XSSO\'HVLJQ7XUQLQJ21WKH3RZHU6XS ...
- マニュアル
... overall system even if errors or malfunctions occur in data link communications. You must take fail-safe measures to ensure safety in the event of incorrect, missing, or abnormal signals caused by broken signal lines, momentary power interruptions, or other causes. Not doing ...
- マニュアル
... of the operating mode of the CPU Unit. Provide safety measures in external circuits to ensure safety in the system if an abnormality occurs due to malfunction of the CPU Unit, other Units, or slaves or due to other external factors affecting operation. Not doing ...
- マニュアル
...: Specifications are subject to change without notice. Printed in China. (5) You must take fail-safe measures to ensure safety in the event of incorrect, missing, or abnormal signals caused by broken signal lines, momentary power interruptions, or other causes. Not doing ...
- マニュアル
... input points are energized. It is suitable for 55°C when 26 input points maximum are energized. When using in a surrounding air temperature of over 50° C, maximum 26 of the input circuits shall be connected or the input circuitry shall be designed ...
- マニュアル
... damage. Caution Indicates a potentially hazardous situation which, if not avoided, may result in minor or moderate injury, or property damage. Safety Precautions WARNING Do not touch any of the terminals or terminal blocks while the power is being supplied. Doing ...
- マニュアル
...or property damage. WARNING Serious injury may possibly occur due to loss of required safety functions. • Use equipment and parts that comply with applicable standards for the required safety levels and safety categories for all safety functions. • Wire the safety input and output lines ...
- マニュアル
... injury,or property damage. Serious injury may possibly occur due to loss of required safety functions. • Use equipment and parts that comply with applicable standards for the required safety levels and safety categories for all safety functions. • Wire the safety input and output lines ...
- マニュアル
.../IP are trademarks of ODVA. Other company names and product names in this document are the trademarks or registered trademarks of their respective companies. Precautions for Safe Use Disassembly and Dropping •Do not attempt to disassemble, repair, or modify any Units. Doing ...
- マニュアル
...す。 通信ケーブル診断はシステムに影響ない事を確認した上で、 実施してください。 Do not touch the terminals while power is being supplied. Doing so may result in electric shock. Do not attempt to disassemble the Unit. Some parts have a high voltage, particularly while the power is ON or immediately after the power isturned OFF, and they can be a cause of electric shock. Also, the sharp internal components may cause an injury. Provide external safety measures ...
- マニュアル
... external power supplies for slaves or other devices are overloaded or short-circuited, the voltage will drop, outputs will turn OFF, and the system may be unable to read inputs. Provide external safety measures in controls with monitoring of external power supply voltage as required ...
- マニュアル
... bus connector NX bus connector Provide safety measures in external circuits to ensure safety in the system if an abnormality occurs due to malfunction of the CPU Unit , Industrial PC, other Units, or slaves or due to other external factors affecting operation. Not doing ...
- マニュアル
... damage. Caution Indicates a potentially hazardous situation which, if not avoided, may result in minor or moderate injury, or property damage. Safety Precautions WARNING Do not touch any of the terminals or terminal blocks while the power is being supplied. Doing ...
- マニュアル
.... Caution Indicates a potentially hazardous situation which, if not avoided, may result in minor or moderate injury, or property damage. Safety Precautions WARNING Do not touch any of the terminals or terminal blocks while the power is being supplied. Doing ...
- マニュアル
...correctly. to the procedures provided in A slave in Free-Run Mode is set 6.4.2 Distributed Clock Setup. to the reference clock. The servo task processing time Review the program or servo exceeds the set period. frequency to adjust it, ...
- マニュアル
...correctly. to the procedures provided in A slave in Free-Run Mode is set 6.4.2 Distributed Clock Setup. to the reference clock. The servo task processing time Review the program or servo exceeds the set period. frequency to adjust it, ...
- マニュアル
...correctly. to the procedures provided in A slave in Free-Run Mode is set 6.4.2 Distributed Clock Setup. to the reference clock. The servo task processing time Review the program or servo exceeds the set period. frequency to adjust it, ...
- マニュアル
...correctly. to the procedures provided in A slave in Free-Run Mode is set 6.4.2 Distributed Clock Setup. to the reference clock. The servo task processing time Review the program or servo exceeds the set period. frequency to adjust it, ...