全 2436 件が検索されました。(1081 - 1100件を表示)

  • マニュアル

    ...T_SEGN=S11 T_SEGL=8 T_SEGN=S12 T_SEGL=8 T_SEGN=S13 T_SEGL=8 T_SEGN=S14 T_SEGL=8 T_SEGN=S15 T_SEGL=8 ::END _ CIDRW System User’s Manual 61 SECTION 3 Preparing for Communications Change Response Time-out Time In the initial settings of the CIDRW Controller, when ID Tag (RI-TRP-DR2B(-30), made by Texas Instruments) data is read or written, a response time-out may occur. Be sure to set the response time-out time to 10 s. The commands, and the parameters that can be set are indicated ...

  • マニュアル

    ...check at startup. Antenna "Error" is displayed if an error is detected in the CID Head that is connected to the Amplifier Unit (or if a CID Head is not connected). Comments "OK" is displayed for normal status. CIDRW System User’s Manual ...

  • マニュアル

    ... is ±10 mm. Steps and Warpage Double Sheet Detection Thickness Positioning Eccentricity and Surface Deflection DETAILED SETTINGS TROUBLESHOOTING SPECIFICATIONS INDEX SETTING TRANSITION CHARTS ZX2 User’s Manual Thickness ...

  • マニュアル

    ... input from and output to an external device. Display ON Setup Mode Run Mode The BUSY signal that was always ON will turn OFF. BUSY signal OFF 6 Operation FQ-CR2 User’s Manual Starting Operation 61 6-2 Configuring the Run Mode Display There are six types of displays that can be used, as shown below. Select the display as desired. Checking the Judgement Results of Inspection Items Graphics The image and region currently being measured will appear. Checking the Judgements of All Inspection Items in a List Checking the Overall Judgement Result History Graphics + Details In addition ...

  • マニュアル

    ....  Relation between Result Output and Data Indicators Result output* Data indicator status 7 6 5 Result output* Data indicator status 4 00 to 09 7 6 5 4 Section 3 ID Slave Page 61 30 to 39 3 2 1 0 3 2 1 0 7 6 5 4 7 6 5 4 3 2 1 0 10 to 19 40 to 99 3 2 1 0 7 6 5 4 3 2 1 0 *Result output converted to a decimal value. 20 to 29 : OFF : ON  Influence of Noise on Result Output and Communications Range (for...

  • マニュアル

    ... not to specify a range in the read data to output from when [Output characters] is set to ON. Sets the first and last digit positions to output. If the read text string contains non-targeted digits, the error string is output. Reading 2D-codes ...

  • マニュアル

    ... 54 0.381 60 to 185 44 × 28 to 137 × 87 Data Matrix 0.254 80 to 145 59 × 38 to 107 × 68 PDF417 0.169 85 to 130 63 × 40 to 96 × 61 0.254 65 to 180 48 × 30 to 133 × 85 QR Code Section 2 Preliminary Examination Bar code (typical example) Code types Code39 Resolution Reading distance Field-of-view size at reading distance 0.127 90 to 125 66 × 42 to 93 × 59 0.254 70 to 190 52 × 33 to 141 × 89...

  • マニュアル

    ...Height Width 8. To improve reading reliability • When the digit is determined, designate the digit to use the bar code. • Use the modulus check (addition of check digit). • Bar codes other than the reading object should be set to reading prohibition. p....

  • マニュアル

    ...59 Unused Zone Status Beams #44 (Beams 689-704 ) Unused beams set to zero. Note: Data used to maintain 32-bit alignment.. 60 Warning Zone #1 Status Beams #1 (Beams 1-16 ) Beam status bit0 to bit16 (0 = Clear , 1 = Blocked) ...

  • マニュアル

    .... 55 Power Supply Specifications When a Switching Regulator Is Connected . . . . 55 FQ-SDU20/SDU25 RS-232C Pin Signal Names . . . . . . . . . . . . . . . . . . . . . . . . 61 2-6 Setting Up Ethernet. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 67 Connecting to Sensors from the Touch Finder . . . . . . . . . . . . . . . . . . . . . . . . . 67 Connecting to Sensors from External Devices Such as PLCs . . . . . . . . . . . . . 68 Connecting to Sensors from a Computer Using the PC Tool . . . . . . . . . . . . . . 69 FQ2-S/CH User’s Manual 11 3. Taking Images 3-1 Selecting a Sensor for Configuration . . . . . . . . . . . . . . . . . . . . . . . . . . . . 74 3-2 Setting Conditions for Taking Images. . . . . . . . . . . . . . . . . . . . . . . . . . . . 75 3-3 Adjusting Image Quality . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 76 Adjusting the Focus . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 76 Adjusting Image Brightness with External Lighting . . . . . . . . . . . . . . . . . . . . . . 77 Adjusting ...

  • マニュアル

    ...Setting Output Data . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 61 Aligning the Data Output Timing with the External Device . . . . . . . . . . . . . . . . 66 Changing the Settings of the I/O Signals . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 73 Controlling Operation from an External Device . . . . . . . . . . . . . . . . . . . . . . . . . 75 3. Controlling Operation and Outputting Data with an Ethernet Connection 3-1 Controlling Operation and Outputting Data with EtherNet/IP Communications 88 Introduction to EtherNet/IP . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 88 FQ2-S/CH User’s Manual for Communications Settings 3 FQ2 Communications for EtherNet/IP Connections . . . . . . . . . . . . . . . . . . . . . 90 Setting Up EtherNet/IP Communications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 92 Tag Data Link Setting Methods . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 95 Setting the Data to Output Automatically after Measurements . . . . . . . . . . . . . 97 Memory Assignments and Commands . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 102...

  • マニュアル

    ...HREV=001.00 CIDOF=00 CIDLN=16 NVASC=NOM ::END V700-L22-V2 Operation Example CIDRW System User’s Manual SECTION 3 Setting the Communications Conditions for the CIDRW Controller Do not change operation parameters other than RT, CIDOF, ...

  • マニュアル

    ... for Amplifier Units 35 Communications Test 39 SECTION 4 Reading from/Writing to ID Tags Command/Response Format SECTION 5 Browser Interface Table of Contents Introduction 41 42 59 Browser Operation Windows 60 Window Configuration ...

  • マニュアル

    ... hook Used when fixing the Sensor Controller on DIN track. Bottom view No. Names Functions 32 Installation screw hole Used when fixing the Sensor Controller with screws. ZW-8000/7000/5000 User's Manual Part Names and Functions ...

  • マニュアル

    ... data of the executed command is stored. EtherCAT Connection TASK status Command code 3 TASKSTAT_T1-4 * SYNC signal's area is disabled in External synchronous measurement mode. ZW-8000/7000/5000 User’s Manual for Communications Settings EtherCAT Connection ...

  • マニュアル

    ...3-4-7 3-4-8 C-mount Lens for 1/3-inch Image Sensor (SV-V Series) ..........................................................3-59 C-mount Lens for 2/3-inch Image Sensor (SV-H Series) ..........................................................3-60 C-mount Lens for 1-inch Image Sensor (VS-H1 Series) ...........................................................3-...

  • マニュアル

    ... (when there is no angle information available from the Processing item used to detect the target work pieces, only the cross-hairs pointer will be displayed. 60 ・No- GripInterferenceCheck work pieces: Green ・GripInterferenceChecked work pieces: Red Debug mode: Does not display in Release mode. ...

  • マニュアル

    ...] ages with varying shutter speeds, and merge the images to produce an image with a broad dynamic range. Select an appropriate option according to the image capture environment for which you will perform calibration. Refer to Camera Image Input HDR on page ...

  • マニュアル

    ...Communications method with RF Tags Tag communications protocol Polarization characteristic Multiaccess communications V780-HMD68-ETN-JP/V780-HMD68-ETN-JP-S Japan 4 W e.i.r.p 15 to 27 dBm (Switchable in 1-dB increments.) Signal level: -35 to -...

  • マニュアル

    ...Usage: Serial Cmd: Default: Options: Only changed if necessary to match host setting. Eight 0 = Seven 1 = Eight Auto Focus Multi Code Reader V430-F-series User’s Manual (Z392) A-...