全 2268 件が検索されました。(1041 - 1060件を表示)

  • マニュアル

    ...SEND㈹ RECV(↑) CMND㈹ MSG{↑) 1/O READl/O WRITEl/O NETWORKSEND NETWORKREC日V£ DELIVERCOMMAND MεSSAGE Processingln・4strUdlons 20 TOUT SFC TRANSI一 Co加ol TION hstrudi㎝S OUTPUT 21 SA㈹ SP㈹ SR㈹ SF㈹ SE㈹ SOFF{↑} ACTIVATE PAUS[≡ RESTART ENDSTEP DEACTI一 RES[≡T STEP ST∈P STEP VATEST巨P STEP 22 '・・ 23 CNn(↑) 一ー一 RESET TIMERノ COUNTER 1・・5-2AEphabetica。 。 fist◎f納nem◎nics Mnemonic Code Name ADB㈹ 080 BINARYADD ADBL(↑) 084 DOUBLEBlNARYADD ADD(↑) 070 BCDADD ADDL(↑) 074 DOUBLEBCDADD AND(1↑↓) None AND ANDL(↑) 134 DOUBLELOGlCALAND ANDLD None ANDLOAD ANDNOT(り None...

  • マニュアル

    ...SFC Control Instructions Code 202 Mnemonic TOUT** Name TRANSITION OUTPUT Data Control, Special Calculation, and Data Conversion Instructions Code Mnemonic Name 210 SA(j)** ACTIVATE STEP 270 PID* PID CONTROL 211 ...

  • マニュアル

    ... a heater burnout detection setting range of 0.1 to 4.9 A, and allows for the rapid correction of problems. Heater burnout detection is possible for each of the two control loops. Eight Banks of Data Settings Eight data values such as set point (...

  • マニュアル

    ...Auto Mode CDD@ Manual Mode CDC@ CCD@ CCC@ ❍ ❍ ❍ ❍ EE00 EE00 ❍ ❍ ❍ ❍ ❍ ❍ ❍ ❍ ❍ ❍ ❍ ❍ ❍ ❍ AT CFC@ Cancel AT CFD@ Write SP CEEA I/O allocation commands C@@@ Write Read ❍ ❍ ❍ ❍ ❍ ❍ ❍ ❍ EE00 ❍ ❍ ❍ EE01 EE01 EE01 EE01 EE01 EE01 ❍ ❍ ❍ ❍ ❍ ❍ ❍ ❍ ❍ ❍ ❍ ❍ ❍ = Command valid Errors: EE00 = Parameter change attempted during autotuning. EE01 = Setting error When “A” is used to specify all loops, the command will not be executed for any loops if even one of the four loops does not meet execution conditions. 4. During manual operation, the manual manipulated variable will be output regardless of RUN/STOP status. 259 Section 2-6 Application 5. Parameters cannot be written and ...

  • マニュアル

    ...With SYSMAC BUS SK20-C1DT-D 8 outputs Without SYSMAC BUS SK20-C2DT-D Programming Console Vertical, hand-held with backlit LCD display. Compatible with Memory Cards. Memory Card and Connecting Cable sold separately (see below). Usable only with ...

  • マニュアル

    ...口usesaplatinumresistancethermemeter. 1「woHeaVCoolControlLoopswlthaSlngleUnlt TWoheatingandcoolingcontrolloopsarep◎ssiblewithoneUnit. Comprehenslve◎utputSpeclflcatlons Threetypesofoutputspecificationversiensareavailable:C200H-↑V口口1for transistoroutput,C200H-TV口口2forvoltageoutput,andC200H-TV口口3for currentoutput. HeaterBu『nOUtDeteCtlOn ACurrentTransformer(withadetectioncurrentrangeofO.1to49.9Aandaminimumdetectioncurrentdifferenceof2.5A)canbeconnectedtoeachofthetwo controlbopstofacilitaterapidheaterburnoutdetectionandpromptcorrectionof problems. EightBanksofDataSettings EightdatavaluessuchassetpOint(...

  • マニュアル

    ... effective in quick-response systems. Comprehensive Output Specifications Three types of output specification versions are available: C200H-PID01 for transistor output, C200H-PID02 for voltage output, and C200H-PID03 for current output. Eight Banks of Data Settings Eight data values such as set point (...

  • マニュアル

    ...『atien Connectgeneral-purposeTemperatureControllerO(∈5EiX).Downloaddata mustbesetinDO5000anditssucceedingaddresses. 1cycieON {020} ト{CMP AIwaysON 190◎00 (130) ANDW (030} MOV (030) MOV {OO1) END Execu!esdownloadprocessingwhenthe CV500-TDL21startsoperatingandsetsthecommunicationmodeofTemperatureControlierOto#2000, #2000 』 Thermac Downloadmode〈...

  • マニュアル

    ...「ばCO抑留nentsαπ45!witchSeUtnS Section2-1 、 2・1■2hStallingUserMemeiy TheCPUBoarddoesnotcomewithUserMemory,UserMemorymustbepurchasedseparatelyandirls抱1ledin伽eCPUBoard'sUserMe而◎rysocket f,2,3e..1.,Se{ectamemorychip.,ThereareRAM,EEPROM,andEPROMchipsavailablewitheitler4KwordsOr8KwOrdSOfmemory,, 2,WithCPUBoardpOweroff,atignthememorychip'snotchwiththes㏄ket's notchandinsertthechipfirmlyintOthesocket.. CPUBoard Notet,TheRAMcontentswillberetainedforabOut20daysa爺erthePC'...

  • マニュアル

    ...)controller Semi-closedloopsystemsoccupythemainstreamlnmodernservosystemsap・ pliedtopositioningdevicesforindustrialapplications. lnte『nalO erats◎ns◎ftheMCUni CommandstotheMCUnit,speedcontrolvoltagetotheservodriver,andthe feedbacksignalsfromtheencoderaredescribedinthenextfewpages. ① Desiredposition Pulsestring Error counter ⑤ Speed contrel ②veltage D/A converter Positionfeedback Feedbackpulses ③ Servodriver Servomotor ...

  • マニュアル

    ...beturnedONandtheerrorcodewillbeoutputtoDMwordm+45.{Theerror messageinparentheseswiilbedisplayedattheTeachingBox.} Code Error ErrorProcessing 0001 Systemparametersdestroyed(SYSPARACORRUPT) Thesystemparametershavebeendestroyed.(Seenotet)DownbadthesystemparametersfromtheMCSupportSoftwareagain,andthenturnthepowerOFFandON.Thesystemparameterscanbedestroyedbyanyofthefolbwing:Thememorydatamighthavebeendestroyedbynoise.Thebackupbatteryvo‖agemighthavedropped.ThePC{MCUn‖)mighthavebeenturnedOFFwhilethesystemparameterswerebeingdownloaded.Thiserrorcan'tbeclearedbyanerrorreset. 0002 Wrongnumberoftasks(TASKNOTCONSIST) Thenumberoftasksregisteredinthesystemparametersdoesn'tmatchthenumberregisterintheprogram.(Seenote1.)Eitherdeletea‖programsusingtheMCSupportSoftwareordownloadsystemparameterswiththenumberoftasksthatmatchesthenumberregisteredhtheP「ogram・Theerrorisclearedautomaticallywhenallprogramsaredeleted.D◎wnloadtheprogram(s)again.Whendownloadingthesystemparametersagain,tumtheUnit'...

  • マニュアル

    ...q N No. Communications sequence q name Function Ladder interface Send word allocation Yes Receive word allocation Yes 000 Read process value Reads the process value. 001 Read set point during SP ramp Yes Yes 002 Read MV Reads the set point during ...

  • マニュアル

    ...The BASIC character set comprises alphabetical characters, numeric characters, and special characters. The alphabetic characters in BASIC are the uppercase and lowercase letters of the alphabet. The numeric characters in BASIC are the digits 0 through 9. The following special characters are recognized by BASIC: ...

  • マニュアル

    ...Attempted to output an M code from a position data address or register, but the content wasn’t within the acceptable range for M codes (000 to 999). Make sure that the M code is from 000 to 999. 0026 Interpolation rate not set (INTER ...

  • マニュアル

    ...)◆・RXO・4・$(N,1}◆・00・◆1』RC{HParity){e){2byteASC)+【2AOD】 3・8・4ReceiveMessageCreati◎n ●Writingthedataofthemeasuredtemperaturetothethirdoperandofthe PMCRinstruction+(2N+1)withoutfixingtheIength. Note:Nmeansthevalueoftherepeatcounter. DNUO100 +2 n+3 舗 Thrdepennd −Eヨ4byles -Eiヨ・t・ytes −ー一→レ...

  • マニュアル

    ...C T T C T C I N I T N I N M T M I T M T W W H M R (SP) (SP) Note “SP” represents a space (20 Hex). Response Format @ x 101 x 100 Unit No. (BCD) Parameters R # Header code x 161 x 160 x 103 x 102 x 101 x 100 End code SV of instruction designated by command (constant) * FCS ↵ Terminator Timer/Counter Type (Command) Designate in ASCII characters the type of TC instruction for reading the constant SV. Timer Counter Number (Command) Designate in four digits (BCD) the timer/counter ...

  • マニュアル

    ... Board via RS-232C or RS-485 cable. Structure of the Protocol The following table shows the structure of the E5@K Digital Controller Read Protocol. Sequence No. 000 001 Communications sequence name Read process value Read set point during ...

  • マニュアル

    ... to set initial data S and the CX-Process Monitor is normally used to set operation data O. Data classification Initial settings Type ITEM Example: PID Block S Initial setting parameter for each function block Forward/Reverse direction, ...

  • マニュアル

    ...Monitor. Also, when using the CX-Process Monitor, make sure that the License key WS02-LCTK1-EL01 is always connected to the printer port. You can also perform the following four functions. Monitoring Function Blocks in a Loop Control Unit Monitor PV, ...

  • マニュアル

    ... read and write CPU Unit I/O memory. Connect ES100X Controllers Externally (CS1W-LCB01/05 Only) ES100X Controllers can be connected to the RS-232C port on the Loop Controller and ES100X External Controller Terminal function blocks can be used to monitor ES100X parameters, such as the ...