全 2268 件が検索されました。(1081 - 1100件を表示)
- マニュアル
... the power turned ON. Normally, there are no problems in using the default settings. • Auto command abort time • Write verification The CF Reader/Writer is initialized when the power is turned OFF and the operating parameter settings are not stored. Refer to Parameter Setting (...
- マニュアル
...1101 1010 1011 1100 1101 1110 1111 0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 TC7(DLE) (SP) 0 @ P ` p A Q a q Undefined Undefined Undefined Undefined Undefined Undefined Right digit b8 to b5 Undefined Left digit Undefined List of ASCII Characters Column b4 to b1 List of ASCII Characters Section 6 Row 136 0000 0 NUL 0001 1 TC1(SOH) DC1 ! 1 0010 2 TC2(STX) DC2 " 2 B R b r 0011 3 TC3(ETX) DC3 # 3 C S c s 0100 4 TC4(EOT) DC4 $ 4 D...
- マニュアル
... 1101 1010 Undefined 1001 Undefined b4 to b1 0000 Undefined Rightmost digit b8 to b5 Undefined Leftmost digit Row 0000 0 NUL 0001 1 TC1(SOH) DC1 TC7(DLE) (SP) @ P ` p 1 A Q a q 0010 2 0011 3 TC2(STX) DC2 " 2 B R b r TC3(ETX) DC3 # 3 C S c s 0100 4 TC4(EOT) DC4 $ 4 D T d t 0101 5 TC5(NEQ) TC8(NAK) % 5 E U e u 0110 6 TC6(ACK) TC9(SYN) & 6 F V f v 0111 7 BEL TC10(ETB) ' 7 G W g w...
- マニュアル
... to LF(0Ah) is 512 bytes or less. Command frame for Ethernet Command Code Command Data LF 4 n 1 UHF RFID System User's Manual SECTION 5 Command Line Interface Command Format Command Code SP Parameter 1 ...
- マニュアル
...Output from when a command is received from the host device until communications have been completed. ERROR Output for 500 ms when there is an error in Data Carrier communications, host device communications, or hardware. The output time can be changed with the SET PARAMETER (...
- マニュアル
...No designated number of digits Detail condition CODE39 detail setting Invalid C/D of CODE39 Section 4 Menu Sheet/Command List Transfer C/D of CODE39 NW-7 detail setting ITF/STF detail setting Reading condition C0 C2 Transfer ST/...
- マニュアル
...V680-HA63A V680-HS51 V680-HS52 V680-HS61 V680-HS63 V680-HS65 V680-H01-V2 RF Tags V680-D1KP52MT V680-D1KP52M-BT01 V680-D1KP52M-BT11 V680-D1KP53M V680-D1KP54T V680-D1KP66T V680-D1KP66MT V680-D1KP66T-SP V680-D1KP58HTN Man. No.: Z262-E1-10 Introduction Thank you for purchasing a V680-series RFID System. This manual describes the functions, performance, and application methods needed for optimum use of the V680-series RFID System. Please observe the following items when using the RFID System. • Allow the RFID System to be installed and operated only by qualified specialist with a sufficient knowledge of ...
- マニュアル
...settings UPC-E: Transfer C/D without an 0 in the beginning Section 4 Menu Sheet/Command List EAN-13: Transfer C/D EAN-8: Transfer C/D CODE39 detail settings Not calculate C/D Transfer C/D Not transfer ST/...
- マニュアル
... field of view of measurement object is 40 mm, and a 3Z4S-LEML-5018 lens is used, the camera setting distance is set at 500 mm, and a 5 mm extension tube is required. 9 Appendixes Small camera FZ-SF 316 About Lenses /...
- マニュアル
... stage coordinate system by inputting the robot or X-Y-Theta stage movement amounts and measuring the reference marks. P.73 1-3 Limitations and Precautions [Compatible cameras] - Only the monochrome cameras listed below are compatible. FZ-S/FZ-S2M/FZ-S5M/FZ-...
- マニュアル
...Stand-alone camera - 300,000-pixel Color/Monochrome camera FZ-SC/FZ-S 300,000-pixel Small-size flat type Color/Monochrome camera FZ-SF/FZ-SFC(*2) 300,000-pixel Small-size pen type Color/Monochrome camera FZ-...
- マニュアル
... B. Switch Code Set to C. US (0 1F) or Delete (0 7F) Text shift indicator 1 1 1 1 1 1 1 Input text and the meanings in Code Sets A and B Input Sp ! " # $ % & ' ( ) * + , . / Code A Sp ! " # $ % & ' ( ) * + , . / Code B ...
- マニュアル
...Switch Code Set to A. Switch Code Set to B. Switch Code Set to C. US (0 1F) or Delete (0 7F) Text shift indicator Input text and the meanings in Code Sets A and B 2 - 48 Input Sp ! " # $ % & ' ( ) * + , . / Code A ...
- マニュアル
... bits Upper 4 bits 360 0 1 2 3 4 5 6 7 8 9 A B C D E F 0 1 2 3 4 5 6 D SP 0 @ P ` E S D 1 A Q a H 1 ! S D 2 B R b X 2 ” E D C S c X 3 # 3 E D D T d T 4 $ 4 E N E U e Q K % 5 A S F V f K N & 6 B E L B B C S H N E T L M S F H B E...
- マニュアル
...FH-SC04 FH-SM04 FZ-S5M3 FZ-SC2M FZ-S2M FZ-SC FZ-S FZ-SHC 4.9 ms 12.5 ms 12.5 ms FZ-SH FZ-SFC FZ-SF FZ-SPC FZ-SP Vision System FZ5 series Hardware Setup Manual (Z423) 1 Confirm the Package Type Intelligent Compact Digital CMOS Cameras (Camera + Manual Focus Lens + High power Lighting) Description Color / Monochrome Narrow view Color Standard view Color Wide View (long-distance) Color Wide View (short-distance) Color Image Acquisition Model Reference Time*1 FZ-SQ010F FZ-SQ050F 16.7 ms FZ-SQ100F FZ-SQ100N 1 *1. The image ...
- マニュアル
...ください。 感電・火災・故障の原因になります。 ・出力の負荷は短絡させないでください。 8 2 DI GI T A L I ON DI SP L A Y ・放電モジュールは、45°回転することで取り外し、取り付けが可能です。 ① 設置場所・本体は、壁から30mm以上離して設置してくだ...
...K3FM-RS 測温抵抗体変換器 (アナログ形) 全抵抗値 100Ω∼10kΩ 形K3FM-MS ポテンショメータ変換器 (アナログ形) 形K3FM-SP スローパルス変換器 (50Hz以上) 無電圧スイッチ、 電圧パルス センサ入力変換器 交流電圧 形K3FM-PA/PE PT変換器 交流電流 形K3FM-CA/CE CT変換器 交...
- 商品情報
...ジュールのバージョン】 2.5 【このプログラムでの修正事項】 オフラインで設定した後、オンラインにしても「PVのみ(SP表示なし)表示の追加」の設定が、接続した形E5□N本体の設定値で上書きされないようにしました。 測温抵抗体入力タイプ...
...は、Microsoft Windows™上で動作するアプリケーションです。 次のバージョンのMicrosoft Windows上で動作します。 • Windows 10 • Windows 8.1 • Windows 8 • Windows 7 SP 1 PowerPMAC IDEには.NET Framework 4.6以上が必要です。 存在しないフレームワークが識別され、自動的にインストールされます。 ハードウェア • • • • • 1....
- 商品情報
...7-4 制御演算機能 D-AT 起動判定と外乱発生判定を行う温度偏差を設定します。 D-AT 実行時、測定値 (PV) と目標値 (SP) の絶対偏差が本パラメータ以下であれば D-AT が起動します。 D-AT 起動後、測定値 (PV) と目標値 (...