全 194 件が検索されました。(81 - 100件を表示)
- マニュアル
...mm2) 9-Pin socket NX-series Communications Interface Units User’s Manual (W540) UL2464 AWG28 ´ 5P IFS-RVV-SB (UL Product) AWG28 ´ 5P IFVV-SB (Non-UL Product) • Hitachi Metal UL2464-SB (MA) 5P ´ 28AWG (7/0.127) (UL Product) CO-MA-...
- マニュアル
... hex 8 03 hex 16 6YYY hex YY hex PDO-Length: 32 bits PDO_1 Application object 6TTT hex TT hex Object B Object D Object A 6UUU hex UU hex Object B 6VVV hex VV hex Object C 6YYY hex YY hex Object D 6ZZZ hex Object E ZZ hex Object A PDO Mapping with EtherCAT Slave Units EtherCAT Slave Units have fixed PDO mapping and adjustments to the objects are not possible. The fixed PDO mapping of the EtherCAT Slave Units is provided in the table below. RxPDO PDO mapping object Name Index number I/O ...
- マニュアル
... hex 8 03 hex 16 6YYY hex YY hex PDO-Length: 32 bits PDO_1 Application object 6TTT hex TT hex Object D Object B Object A 6UUU hex UU hex Object B 6VVV hex VV hex Object C 6YYY hex YY hex Object D 6ZZZ hex Object E ZZ hex Object A PDO Mapping with EtherCAT Slave Units EtherCAT Slave Units have fixed PDO mapping and adjustments to the application objects are not possible. The fixed PDO mapping of the EtherCAT Slave Units is provided in the table below. RxPDO PDO mapping object Name Index number I/...
- マニュアル
...Use shielded twisted-pair cables for the communications cables. • Recommended RS-232C Cables Model numbers Manufacturer UL2464 AWG28x5P IFS-RVV-SB (UL product) AWG28x5P IFVV-SB (non-UL product) Fujikura Ltd. UL2464-SB (MA) 5Px28AWG (7/0.127) (UL product) CO-MA-...
- マニュアル
...Use shielded twisted-pair cables for the communications cables. • Recommended RS-232C Cables Model numbers UL2464 AWG28x5P IFS-RVV-SB (UL product) Manufacturer Fujikura Ltd. AWG28x5P IFVV-SB (non-UL product) UL2464-SB (MA) 5Px28AWG (7/0.127) (UL product) CO-MA-...
- マニュアル
...02 hex 6UUU hex UU hex 8 03 hex 16 6YYY hex YY hex PDO-Length: 32 bits PDO_1 Application object 6TTT hex TT hex Object A 6UUU hex UU hex Object B 6VVV hex VV hex Object C 6YYY hex YY hex Object D 6ZZZ hex Object E ZZ hex Object A Object B Object D Application objects define the I/O data allocated to the PDO mapping objects. The PDO mapping objects define these I/O data sets. PDO Mapping with EtherCAT Slave Units PDO mapping objects contain the I/O data provided by the EtherCAT Slave ...
- マニュアル
...8 — NC — Not connected 9 — NC — Not connected Always OFF Recommended model Manufacturer Cable Connector Socket Hood 32 CIDRW System User’s Manual Model Hitachi Cable CO-MA-VV-SB 5PX28AWG OMRON XM2D-0901 XM2S-0913 SECTION 2 Installation and Connections/Wiring • Wiring The cable length should be no greater than 15 m. PC/AT Computer D-SUB, 9-pin Socket type #4-40 Name Pin No. Pin No. Name NC 1 1 NC RD 2 2 RD SD 3 3 SD NC 4 4 NC SG 5 5 SG NC 6 6 NC RS 7 7 RS NC 8...
- マニュアル
...8 — NC — Not connected 9 — NC — Not connected Always OFF Recommended model Manufacturer Cable Connector Socket Hood 28 CIDRW System User’s Manual Model Hitachi Cable CO-MA-VV-SB 5PX28AWG OMRON XM2D-0901 XM2S-0913 SECTION 2 Installation and Connections/Wiring • Wiring The cable length should be no greater than 15 m. PC/AT Computer D-SUB, 9-pin Socket type #4-40 Name Pin No. Pin No. Name NC 1 1 NC RD 2 2 RD SD 3 3 SD NC 4 4 NC SG 5 5 SG NC 6 6 NC RS 7 7 RS NC 8...
- マニュアル
...8 — NC — Not connected 9 — NC — Not connected Always OFF Recommended Models Manufacturer Cable Connector Socket Hood 38 CIDRW System User’s Manual Model Hitachi Cable CO-MA-VV-SB 5PX28AWG OMRON XM2D-0901 XM2S-0913 SECTION 2 Installation and Connections/Wiring • Wiring The cable length should be no greater than 15 m. PC/AT Computer D-SUB, 9-pin Socket type #4-40 Name Pin No. Pin No. Name NC 1 1 NC RD 2 2 RD SD 3 3 SD NC 4 4 NC SG 5 5 SG NC 6 6 NC RS 7 7 RS NC 8...
- マニュアル
...User’s Manual Section 5 Example of System Configuration Wiring Example of wiring when connecting with PC/AT compatible PC is explained. Cable length should be 15 m or less. Recommended parts Model Cable Connector Manufacturer CO-MA-...
- マニュアル
...8 Clear to send CS Input Operates even if not connected. 9 — NC — Not connected Always OFF Recommended Models Manufacturer Cable*1 Connector Socket Hood Model Hitachi Cable CO-MA-VV-SB 5PX28AWG OMRON XM2D-0901 XM2S-0913 *1: The bending radius of the recommended RS-232C cable is 44 mm. 36 CIDRW System User’s Manual SECTION 2 Installation and Connections/Wiring • Wiring The cable length should be no greater than 15 m. PC/AT Computer D-SUB, 9-pin Socket type #4-40 Name Pin No. Pin No. Name NC 1 1 NC RD 2 2 RD SD...
... Configuration 5.2. Device Configuration The system components required for reproducing the connection procedures described in this guide are as follows. PC (Sysmac Studio installed, OS: Windows 11) NX102-1200 (Built-in EtherCAT port) VTEP-FEC-B1-QL-QL-QP-P-...
...器は以下のとおりです。 形 NX102-1200 パソコン(Sysmac Studio、 (内蔵 EtherCAT ポート) インストール済み、 OS:Windows 11) VTEP-FEC-B1-QL-QL-QP-P-VV 電源 LAN ケーブル Ethernet ケーブルユニット用電源バルブ用電源 メーカオムロン 名称 NX シリーズ CPU ユニット (内蔵 EtherCAT ポート) 形式形 NX102-1200 - オ...
- 商品情報
...形 XM2S-2511 25 ピンオムロン製 AWG28 5P マルチコアシールドケー --ブル IFVV-SB 形 CV500-LK201 形 C200H-LK201-EV1 フジクラ製 CO-MA-VV-SB 5P 28AWG マルチコアシールドケー --ブル 日立電線製注)通信ケーブルを接続した後は、必ずコネクタのネジを締めてください。 2- 58 2−6 RS-...
- マニュアル
...16 6YYY hex YY hex PDO-Length : 32 Bit PDO_1 Application objects 6TTT hex TT hex 5-4-3 Object A Object B Object D Object A 6UUU hex UU hex Object B 6VVV hex VV hex Object C 6YYY hex YY hex Object D 6ZZZ hex ZZ hex Object E Sync Manager PDO Assignment Settings A sync manager channel consists of several PDOs. The sync manager PDO assignment objects describe how these PDOs are related to the Sync Manager. The number of PDOs is given in sub-index 0 of the sync manager PDO assignment table. In this ...
- マニュアル
...Level 1 Mode Heater current monitor Conditions of Use The HBA output function must be assigned as the output. • Measures the current value of the heater from CT input. Function • This parameter is not displayed when the linear output unit (E53-CV, E53-...
- マニュアル
...Level 1 Mode Heater current monitor Conditions of Use The HBA output function must be assigned as the output. • Measures the current value of the heater from CT input. Function • This parameter is not displayed when the linear output unit (E53-CV, E53-...
- マニュアル
...(0! %. +),-! 2%/$ /$! 1(0! .!/ . /$! 5$!/!- 0-*+0/ .!/ 1(0! * /$! +0/,0/ !+)!. /%1! . /$! $!/!- 0-*+0/ (-) • !/ /$! $!/!- 0-*+0/ .!/ 1(0! %* /$! 5$!/!- 0-*+0/ !/!/%+* ,-)!/!- &0./)!*/ (!1!( + )+*%/+- /$! 0--!*/ 1(0! +" /$! 0-7 -!*/ /-*."+-)!- 0.! /$! 5$!/!- 0--!*/ )+*%/+- ,-)!/!- • $!* "0*/%+* %. *+/ 0.! .!/ /$! 5$!/!- 0-*+0/ ,-)!/! 1*! "0*/%+* .!//%*# (!1!( /+ 5 ...
- マニュアル
...leSS),motorOVerheatingOrlnVertermalfunctionmayOCCUr. OutputLimiterSelectienWhenV/fissettoanexcessivelylargevalue,aninverterfaultmay occur.Therefore,inordertopreventmalfunction,anupperlimit canbesetfortheoutputvoltage.However,thesettjngisnotnecessaryundernormaloperation. No.Oi=Oxxx L4thdigit O:DesiredV/fwithoutputvoltagelimiter 1:DesiredV/fwithoutoutputvoitagelimiter V む 25 (㌃←o=Φωの) Φぽ壱三コ巳コO ...
- マニュアル
...A6001(・ロ) A8002{・ロ) A日oo4←口} ABOO7(・口) ABO15{・ロ} SlnglephaselThreePhase,200V瓜C Power鯛pply RatedvoltageandfreqUency 一一.Single・phase,200to240VAC,50κ}OHzThree・phase,200to230VAC,50160Hz Albwabbvol抽gefluctuatlon 一15%b10% −Allowabl6frequencyfluctu8tlon ±5% }■{6atlngvalue(...