全 208 件が検索されました。(81 - 100件を表示)

  • マニュアル

    ...) e.g.: Tm = 0.05s, Ts = 0.01s, d =25 mm: S = 2,000 mm/s x (0.05s + 0.01s) + 8 (25 mm - 14 mm) = 208 mm Safety distance Beam centre-line Hazardous part Intrusion direction Detection zone Use S = 100 mm if the result of equation (2) is less than 100 mm. Recalculate using the following equation with K = 1,600 mm/s if the result is over 500 mm. S = 1,600 mm/s x (Tm + Ts) + 8 (d - 14 mm) ...(3) Use S = 500 mm if the result from equation (3) is less than 500 ...

  • マニュアル

    ...) e.g.: Tm = 0.05s, Ts = 0.01s, d =14 mm: S = 2,000 mm/s x (0.05s + 0.01s) + 8 (14 mm - 14 mm) = 120 mm Safety distance Beam centre-line Hazardous part Intrusion direction Detection zone Use S = 100 mm if the result of equation (2) is less than 100 mm. Recalculate using the following equation with K = 1,600 mm/s if the result is over 500 mm. S = 1,600 mm/s x (Tm + Ts) + 8 (d - 14 mm) ...(3) Use S = 500 mm if the result from equation (3) is less than 500 ...

  • マニュアル

    ... the F3SR-B (mm) [Calculation example] When Tm = 0.05 s, Ts = 0.015 s, and d = 30 mm: S = 2,000 mm/s × (0.05 s + 0.015 s) + 8 × (30 mm - 14 mm) = 258 mm If the result < 100 mm, use S = 100 mm. If the result exceeds 500 mm, use the following expression where K = 1,600 mm/s. S = 1,600 mm/s × (Tm + Ts) + 8 × (d - 14 mm). . . formula (2) If the result of this formula (2) < 500 mm, use S = 500 mm. 17 F3SR-B User’s Manual Wiring/...

  • マニュアル

    ...” setting is valid. Do not select “Indrct”. 118 Creating Graphs Section 4-8 S Ref Table: Specify the number of the memory table to be referenced here. Pressing the [F1] (Lst Slct) key enables selection from a memory table list. ...

  • マニュアル

    ...4,800 = 110,648 (µs) ≅ 111 (ms) And the communications cycle time in token-bus mode is as follows: 9.1 × 8,000 + 1,300 × 4 + 290 × 8 + 320 × 2 + 4 × 4,024 + 2 × 7 × 8 + 2,290 = 99,458 (µs) ≅ 100 (ms) 9-2-2 Inactive Data Links The following equations are used to calculate a communications cycle time when the data link is inactive. Token-ring Mode 1,740 × B +450 × C + 1,100 × D + 4 × E + 2 × F + 3,000 (µs) Token-bus Mode 1,...

  • マニュアル

    ... one Ai4 Terminal, Segment Linearizer, Basic PID, and A04 terminal) is shown in the following table. CS1W-LCB01/05 (LCCB01/05) Operation cycle: Maximum number of loops 0.01 s: 20 loops 0.02 s: 35 loops 0.05 s: 70 loops 0.1 ...

  • マニュアル

    ... function) Tags 480 max. 960 max. Maximum save Collection cycle Collection cycle time 1 s: 10 h 1 min: 30 days 2 s: 20 h 5 min: 150 days 5 s: 50 h 10 min: 300 days 10 s: 100 h 30 min: 900 days 30 s: 300 h 60 min: 1,800 days Collection cycle Data display Horizontal axis Collection cycle 1 min: 2 h to 10 days 1 s: 2 min to 240 min 5 min: 10 h to 50 days 2 s: 4 min to 240 min 10 min: 20 h to 100 days 5 s: ...

  • マニュアル

    ... up logging. Operation Procedure 1. Display the [Logging Standby] window and start logging. Setting item Description You can select the width of the horizontal axis of the graph according to the Horizontal axis of graph logging time. (Not plot, 1 s, 10 ...

  • マニュアル

    ...[Calculation example] When Tm = 0.05 s, Ts = 0.008 s, and d = 14 mm: S=2,000 mm/s x (0.05 s + 0.008 s) + 8 x (14 mm - 14 mm) = 116 mm . . . Formula (2) If the result < 100 mm, use S = 100 mm. If the result exceeds 500 mm, use the following expression where K = 1,600 mm/s. S=1,600 mm/s x (Tm + Ts) + 8 x (d - 14 mm) . . . Formula (3) If the result of this formula (3) < 500 mm, use S = 500 mm. Calculation Example for Systems with Larger Detection Capability than ...

  • マニュアル

    ...[Calculation example] When Tm = 0.05 s, Ts = 0.008 s, and d = 25 mm: S=2,000 mm/s x (0.05 s + 0.008 s) + 8 x (25 mm - 14 mm) = 204 mm . . . Formula (2) If the result < 100 mm, use S = 100 mm. If the result exceeds 500 mm, use the following expression where K = 1,600 mm/s. S=1,600 mm/s x (Tm + Ts) + 8 x (d - 14 mm) . . . Formula (3) If the result of this formula (3) < 500 mm, use S = 500 mm. 36 F3SG-4RA-25-01TS User’s Manual Wiring/...

  • マニュアル

    ...[Calculation example] When Tm = 0.05 s, Ts = 0.008 s, and d = 14 mm: S=2,000 mm/s x (0.05 s + 0.008 s) + 8 x (14 mm - 14 mm) = 116 mm . . . Formula (2) If the result < 100 mm, use S = 100 mm. If the result exceeds 500 mm, use the following expression where K = 1,600 mm/s. S=1,600 mm/s x (Tm + Ts) + 8 x (d - 14 mm) . . . Formula (3) If the result of this formula (3) < 500 mm, use S = 500 mm. 108 F3SG-RR User’s Manual Wiring/Installation Calculation ...

  • マニュアル

    ...[Calculation example] When Tm = 0.05 s, Ts = 0.008 s, and d = 25 mm: S=2,000 mm/s x (0.05 s + 0.008 s) + 8 x (25 mm - 14 mm) = 204 mm . . . Formula (2) If the result < 100 mm, use S = 100 mm. If the result exceeds 500 mm, use the following expression where K = 1,600 mm/s. S=1,600 mm/s x (Tm + Ts) + 8 x (d - 14 mm) . . . Formula (3) If the result of this formula (3) < 500 mm, use S = 500 mm. 36 F3SG-4RA-25-02TS User’s Manual Wiring/...

  • 商品情報

    ...ズの機能です。 日本語 English PDF出力 画像をクリックすると大きくなります Power OFF-delay Timer, 8-pin, Forced reset: None, Time range 0.05 to 12 s, 100/110/120 VAC Power OFF-delay Timer, 8-pin, Forced reset: None, Time range 0.05 to 12 ...

  • 商品情報

    ...ズの機能です。 日本語 English PDF出力 画像をクリックすると大きくなります Solid-state Timer, Power OFF-delay Timer, Control output: SPDT, Time range 1 to 120 s, 100 to 120 VAC Solid-state Timer, Power OFF-delay Timer, Control output: SPDT, Time range 1 to 120 ...

  • 商品情報

    ...の機能です。 日本語 English PDF出力 画像をクリックすると大きくなります Solid-state Timer, Power OFF-delay Timer, Control output: SPDT, Time range 0.1 to 12 s, 100 to 120 VAC Solid-state Timer, Power OFF-delay Timer, Control output: SPDT, Time range 0.1 to 12 ...

  • 商品情報

    ...) Insulation resistance 20 MΩ min. (at 500 VDC) Dielectric strength Between the entire external terminal and case: 2,300 VAC 1 min Noise immunity ±1,500 V at power supply terminals in normal or common mode (waveform with 1-ns rising edge and pulse width of 1 µ...

  • 商品情報

    ...) Insulation resistance 20 MΩ min. (at 500 VDC) Dielectric strength Between the entire external terminal and case: 2,300 VAC 1 min Noise immunity ±1,500 V at power supply terminals in normal or common mode (waveform with 1-ns rising edge and pulse width of 1 µ...

  • 商品情報

    ...%.) Insulation resistance 20 MΩ min. (at 500 VDC) Dielectric strength Between the entire external terminal and case: 2,300 VAC 1 min Noise immunity ±1,500 V at power supply terminals in normal or common mode (waveform with 1-ns rising edge and pulse width of 1 µ...

  • 商品情報

    ...%.) Insulation resistance 20 MΩ min. (at 500 VDC) Dielectric strength Between the entire external terminal and case: 2,300 VAC 1 min Noise immunity ±1,500 V at power supply terminals in normal or common mode (waveform with 1-ns rising edge and pulse width of 1 µ...

  • 商品情報

    ...%.) Insulation resistance 20 MΩ min. (at 500 VDC) Dielectric strength Between the entire external terminal and case: 2,300 VAC 1 min Noise immunity ±1,500 V at power supply terminals in normal or common mode (waveform with 1-ns rising edge and pulse width of 1 µ...