全 208 件が検索されました。(21 - 40件を表示)

  • マニュアル

    ...Between external terminals and case 2,300 VAC for 1 min between external terminals and case Noise immunity 100 to 240-VAC models: ±1,500 V at power supply terminals in normal or common mode (waveform with 1-ns rising edge and pulse width of 1 µ...

  • マニュアル

    .... by H’FFFFFFF7 to H’00000009: (−9 to 9) 10 -9 to 10 9 10 0 --- --- 0015 Time unit time H’00000000: OFF (0) H’00000001: min (1) H’00000002: hour: min: s (2) H’00000003: min, s: 100 ms (3) off, min, h. mm. ss, mm. ss. d off --- --- 000D Decimal point position dp H’00000000 to H’00000004: (0 to 4) \\\\\, \\\\. \, \\\. \\, \\. \\\, \. \\\\ \\\\\ --- --- 000E Comparative output pattern out-p H’00000000: Standard outputs (0) H’00000001: Zone outputs (1) H’00000002: Level outputs (2) nomal, zone, level nomal --- --- The values beginning with H' in the Monitor/Setting range column ...

  • マニュアル

    ...0.0000 to 9.9999 0. 0000 to 9. 9999 1.0000 4 --- Prescale BY ps. by −9 to 9 -9 to 9 0 --- --- Time unit time OFF, min, hour: s:, min, s: 100 ms off, min, h. mm. ss, mm. ss. d OFF --- --- Decimal point position dp 0 to 4 \\\\\, \\\\. \, \\\. \\, \\. \\\, \. \\\\ 0 --- --- Comparative output pattern out-p Standard outputs, zone outputs, level outputs normal, zone, level Standard outputs --- --- Move to the advanced function setting level amo? −19999 to 99999 :9999 to 99999 0 --- --- Averaging type a?g-t Simple average, moving average smpl, mo?e Simple average --- --- Averaging times a?...

  • マニュアル

    ...ンスマニュアル(SBCA-356) 2 各命令の説明 サンプルプログラム 0.00 MLPX 100 K #0021 D D100 15 K: # 桁→ S:100 8 7 4 3 0 0 0 2 1 3 F 2 A 1 6 0 ビット0∼3:開始桁ビット4∼7:デコード対象の桁数 2 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0 1 100CHの桁1の"6"...

  • マニュアル

    ...int float int i = (int)100 float f = (float)100 i = 100 f = 100 double double d = (double)100 d = 100 bool bool flag = (bool)0 flag = true (not null) string string s = (string)100 s = "100" byte byte b = (byte)1000 b = 232 float float f = (float)1000 f = 1000 double double d = (double)1000 d = 1000 bool bool flag = (bool)1000 flag = true (not null) string string s = (string)1000 s = "1000" byte int byte b = (byte)1.23 int i = (int)1.23 b=1 i=1 double double d = (double)1.23 d = 1.23 bool...

  • マニュアル

    ...ると(Dが#0000でないとき)定時割り込み許可状態になります。 まとめて割り込み制御の禁止/許可を設定したいときは、S=100(全ての割り込み禁止)またはS=200(全ての割り込みを許可)を指定します。 割り込みプログラムと通常プログラムでデ...

  • マニュアル

    ...- 間接データメモリ定数 - - *D0000-1999 - - - *D0000-6655 - - - HR00-99 AR00-27 LR00-63 T/C000-511 *2 D0000-6655 *D0000-6655 *3 *1 S=100、200のとき N=任意、D=任意、割り込みサブルーチン内では指定不可 *2 S=002のときDは読み出し専用エリアは不可(253∼255、DM6144∼6655) *3 S=000、001のとき指定不可。 N=000、001のと...

  • マニュアル

    ...ると(Dが#0000でないとき)定時割り込み許可状態になります。 まとめて割り込み制御の禁止/許可を設定したいときは、S=100(全ての割り込み禁止)またはS=200(全ての割り込みを許可)を指定します。 割り込みプログラムと通常プログラムでデ...

  • マニュアル

    ... 100,200 - N 000,001,004 - D *2 000-255 256-511 HR00-99 AR00-27 LR00-63 T/C000-511 *2 D0000-6655 E0000-6143 *D0000-6655 *E0000-6143 *3 *1 S=100、200のとき N=任意、D=任意、割り込みサブルーチン内では指定不可 *2 S=002のときDは読み出し専用エリアは不可(253∼ 255、DM6144∼6655) *3 S=000、001のとき指定不可。 N=000、001...

  • マニュアル

    ... of the detection zone above 300 mm in relation to the reference plane does not offer sufficient protection against crawling below. First, use K = 2,000 mm/s in formula (5) for the calculation. If the result of this calculation is less than 100 mm, use ...

  • マニュアル

    ... of the detection zone above 300 mm in relation to the reference plane does not offer sufficient protection against crawling below. First, use K = 2,000 mm/s in formula (5) for the calculation. If the result of this calculation is less than 100 mm, use ...

  • マニュアル

    ... of the detection zone above 300 mm in relation to the reference plane does not offer sufficient protection against crawling below. First, use K = 2,000 mm/s in formula (5) for the calculation. If the result of this calculation is less than 100 mm, use ...

  • マニュアル

    ... of the detection zone above 300 mm in relation to the reference plane does not offer sufficient protection against crawling below. First, use K = 2,000 mm/s in formula (5) for the calculation. If the result of this calculation is less than 100 mm, use ...

  • マニュアル

    ... of the detection zone above 300 mm in relation to the reference plane does not offer sufficient protection against crawling below. First, use K = 2,000 mm/s in formula (5) for the calculation. If the result of this calculation is less than 100 mm, use ...

  • マニュアル

    ... (mm) [Calculation example] When Tm = 0.05 s, Ts = 0.015 s, and d = 25 mm: S = 2,000 mm/s x (0.05 s + 0.015 s) + 8 x (25 mm - 14 mm) = 218 mm If the result is less than 100 mm, use S = 100 mm. If the result exceeds 500 mm, use the following formula where K = 1,600 mm/s. S = 1,600 mm/s x (Tm + Ts) + 8 x (d - 14 mm) . . . Formula (2) If the result of this formula (2) is less than 500 mm, use S = 500 mm. E F3SJ-E/B...

  • マニュアル

    ... (mm) [Calculation example] When Tm = 0.05 s, Ts = 0.015 s, and d = 25 mm: S = 2,000 mm/s x (0.05 s + 0.015 s) + 8 x (25 mm - 14 mm) = 218 mm If the result is less than 100 mm, use S = 100 mm. If the result exceeds 500 mm, use the following formula where K = 1,600 mm/s. S = 1,600 mm/s x (Tm + Ts) + 8 x (d - 14 mm) . . . Formula (2) If the result of this formula (2) is less than 500 mm, use S = 500 mm. E F3SJ-E/B...

  • マニュアル

    ... (mm) [Calculation example] When Tm = 0.05 s, Ts = 0.015 s, and d = 25 mm: S = 2,000 mm/s x (0.05 s + 0.015 s) + 8 x (25 mm - 14 mm) = 218 mm If the result is less than 100 mm, use S = 100 mm. If the result exceeds 500 mm, use the following formula where K = 1,600 mm/s. S = 1,600 mm/s x (Tm + Ts) + 8 x (d - 14 mm) . . . Formula (2) If the result of this formula (2) is less than 500 mm, use S = 500 mm. E F3SJ-B User’...

  • マニュアル

    ... (mm) [Calculation example] When Tm = 0.05 s, Ts = 0.015 s, and d = 25 mm: S = 2,000 mm/s x (0.05 s + 0.015 s) + 8 x (25 mm - 14 mm) = 218 mm If the result is less than 100 mm, use S = 100 mm. If the result exceeds 500 mm, use the following formula where K = 1,600 mm/s. S = 1,600 mm/s x (Tm + Ts) + 8 x (d - 14 mm) . . . Formula (2) If the result of this formula (2) is less than 500 mm, use S = 500 mm. E F3SJ-B User’...

  • マニュアル

    ... (mm) [Calculation example] When Tm = 0.05 s, Ts = 0.015 s, and d = 25 mm: S = 2,000 mm/s x (0.05 s + 0.015 s) + 8 x (25 mm - 14 mm) = 218 mm If the result is less than 100 mm, use S = 100 mm. If the result exceeds 500 mm, use the following formula where K = 1,600 mm/s. S = 1,600 mm/s x (Tm + Ts) + 8 x (d - 14 mm) . . . Formula (2) If the result of this formula (2) is less than 500 mm, use S = 500 mm. E F3SJ-B User’...

  • マニュアル

    ...方たとえば、セルサイズ:0.3mm、ラインスピード:300mm/sの場合は、露光時間は、100μs以下にしてくだ法は? さい。 0.1×0.3(mm)/300(mm/s) = 100(μs) 右パネルにある[カウント]の[読み取り率]は、読み取りサイクルの設定によっては使用できない場合があります。 読み...