全 208 件が検索されました。(41 - 60件を表示)
- マニュアル
...方たとえば、セルサイズ:0.3mm、ラインスピード:300mm/sの場合は、露光時間は、100μs以下にしてくだ法は? さい。 0.1×0.3(mm)/300(mm/s) = 100(μs) V440-F Cマウントコードリーダ ユーザーズマニュアル(SDNC-756) R-3 付録 右パネルにある[カウント]の[読み取り率]は、読み...
- マニュアル
.... Monitor Time Ranges The following table lists the units and ranges of monitor times that can be set. Values 00 to 99 00 to 99 00 to 99 00 to 99 Time unit 0.01 s (10 ms) 0.1 s (100 ms) 1s 1m Note Monitoring will not be performed if “00” is input as the value. 7-2 7-2-1 Editing Sequences Displaying a Sequence List Use one of the following procedures to display a sequence list within a protocol. • Double-click the Protocol List Icon in the project workspace and then left-click the protocol ...
- マニュアル
...4,800 = 110,648 (µs) ≅ 111 (ms) And the communications cycle time in token-bus mode is as follows: 9.1 × 8,000 + 1,300 × 4 + 290 × 8 + 320 × 2 + 4 × 4,024 + 2 × 7 × 8 + 2,290 = 99,458 (µs) ≅ 100 (ms) 9-2-2 Inactive Data Links The following equations are used to calculate a communications cycle time when the data link is inactive. Token-ring Mode 1,740 × B +450 × C + 1,100 × D + 4 × E + 2 × F + 3,000 (µs) Token-bus Mode 1,...
- マニュアル
... one Ai4 Terminal, Segment Linearizer, Basic PID, and A04 terminal) is shown in the following table. CS1W-LCB01/05 (LCCB01/05) Operation cycle: Maximum number of loops 0.01 s: 20 loops 0.02 s: 35 loops 0.05 s: 70 loops 0.1 ...
- マニュアル
... function) Tags 480 max. 960 max. Maximum save Collection cycle Collection cycle time 1 s: 10 h 1 min: 30 days 2 s: 20 h 5 min: 150 days 5 s: 50 h 10 min: 300 days 10 s: 100 h 30 min: 900 days 30 s: 300 h 60 min: 1,800 days Collection cycle Data display Horizontal axis Collection cycle 1 min: 2 h to 10 days 1 s: 2 min to 240 min 5 min: 10 h to 50 days 2 s: 4 min to 240 min 10 min: 20 h to 100 days 5 s: ...
- マニュアル
... is ON in the following example, MLPX(076) will convert 3 digits in S beginning with digit 1 (the second digit), as indicated by C (#0021). The corresponding bits in D100, D101, and D102 will be turned ON. 2 Digits 3 F ...
- マニュアル
... S. S 0.1×C/L reading a moving For example, When a cell size is 0.3 [mm] and a line speed is 300 [mm/s], the exposure time should symbol? be 100 [μs] or less. 0.1×0.3 [mm]/300 [mm/s] = 100 [μs] Read Rate of Counts on the right panel is sometimes not available depending on the setting of Read Cycle. Read Cycle Presentation Continuous Read Triggered Start/Stop Custom Read Rate Unavailable Unavailable Available Available Refer to below Read Rate of Counts on the right When Read Cycle is Custom, it sometimes is ...
- マニュアル
...[Calculation example] When Tm = 0.05 s, Ts = 0.008 s, and d = 14 mm: S=2,000 mm/s x (0.05 s + 0.008 s) + 8 x (14 mm - 14 mm) = 116 mm . . . Formula (2) If the result < 100 mm, use S = 100 mm. If the result exceeds 500 mm, use the following expression where K = 1,600 mm/s. S=1,600 mm/s x (Tm + Ts) + 8 x (d - 14 mm) . . . Formula (3) If the result of this formula (3) < 500 mm, use S = 500 mm. 308 F3SG-SR/PG User’s Manual Wiring and ...
- マニュアル
... exposure time S. reading a moving S ≤ 0.1×C/L symbol? For example, When a cell size is 0.3 [mm] and a line speed is 300 [mm/s], the exposure time should be 100 [μs] or less. 0.1×0.3 [mm]/300 [mm/s] = 100...
- マニュアル
...], use the following formula to get the exposure time S. S ≤ 0.1×C/L For example, When a cell size is 0.3 [mm] and a line speed is 300 [mm/s], the exposure time should be 100 [μs] or less. 0.1×0.3 [mm]/300 [mm/...
- カタログ
..., and A04 terminal) is shown in the following table. CJ1G-CPU43P/44P/45P (LCB03) Operation cycle: Maximum number of loops Number of control loops 0.01 s: 20 loops 0.02 s: 35 loops 0.05 s: 70 loops 0.1 ...
- カタログ
... the edge to be detected. , OFF-delay timer: , One-shot timer: , Used to enable or disable timers. 1 to 20 ms: 1-ms increments, 20 to 200 ms: 5-ms increments, Used to change timer setting when timer is enabled. 200 ms to 1 ...
- カタログ
..., 30 ms, 50 ms, 100 ms, 200 ms or 400 ms. Functions Timer functions Light ON: OFF-delay timer, Dark ON: ON-delay timer 0 to 5 s (1 to 20 ms: 1-ms units, 20 to 200 ms: 5-ms units, 200 ms to 1 s: 100 ms, 1 to 5 s: 1-s units) APC Yes Zero-reset Yes (Negative values can be displayed.) Initial reset Yes (Settings can be returned to defaults.) Sensitivity selection Yes (HIGH/LOW) Teaching level One-point teaching level can be varied from 1% to 50% in increments of 1% Indicators Operation ...
- カタログ
...MODE Key ✽ Power tuning target value (performing power tuning) Used to set the edge to be detected. , 1 to 20 ms: 1-ms increments, 20 to 200 ms: 10-ms increments, Used to change timer settings when timers are enabled. 200 ms to 1 ...
- カタログ
... detection precision. , Used to enable or disable timers. 1 to 20 ms: 1-ms increments, 20 to 200 ms: 5-ms increments, Used to change timer settings when timers are enabled. The timer can be set from 1 to 5000 ms. 200 ms to 1 ...
- カタログ
... intensity determination for red, green, or blue) Timer disabled: , OFF-delay timer: , ON-delay timer: , One-shot timer: 1 to 5000 ms: to 1 to 20 ms: 1-ms increments, 20 to 200 ms: 5-ms increments, 200 ms to 1 ...
- カタログ
...Ratings Rated voltage 24 VDC ±20% (at ambient temperature of 20°C) Rated current Power line: 2.4 A, Signal line: 0.3 A Characteristics Contact resistance 40 mΩ max. (connector section) Insulation resistance After applying 500 VDC for 60 ...
- カタログ
... example] When Tm = 0.05 s, Ts = 0.015 s, and d = 30 mm: S = 2,000 mm/s × (0.05 s + 0.015 s) + 8 × (30 mm - 14 mm) = 258 mm ... formula (2) If the result is less than 100 mm, use S = 100 mm. If the result exceeds 500 mm, use the following formula where K = 1,600 mm/s. S = 1,600 mm/s × (Tm + Ts) + 8 × (d - 14 mm)... formula (3) Approach speed K is not specified in the ANSI B.11.19 standard.To determine the value of K to ...
- カタログ
...ンの0∼50% (変換器前面から可変) 入力スパンの50∼100% (変換器前面から可変) K 3 F S R M S ①z…… 0%、s……100%標準入力 ②z…… 0%、s…… 50% ③z……50%、s…… 50% (②の平行移動) ④z……50%、s……100% (①の平行移動) *出力値を0%に調整するには入力値が0∼50%の範囲内であればできます。 222 K 3FS- ...
- カタログ
.... Power consumption 5 VA max. insulation resistance 20 MΩ min. (at 500 VDC) Dielectric withstand voltage 1,500 VAC for 1 minute (between inputs and outputs) Noise immunity ±1,500 V on input voltage terminals in normal or common mode ±1 µ...