全 1173 件が検索されました。(921 - 940件を表示)

  • マニュアル

    ... Evaluation Criteria while Viewing Measurements. → p. 85 101 Section Display Settings Item 5-4 Details Image age storage s o age Select the conditions for storage of measured images. Coordinates Coo d a es ...

  • マニュアル

    ... 21 cell to 41 x 41 cell (Version 1 to 6) 10 x 10 cell to 26 x 26 cell Readable direction 360 degrees (All directions) Resolution Varies a es acco according d g to o magnification ag ca o a and d f t features off the th lens l to t be b used. d (See (S note.) t ) Reading region Reading depth Note Adjust the field of vision to be at least five pixels per cell. Pixel number is measured by SET/Image Analysis/Measure Length. → p. 127 5 Trigger Inputs and Outputs 1-3 Section ...

  • マニュアル

    ... 1 to 6) 10 x 10 cell to 26 x 26 cell (8 x 32 cell: Pattern only) Readable direction 360 degrees (All directions) Resolution Varies according and a es acco d g to o magnification ag ca o a d f t d (S t ) features off th the llens tto b be used. (See note.) Reading region Reading depth Note Adjust the field of vision to be at least five pixels per cell. Pixel number is measured by SET/Image Analysis/Measure Length. → p. 149 5 Trigger Inputs and Outputs 1-3 Section 1-3 Trigger Inputs ...

  • マニュアル

    ... Evaluation Criteria Evaluation criteria are set for the correlation with the model and the coordinates where the model is found. Scn 0 = SET = 4. Gray search Correlation value range for an OK judgement (0 to 100) Model registration Se Correlation :79 ...

  • マニュアル

    ...OR 24VDC 1.2A + MONITOR VISION MATE CONTROLLER F160 RUN ERROR GATE BUSY ERROR RUN COMIN RESET POWER LLEL PARA STEP 2 CAMERA 1 RD RY CA MEMO - RS-232C/422 INCORRECT Section 1-1 Installation Precautions Ambient Temperature 1,2,3... 1. Maintain a minimum clearance of 50 mm above and below the F160 to improve air circulation. 2. Do not install the F160 immediately above significant heat sources, such as heaters, transformers, or large-capacity resistors. 3. Do not let the ambient operating temperature exceed 50°C (122°F). 4. Provide a forced-air fan cooling or air ...

  • マニュアル

    ...OR 24VDC 1.2A + MONITOR VISION MATE CONTROLLER F160 RUN ERROR GATE BUSY ERROR RUN COMIN RESET POWER LLEL PARA STEP 2 CAMERA 1 RD RY CA MEMO - RS-232C/422 INCORRECT Section 1-1 Installation Precautions Ambient Temperature 1,2,3... 1. Maintain a minimum clearance of 50 mm above and below the F160 to improve air circulation. 2. Do not install the F160 immediately above significant heat sources, such as heaters, transformers, or large-capacity resistors. 3. Do not let the ambient operating temperature exceed 50°C (122°F). 4. Provide a forced-air fan cooling or air ...

  • マニュアル

    ...A variable area is accessed by specifying the position of a variable within the variable area using the variable type and address. Variable types in variable areas are as follows: Variable type C4 C5 C6 C7 C8 C9 ...

  • マニュアル

    ...Application Z183-01.book Page 141 Friday, November 28, 2003 6:43 PM Appendix E Allocations and Setting Sheets Counter Settings Counter address C0 C1 C2 C3 C4 C5 C6 C7 C8 C9 Ca Cb Cc Cd Ce Cf Setting (No. of times) Application Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: 141 Z183-01.book Page 142 Friday, November ...

  • マニュアル

    ...1. Press the EJECT button on the Memory Card Dummy card EJECT button 2. Insert the Memory Card. Insert the Memory Card with its label surface facing up. Com pact Flas h ME MO RY CA RD IN A OM RON Memory Card ■ Removing the Memory Card Before removing the Memory Card, make sure that both the CF power LED and CF access LED are out. Removing the Memory Card with these LEDs lit might cause data recorded on the Memory Section 2 INSTALLATION & CONNECTION slot, and remove the protective dummy card. Card to be lost, or damage the Memory ...

  • マニュアル

    ...; ■: OFF delay; O: One-shot pulse; F: Flashing pulse; W: Twin timer 160 Appendix F Allocations and Setting Table Counter Settings Counter address C0 C1 C2 C3 C4 C5 C6 C7 C8 C9 Ca Cb Cc Cd Ce Cf Setting (No. of times) Application Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: 161 Appendix F Allocations and Setting Table...

  • マニュアル

    ...: A0 Bit 1: A1 Bit 2: A2 Bit 3: A3 --- 0010 Comparator operator H'00000000 to H'00000029 (-) Comparator number specified by leftmost 2 digits of address. P.19 Bit 8: C8 Bit 9: C9 Bit 10: Ca Bit 11: Cb Bit 12: Cc Bit 13: Cd Bit 14: Ce Bit 15: Cf Bit 8: @8 Bit 9: @9 Bit 10: @a Bit 11: @b Bit 12: @c Bit 13: @d Bit 14: @e Bit 15: @f 37 Com Data 0005 SECTION 3 Communications Data Com Data Address Data name Data range (unit) Remarks Bit 8: P8 Bit 9: ...

  • マニュアル

    ...IDRW head 24 V power supply ID tag RS-485 ID link unit (Max. 31 units) IDRW head 24 V power supply For detailed information about the above-mentioned standards, contact SEMI addressed at: 805 East Middlefield Road, Mountain View, ...

  • マニュアル

    ... timer Z234-01.book Page 141 Tuesday, September 13, 2005 5:22 PM Appendix F Allocations and Setting Table Counter Settings Counter address C0 C1 C2 C3 C4 C5 C6 C7 C8 C9 Ca Cb Cc Cd Ce Cf Setting (No. of times) Application Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: Incrementing: Decrementing: Reset: 141 Z234-01.book Page 142 Tuesday, ...

  • マニュアル

    ...Description Fix Value MFT Manufacturer Manufacturer name is read. “OMRON Corporation“ TYP Type of the reader Product form is read. “V750-BA50C04-US“ FWV Firmware version Version of the firmware is read. XXX-XXX-XXX-X SH-MB-FP-...

  • マニュアル

    ... signal OUTPUT signal ENABLE signal ZFV-C User’s Manual 117 Section 5 Setting for Amplifier Unit Gang-Mount Restrictions when Gang-Mounting Amplifier Units ■ ZFV-A_ _ Gang-mounting units The ZFV-A_ _ units cannot be gang-mounted. ■ ZFV-...

  • マニュアル

    ...XMODEM protocol. DATASAVE DATASAVE OK Saves setting data to the controller (flash memory). DATAINIT DATAINIT OK Returns all controller setting data (contents of Flash memory) to their defaults. VERGET VERGET ZFV-...

  • マニュアル

    ... a Smart Sensor and a PLC or other controller using CompoNet communications. It enables monitoring Sensor measurement values and judgment results, as well as reading and setting parameters, from the controller. (The following Sensor Controllers are compatible: ZS-LDC@@, ZS-MDC@@, ZS-HLDC@@, ZFV-...

  • マニュアル

    ... recycling regulation. Japan EU Taiwan Li-ion00 • California regulations concerning perchlorate: This product is a lithium battery that contains perchlorate, which is regulated by the State of California. Please comply with these regulations. For details see the following URL: www.dtsc....

  • マニュアル

    ...Taiwan 2 Installation and Connections Li-ion00 • California regulations concerning perchlorate: This product is a lithium battery that contains perchlorate, which is regulated by the State of California. Please comply with these regulations. For details see the following URL: www.dtsc....

  • マニュアル

    ... Distributor: Tokyo, JAPAN Contact: www.ia.omron.com Regional Headquarters OMRON EUROPE B.V. Wegalaan 67-69-2132 JD Hoofddorp The Netherlands Tel: (31)2356-81-300/Fax: (31)2356-81-388 OMRON SCIENTIFIC TECHNOLOGIES INC. 6550 Dumbarton Circle Fremont, ...